BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Need help with E14  Beaglebone  4.3  LCD  Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 23 replies
  • Answers 6 answers
  • Subscribers 109 subscribers
  • Views 6021 views
  • Users 0 members are here
  • lcd
  • beaglebone black lcd
  • lcd display
  • beagle bone black
  • 4.3" lcd
  • lcd screen
  • BeagleBone
  • beagle_bone
  • beagle_bone_black
  • beagleboneblackwireless
  • beaglebone_black_accessory
  • beagle_board
Related

Need help with E14  Beaglebone  4.3  LCD  Display

ninjatrent
ninjatrent over 9 years ago

I  am  having  trouble  flashing  the  Beaglebone  Black  Wireless eMMC  with  the  image  file  provided for  the  E14 Beaglebone  4.3  LCD  Display.

 

 

README - 4.3 LCD Display Cape for Beaglebone Black

 

4.3 LCD Display Cape for Beaglebone Board (White, Black, or Wireless)

 

 

I have  followed  the  instructions  for  flashing  the  eMMC but it's  not  working.

 

The  LED status lights  on the  BeagleBone  Black  W blink for  a  few seconds  and  go out. The  micro  SD status  light  remains  on constant after attempt  to  flash.

 

I can't figure  this  out. Beginning to  regret  the  purchase  of  this  Display.

The  first  one  arrived  damaged, had to  wait  for  a  replacement .

 

Now on day two  of  trying  to  get  this  display  to  work  with  the  Beaglebone  Black  W.

 

The image will boot from microSD and display will work.

 

I need to flash the eMMC with this image.

 

So far unsuccessful

 

It seems  the   image  is not   compatible  with  the  BBB Wireless.

 

When   checking   available   services  with   " connmanctl  technologies   ", ethernet   and gadget   were   listed   but   not   Bluetooth  and   wifi .image

 

This image   seems  to  be  only  compatible  with  the   Beaglebone  Black  and   not   the   Beaglebone  Black  Wireless .

 

Is there  any  one  who  might  be  able  to  assist  with  finding  a  solution  to  this  problem?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +3 suggested
    Hi Trent, Just by coincidence I was trying to put an image on the BBB Wireless a few nights ago. I don't have a display, so in my case I was using the images on the beagleboard website. Out of curiosity…
  • ninjatrent
    ninjatrent over 8 years ago +3 suggested
    The Debian 9.1 2017-08-31 4GB SD LXQT Desktop image available at Beagleboard is confirmed working properly with the Beaglebone LCD Display Cape. Wi-Fi and Bluetooth are detected. Chromium Desktop works…
  • alager
    alager over 9 years ago +2 suggested
    I don't have the wireless version, but I too had issues getting the image to transfer to the eMMC. What I finally found was that the image that has the bbcape43 support has the eMMC disabled. So in /boot…
Parents
  • alager
    0 alager over 9 years ago

    I don't have the wireless version, but I too had issues getting the image to transfer to the eMMC.  What I finally found was that the image that has the bbcape43 support has the eMMC disabled.

    So in /boot/uEnv.txt make sure that the folllowing two lines are NOT commented out:

     

    ##BeagleBone Black: HDMI (Audio/Video) disabled:

    dtb=am335x-boneblack-emmc-overlay.dtb

     

    and

     

    ##enable Generic eMMC Flasher:

    cmdline=init=/opt/scripts/tools/eMMC/init-eMMC-flasher-v3.sh

     

    The first one enables the eMMC the second one enables the auto copy.  The blue LEDs should go into a night rider mode after 20 seconds or so to indicate thtat the copy is in progress.

    No button presses were required, just insert the SD card then power on.

     

    Aaron

     

    EDIT:

    These are the steps in order, just to be clear:

    1) boot using the SD image that has bbcape43 support.

    2) do the above edits (this will modify the SD card)

    3) reboot

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ninjatrent
    0 ninjatrent over 9 years ago in reply to alager

    The main issue is that this bbcape43 image does not support the onboard wifi chip of the BBB Wireless.

     

     

    You are correct in enabling the eMMC flash process. This is helpful.

     

    The image is not compatible with the BBB Wireless. No matter what I do it only shows ethernet and usb host as available onboard resources. Wireless and Bluetooth work properly with the official Beagleboard Debian image with desktop and smaller iot image. I will have to try these images with the display attached.

     

    Hopefully the bbcape43 image will be updated in future for support of the Wireless and Bluetooth capabilities of the BBB Wireless.

     

    If the official Beagleboard image does not work then I might have to purchase a BBB for use with this display.

     

    Thanks for suggestion.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ninjatrent
    0 ninjatrent over 9 years ago in reply to alager

    The main issue is that this bbcape43 image does not support the onboard wifi chip of the BBB Wireless.

     

     

    You are correct in enabling the eMMC flash process. This is helpful.

     

    The image is not compatible with the BBB Wireless. No matter what I do it only shows ethernet and usb host as available onboard resources. Wireless and Bluetooth work properly with the official Beagleboard Debian image with desktop and smaller iot image. I will have to try these images with the display attached.

     

    Hopefully the bbcape43 image will be updated in future for support of the Wireless and Bluetooth capabilities of the BBB Wireless.

     

    If the official Beagleboard image does not work then I might have to purchase a BBB for use with this display.

     

    Thanks for suggestion.