BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Need help with E14  Beaglebone  4.3  LCD  Display
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 23 replies
  • Answers 6 answers
  • Subscribers 109 subscribers
  • Views 6021 views
  • Users 0 members are here
  • lcd
  • beaglebone black lcd
  • lcd display
  • beagle bone black
  • 4.3" lcd
  • lcd screen
  • BeagleBone
  • beagle_bone
  • beagle_bone_black
  • beagleboneblackwireless
  • beaglebone_black_accessory
  • beagle_board
Related

Need help with E14  Beaglebone  4.3  LCD  Display

ninjatrent
ninjatrent over 9 years ago

I  am  having  trouble  flashing  the  Beaglebone  Black  Wireless eMMC  with  the  image  file  provided for  the  E14 Beaglebone  4.3  LCD  Display.

 

 

README - 4.3 LCD Display Cape for Beaglebone Black

 

4.3 LCD Display Cape for Beaglebone Board (White, Black, or Wireless)

 

 

I have  followed  the  instructions  for  flashing  the  eMMC but it's  not  working.

 

The  LED status lights  on the  BeagleBone  Black  W blink for  a  few seconds  and  go out. The  micro  SD status  light  remains  on constant after attempt  to  flash.

 

I can't figure  this  out. Beginning to  regret  the  purchase  of  this  Display.

The  first  one  arrived  damaged, had to  wait  for  a  replacement .

 

Now on day two  of  trying  to  get  this  display  to  work  with  the  Beaglebone  Black  W.

 

The image will boot from microSD and display will work.

 

I need to flash the eMMC with this image.

 

So far unsuccessful

 

It seems  the   image  is not   compatible  with  the  BBB Wireless.

 

When   checking   available   services  with   " connmanctl  technologies   ", ethernet   and gadget   were   listed   but   not   Bluetooth  and   wifi .image

 

This image   seems  to  be  only  compatible  with  the   Beaglebone  Black  and   not   the   Beaglebone  Black  Wireless .

 

Is there  any  one  who  might  be  able  to  assist  with  finding  a  solution  to  this  problem?

  • Sign in to reply
  • Cancel

Top Replies

  • shabaz
    shabaz over 8 years ago +3 suggested
    Hi Trent, Just by coincidence I was trying to put an image on the BBB Wireless a few nights ago. I don't have a display, so in my case I was using the images on the beagleboard website. Out of curiosity…
  • ninjatrent
    ninjatrent over 8 years ago +3 suggested
    The Debian 9.1 2017-08-31 4GB SD LXQT Desktop image available at Beagleboard is confirmed working properly with the Beaglebone LCD Display Cape. Wi-Fi and Bluetooth are detected. Chromium Desktop works…
  • alager
    alager over 9 years ago +2 suggested
    I don't have the wireless version, but I too had issues getting the image to transfer to the eMMC. What I finally found was that the image that has the bbcape43 support has the eMMC disabled. So in /boot…
Parents
  • ninjatrent
    0 ninjatrent over 8 years ago

    I spoke too soon. Selecting Shutdown caused infinite loop of reboots.

    Same with " sudo shutdown -h now ".

    Holding Power button down is only way to power off now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ninjatrent
    0 ninjatrent over 8 years ago

    I spoke too soon. Selecting Shutdown caused infinite loop of reboots.

    Same with " sudo shutdown -h now ".

    Holding Power button down is only way to power off now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 8 years ago in reply to ninjatrent

    Hi Trent,

     

    That may be an image issue.. I think I have the same problem on my  BeagleBone Blue  Black Wireless: (  (Just bare BB-Blue BBB-W, I don't have any cape attached).

     

    I'm getting used to super-rapidly pulling out the power after I think the board has powered down : )

    I wanted to investigate further to get to the bottom of it, but not had time so far : ( It's only a matter of time before I corrupt the microSD if I keep doing it this way : (

    I've not googled yet to see if others have this problem too, or if there was some resolution.

     

    It is awesome that you've got the display working though! I didn't realize it was capacitive touch enabled. Looks like a very useful product.

     

    (Edit: corrected, I meant to say BBB-W, not BB-Blue. I've not tested BB-Blue).

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ninjatrent
    0 ninjatrent over 8 years ago in reply to shabaz

    Hi Shabaz,

     

    This is the first time experiencing this issue.

     

    Might have to put this display on the shelf until a later time.

     

    The BBB W is needed on other tasks at the moment.

     

    And it is ironic that you mentioned the BB Blue as it's RT Review is due soon.

     

    Thankfully no issues like this have occurred.

     

    Trent

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • ninjatrent
    0 ninjatrent over 8 years ago in reply to shabaz

    Other than the issue with powering down the BBB W, everything worked as desired.

     

    This display is going on a BBB at later time.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to ninjatrent

    Hi Trent,

     

    I'm so sorry, I made a mistake, I meant to say BBB-W, not BB-Blue : (

    I've not tested BB-Blue.

     

    I'm having the same issue of  BBB-W not powering down, as you are.

     

    I'll correct the post I wrote, with the wrong text with strikethough.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • alager
    0 alager over 8 years ago in reply to ninjatrent

    Any news on the reboot issue?  I was going to update to the 9.3, but wondering if others have had any issues.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 8 years ago in reply to alager

    Hi Aaron,

     

    Trent may be able to comment further, but as I understand (and I could be wrong) the full desktop image does reboot when it should shut down, but the smaller IoT image shuts down fine.

    The full desktop image has the issue only when powered from the 5VDC barrel connector. When powered from the USB connector, it shuts down successfully.

    The workaround for now is to quickly unplug the barrel connector once all the LEDs have switched off, before it reboots.

    This is not an LCD cape hardware or software issue, this is an issue in the Linux distribution image as far as I can tell, because I experience it too, and I do not have the LCD cape.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • alager
    0 alager over 8 years ago in reply to shabaz

    On 9.3 I don't get the reboot issue. I am powering via the barrel connector.  However I don't have the LCD working, so maybe it's related to that somehow.

    EDIT: I was wrong.  Since I didn't have a display running, I didn't notice as well what was happening.  It is rebooting.  image