BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum BeagleBone Blue Quadcopter Drone - Need help
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 10 replies
  • Answers 2 answers
  • Subscribers 108 subscribers
  • Views 3234 views
  • Users 0 members are here
  • debian
  • single board computers
  • octavo
  • brushless motors
  • brushless dc motors
  • ardupilot
  • flight control systems
  • beaglebone blue projects
  • rc
  • beaglebone wireless
  • beaglebone black projects
  • Single Board Computer
  • rc plane
  • beaglebone blue drone
  • beaglebone_blue
  • rc car
  • electronic speed controller
  • robotics
  • beaglebone blue
  • flight controls
  • hobby electronics
  • linux debian
  • robot
  • beagleboard.org
  • drone
  • hobbyist
  • battery
  • BeagleBone
  • robotics cape
  • brushless motor
  • beaglebone drone
  • pocket beagle
  • beagleboard
  • texas instruments
  • beaglebone black wireless
  • quadcopter
  • beaglebone quadcopter
  • beagleboneblackwireless
  • robotics controller
  • ti
  • linux
Related

BeagleBone Blue Quadcopter Drone - Need help

ninjatrent
ninjatrent over 8 years ago

Hello Everyone,

 

I would like to use the BeagleBone Blue as the flight controller of my quadcopter drone and run ardupilotblue.

https://github.com/mirkix/ardupilotblue

image

 

The Brushless Motor Speed Control that I am using is the Racestar 20A 4in1 ESC mentioned in this parts list.

https://www.hackster.io/jkridner/beaglebone-blue-220mm-quadcopter-9801d8

image

 

 

I've been following guidance of these links and this tutorial but I've run into a few issues with construction.

     https://github.com/imfatant/test

 

First question, Is this Propeller Layout correct in this photo?

The orange props are the front/nose of the drone and black props at the rear.

image

The orange props have leading edge facing inwards and with the black props the trailing edge is facing inwards to the body.

My terminology and setup might be completely incorrect. For safety reasons the first test will be performed without the propellers attached.

 

 

 

image

In which direction should the ESC be oriented on the the chassis?

 

And Is the label side of ESC board meant to face upwards with the plug facing front of the drone?

image

Also, Which pins from the esc should be connected to the BeagleBone Blue?

image

I would like to mount the ESC to the bottom of the drone as shown in the photo below.

image

I'm unsure if the ESC should be facing label side upward and which direction the control wiring plug should be facing in orientation to the front of the drone.

The Lipo Battery will be located in the center of frame.

image

There will be a small First Person View Camera and transmitter in the nose with 5V power supplied from the BB Blue.

The BeagleBone Blue will be secured to the top deck with the onboard IMU chip at dead center.

 

I am waiting for the FPV Cam/Transmitter and Ublox M8N GPS to arrive tomorrow.

When complete this BB Blue Drone will be running ArduPilotBlue and will be carrying a GoPro Hero 5 Session on flights.

 

Thanks for your time reading this post and for any help.

 

Trent

ninjatrent

  • Sign in to reply
  • Cancel

Top Replies

  • Fred27
    Fred27 over 8 years ago in reply to ninjatrent +2
    They seem to be working now.
  • Fred27
    Fred27 over 8 years ago +2 suggested
    The props look like they match the setup in the Quad X Diagram to me. They will be providing lift when rotating in the direction shown in that diagram. The orientation of the ESC shouldn't matter. The…
  • shabaz
    shabaz over 8 years ago +2 verified
    Hi Trent, Quite surprising how elsewhere on the Internet this project doesn't have a single overall solution diagram or wiring diagram, or a single photo showing such detail. It looks like the original…
Parents
  • shabaz
    0 shabaz over 8 years ago

    Hi Trent,

     

    Quite surprising how elsewhere on the Internet this project doesn't have a single overall solution diagram or wiring diagram, or a single photo showing such detail.

    It looks like the original source of those diagrams is here:

    Connect ESCs and Motors — Copter  documentation

    According to that, the number inside the green and blue circles are the "connected autopilot output pin" .

    The ESC will map the S1..4 signals to the M1..4 motors respectively, so for simplicity I suggest each circled number could be connected to the corresponding M number on the ESC. Then, label the connectors that will go to the BBB end with the same numbers 1..4, and test with them inserted in the order 1,2,3,4, since apparently the software has a test function which has buttons for Test A..D. The diagrams at the link above show what number motor should correspond to A..D, for the Quad + and Quad X etc formations. At that stage (i.e. with no propellers attached), you'll be able to swap the connectors at the BBB end until you've got the motors matching to what the software expects. Then, confirm the rotation directions are correct. If they are not, the motor wires need swapping (pick any two of the three wires to the motor, and swap them).

    So, all this should get the correct motors spinning in the correct directions - I hope! Please do document it when it works : )

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • ninjatrent
    0 ninjatrent over 8 years ago in reply to shabaz

    I think you have the solution here! There will be plenty of photos and documentation. I've taken notes, pics and created a wiring diagram for this ESC. It seems the ESC is meant to be label-side upwards. The motor orientation on this ESC is different than traditional 4 in 1 according to a review. The manual shows wiring for single esc which is not very helpful. The diagram provided by Ardupilot should be the correct layout.

     

    Do you know what the pinout is on brushless motors? On the esc the label for each motor is A,B,C. I can't be so simple as the motor pinouts match the ESC pinout.

     

    Trent

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • ninjatrent
    0 ninjatrent over 8 years ago in reply to shabaz

    I think you have the solution here! There will be plenty of photos and documentation. I've taken notes, pics and created a wiring diagram for this ESC. It seems the ESC is meant to be label-side upwards. The motor orientation on this ESC is different than traditional 4 in 1 according to a review. The manual shows wiring for single esc which is not very helpful. The diagram provided by Ardupilot should be the correct layout.

     

    Do you know what the pinout is on brushless motors? On the esc the label for each motor is A,B,C. I can't be so simple as the motor pinouts match the ESC pinout.

     

    Trent

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • shabaz
    0 shabaz over 8 years ago in reply to ninjatrent

    Hi Trent,

     

    It is great to see all your excellent photos.

    The motors can be wired any way, the connections are symmetrical (i.e. all of the three wires looks the same electrically, each correspond to one end of three windings (the other end is common inside the motor and not accessible). The direction of rotation will depend on the order, but it may be hard to identify that from the motor/wire markings. So, the solution is to wire them up in any order, and see which direction it turns. If the direction is wrong, then any two wires can be swapped around (it doesn't matter which two you select from the three) and the direction of rotation will reverse.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer