BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum BBB can not access Internet via USB to Win-10
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 6 replies
  • Subscribers 108 subscribers
  • Views 4077 views
  • Users 0 members are here
Related

BBB can not access Internet via USB to Win-10

kenunix
kenunix over 6 years ago

I can SSH to 192.168.7.2 OK.

I can connect to virtual USB COM port OK.

I can connect to virtual serial COM port to JTAG OK.

Above using putty

 

I can Firefox to 192.168.7.2 OK

 

I can not ping off the BBB to an external address. I.E.  ping 23.194.117.73 ping to 192.168.7.1 OK.

 

Destination Gateway     Genmask     Flags Metric RefUse Iface
default     192.168.7.1 0.0.0.0     UG0  0    0 usb0
192.168.6.0 0.0.0.0     255.255.255.252 U 0  0    0 usb1
192.168.7.0 0.0.0.0     255.255.255.252 U 0  0    0 usb0

 

 

Is the Win-10 set up to forward packets? I need some help here. Thanks.

  • Sign in to reply
  • Cancel

Top Replies

  • kenunix
    kenunix over 6 years ago +1 verified
    Actually what I had to do follows for Internet access. Took some trial and error. Out of the box the IP addresses 192.168.7.x are only good between two devices. Example a Laptop and the BBB. If you want…
Parents
  • shabaz
    0 shabaz over 6 years ago

    Hi Ken,

     

    It's a Windows issue, not a BBB issue. Once you've got the BBB up-and-running, you can shut it down, and plug it into your home router. Then, you can access it as any normal device, and it will have access to other devices.

    If USB is used in this way, then all the usual nonsense (Internet Connection Sharing, Firewall configuration etc) will need to be attempted to try to get it to work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • shabaz
    0 shabaz over 6 years ago

    Hi Ken,

     

    It's a Windows issue, not a BBB issue. Once you've got the BBB up-and-running, you can shut it down, and plug it into your home router. Then, you can access it as any normal device, and it will have access to other devices.

    If USB is used in this way, then all the usual nonsense (Internet Connection Sharing, Firewall configuration etc) will need to be attempted to try to get it to work.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • kenunix
    0 kenunix over 6 years ago in reply to shabaz

    shabaz,

     

    Unfortunately my only Internet access is using my laptops WiFi connection.

     

    Ken

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 6 years ago in reply to kenunix

    Hi Ken,

     

    Another option is a USB-WiFi adaptor - or connect via Ethernet to wherever your WiFi router is.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • kenunix
    0 kenunix over 6 years ago in reply to shabaz

    Hi,

     

    About your nice article on the BBB A1 serial connection what USB TTL 3.3V, 5V cable did you use?

    A particular brand/model?

     

    Is a case available for the BBB A1 that you know of?

     

    This BBB A1 can still be powered over P.C. to USB-C? Or, separate power supply Volts/Amps?

    If using Usb-C to power BBB how to connect to P.C.?