• Products and Partners
    Products and Partners
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
BeagleBoard
  • Products and Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum BB Blue JST polarity
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 106 subscribers
  • Views 1756 views
  • Users 0 members are here
Related

BB Blue JST polarity

agentsimon
agentsimon over 3 years ago

I cannot find details on the three pin JST battery connectors layout apart from it's positive, sensing and earth. My question is which pin is the positive, is it the one nearest the edge of the board or is this the earth pin? 

I've got a 2P lipo battery but when I plug it into the board all the LEDs flash on and off together. I'm pretty certain that's not meant to happen but can't find any information on what it indicates. 

Any help greatly appreciated. 

  • Sign in to reply
  • Cancel

Top Replies

  • Gough Lui
    Gough Lui over 3 years ago +2
    If this is BeagleBoard Blue - the onboard JST is three-pins and is intended for 2S Li-Pos, not 2P . At a guess, that would be B+, mid, GND being expected, rather than a thermistor as in the single-cell…
  • Gough Lui
    Gough Lui over 3 years ago in reply to agentsimon +1
    I wouldn't pay any mind to any offset in the schematic - that may be purely stylistic and depends on the symbol designer to some extent. https://git.beagleboard.org/beagleboard/beaglebone-blue/-/blob…
  • misaz
    misaz over 3 years ago

    Easiest way is to measure. If you need check battery pinout use DC voltmeter mode on multimeter. If you need to check what pin on board corespond to groud use continuity mode, find some known gound on poin header, test point, or for example connector casings are usualy connected ground. One probe place here and the second probe place on battery connector pin. One pin will beep and this one is ground.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago

    If this is BeagleBoard Blue - the onboard JST is three-pins and is intended for 2S Li-Pos, not 2P. At a guess, that would be B+, mid, GND being expected, rather than a thermistor as in the single-cell sort.

    https://git.beagleboard.org/beagleboard/beaglebone-blue/-/blob/master/BeagleBone_Blue_sch.pdf

    Consult the schematics above - under Battery Connector (Pg1, C7), Pin1 = V_BATT,. Pin2 = BATT_MID, Pin3 = BATT_MINUS.

    - Gough

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • agentsimon
    agentsimon over 3 years ago in reply to Gough Lui

    Thanks, my typos..it's a 2S Li-pos. So, on the physical board which is Pin 1? 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to agentsimon

    Usually the pin that's marked with a triangle indication on the body or a notch in the plastic in the side - the bottom is an example of an JST XH plug that mates with the BeagleBone Blue.
    image

    Of course, this assumes that the board is properly assembled at factory with the connectors facing the right way. If you have doubts, you can probably trace the pins individually and see which lead to ground etc.

    - Gough

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • agentsimon
    agentsimon over 3 years ago in reply to Gough Lui

    Thanks. My eyesight detects the little triangle on the connector. Looking at the schematic there is an left offset to the pins that is mirrored on the physical board. Is that relevant or just a print thing? 

    It's beginning to all click into place.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Gough Lui
    Gough Lui over 3 years ago in reply to agentsimon

    I wouldn't pay any mind to any offset in the schematic - that may be purely stylistic and depends on the symbol designer to some extent.

    https://git.beagleboard.org/beagleboard/beaglebone-blue/-/blob/master/BeagleBone_Blue_brd.pdf

    Refer to the board layout - see the copper top layer:

    image

    Square pads practically always denote the Pin 1 of a connection.

    If these two indications match, then you are absolutely certain of Pin 1 on both plug and receptacle. If not, then someone probably made a mistake somewhere ...

    - Gough