BeagleBoard
  • Products & Partners
  • Dev Tools
  • Single-Board Computers
  • BeagleBoard
  • More
  • Cancel
BeagleBoard
Forum Beaglebone Blue Bricked
  • Blog
  • Forum
  • Documents
  • Quiz
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join BeagleBoard to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 18 replies
  • Subscribers 108 subscribers
  • Views 3942 views
  • Users 0 members are here
  • debian
  • beaglebone#
  • beaglebone blue
Related

Beaglebone Blue Bricked

jomoenginer
jomoenginer over 8 years ago

So, I loaded the latest Debian image for the Beaglebone boards, Debian 9.5 2018-10-07 4GB SD LXQT, and was using this for a short bit, but for some reason after trying to run a QT compiled program via remote ssh the BBBlue froze and will not boot any more.  I powered off the board and when it powers on only the Green and Red LEDS from the status bank stay constantly on and the Battery LEDs flash a bit but then 2 stay on constantly; CHG and the one labeled 75.

I have removed all of the EduMIP connections from the board as well as a n LCD that was connected but still nothing happens.  This board does not have the FTDI connections like the Black so I do not have a way to get a console to it to see if it is locking up somewhere.  

 

I've tried removing the SD card as well as use a known good one but still no luck. 

 

This board was running fine for sometime now so I am not sure what happened.  It was not until I loaded the new image that I ran into an issue.

 

Anyone else run into this issue with the Blue?

  • Sign in to reply
  • Cancel

Top Replies

  • Jan Cumps
    Jan Cumps over 8 years ago +4
    I got it working with an MSP432, Jon I'll write down the instructions. It's easy.
  • Jan Cumps
    Jan Cumps over 8 years ago +3
    I have a Green (from Seeed) - so not the same one as you. Have you tried pushing the User button with the working SD Card inserted, and then providing power?
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jomoenginer +3
    Maybe jkridner knows how to revive a bricked Blue?
Parents
  • shabaz
    shabaz over 8 years ago

    That's disappointing if the design doesn't have UART console pins : (

    I don't have a BB-Blue, but was wondering, does it make any difference if a battery is also connected, as well as the 12V supply? With the original BBB design, if it was modified for battery operation, then the battery needed to be present even if it wasn't charged. Probably the BB-Blue design is different but it could be worth a try. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • jomoenginer
    jomoenginer over 8 years ago in reply to shabaz

    There are a couple of UARTs mapped to JST connections on the Blue.  I'll have to see if I rig a FTDI to JSt connection to one of these to see if there is any console output.

     

    As far as power, I've tried with and without the battery connected while the 12v supply was connected.  I also, tried running with just the battery as well as with just the USB connected.  Each has the same result with the Blue not booting. 

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jomoenginer

    if you happen to have a Bus Pirate, it allows to act as a USB / UART passtrough (attention: 3.3 V signals on the TX/RX pins, not RS232 compatible.

     

    If I recall well, you can also turn an MSP432 LaunchPad in a USB to Uart converter by tapping off the pins between debugger and controller section.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Jan Cumps
    Jan Cumps over 8 years ago in reply to jomoenginer

    if you happen to have a Bus Pirate, it allows to act as a USB / UART passtrough (attention: 3.3 V signals on the TX/RX pins, not RS232 compatible.

     

    If I recall well, you can also turn an MSP432 LaunchPad in a USB to Uart converter by tapping off the pins between debugger and controller section.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
Children
  • jomoenginer
    jomoenginer over 8 years ago in reply to Jan Cumps

    A Bus Pirate would be cool, but I have a few FTDI to USB cables so they should suffice with regards to connecting to  a UART on the Blue.  I am just not sure if the console on the Blue is being sent to a UART or not.  I'll have to try and see.

    • Cancel
    • Vote Up +3 Vote Down