Technical Library
  • Products & Partners
  • Dev Tools
  • Technical Library
  • More
  • Cancel
Technical Library
Documents Raspberry Pi Single Board Computer
  • Documents
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Technical Library to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: atomar
  • Date Created: 21 Feb 2012 6:17 AM Date Created
  • Last Updated Last Updated: 10 Sep 2014 6:17 PM
  • Views 9004 views
  • Likes 3 likes
  • Comments 18 comments
Related
Recommended

Raspberry Pi Single Board Computer

Ordering InformationExclusive AccessoriesTechnical DocumentsVideoFeatures

image

 

Raspberry Pi Add-Ons
imageRaspberry Pi Revision 2 - What's New? image
imageRaspberry Pi Model A versus Model B
imageRaspberryPi Group

The Raspberry PiRaspberry Pi is a single-board computer developed in the UK by the Raspberry Pi Foundation. The Raspberry Pi is a credit-card sized computer that plugs into your TV and a keyboard. It’s a capable little PC which can be used for many of the things that your desktop PC does, like spreadsheets, word-processing and games. It also plays high-definition video. The design is based around a Broadcom BCM2835 SoC, which includes an ARM1176JZF-S 700 MHz processor, VideoCore IV GPU, and 256 or 512 Megabytes of RAM. The design does not include a built-in hard disk or solid-state drive, instead relying on an SD card for booting and long-term storage. This board is intended to run Linux kernel based operating systems.

 

 

The foundation has released two versions; Model A & Model B.

 

  • Model B (Revision 2.0) - It's a latest launched Raspberry Pi Revision 2 with 512MB of RAM memory, two USB ports and a 10/100 Ethernet controller. Click Here to Learn What's New?


 

  • Model B (Revision 1.0) - has 256MB RAM memory, two USB ports and a 10/100 Ethernet controller.


 

  • Model A - has 256 Megabytes (MB) RAM memory, one USB port and no Ethernet controller. Though the Model A doesn't have an RJ45 Ethernet port, it can connect to a network by using a user supplied USB Ethernet or Wi-Fi adapter. As typical of modern computers, generic USB keyboards and mice are compatible with the Raspberry Pi.


 

The Raspberry Pi use Linux-kernel based operating systems. Debian GNU/Linux, Iceweasel, Calligra Suite and Python are planned to be bundled with the Raspberry Pi. The Raspberry Pi does not come with a real-time clock, so an OS must use a network time server, or ask the user for time information at boot time to get access to time and date info for file time and date stamping. However a real time clock (such as the DS1307) with battery backup can be easily added via the I2C interface.

 

 

The Raspberry Pi Foundation has released various SD Card image that can be loaded onto an SD Card to produce a preliminary operating system. The image is based upon Linux version of Debian OS (Raspbian) with the LXDE desktop and the Midori browser, plus various programming tools. The image can also run on QEMU allowing the Raspberry Pi to be emulated on various other platforms.

 

 

 

Exclusive Accessories

 


 

PiRack PiFace DigitalPiCamera
http://uk.farnell.com/productimages/farnell/standard/SC13195-40.jpghttp://uk.farnell.com/productimages/farnell/standard/2218566-40.jpghttp://uk.farnell.com/productimages/farnell/standard/2302279-40.jpg

The PiRack is an expansion board allowing the connection of multiple IO boards to the Raspberry Pi.

 

 

BUY NOWBUY NOW

PiFaceTm  Digital plugs onto the top of your Raspberry Pi, and allows you to sense and control the real world. Learn More>>


 

BUY NOWBUY NOW

Raspberry Pi Camera Board is a custom designed add-on for Raspberry Pi. It attaches to Raspberry Pi by way of one of the small sockets on the board upper surface. Learn More>>

 

BUY NOWBUY NOW

Embedded Pi GertboardWi-Pi
http://uk.farnell.com/productimages/farnell/standard/2301086-40.jpghttp://uk.farnell.com/productimages/farnell/standard/SC12828-501.jpghttp://uk.farnell.com/productimages/farnell/standard/2133900-40.jpg

A triple play platform for connecting the worlds of Raspberry Pi, Arduino and 32-bit embedded ARM. Learn More>>

 



BUY NOWBUY NOW

The Assembled GertboardTm allows your Raspberry Pi to detect and respond to external events. Learn More>>

 

 

 

BUY NOWBUY NOW

Wireless dongle to connect your Raspberry Pi to a Wi-Fi local area network. Learn More>>

 

 

 

BUY NOWBUY NOW

 

 

 

Technical Documents

 


 

Learning Center
TypeDescription
Revision Note imageRaspberry Pi Model B Revision 2.0 (512MB) Changes
User ManualRaspberry Pi: Quick User Guide for Raspberry Pi Single Board Computer
DatasheetBroadcom: Datasheet for BCM2835 SoC used in Raspberry Pi
Training VideosRaspberry Pi Training Videos
ImagesRaspberry Pi RAW Beta Board
PeripheralsRaspberry Pi GPIO Expansion - Low Level Peripherals

 

Design Elements

 

TypeDescription
SchematicRaspberry Pi: Schematic for Raspberry Pi Model B Board

 

Back to top

 

Video

 


 

 

Video 1
Video 2
Video 3
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
Back to top

 

Kit Features

 


 

image

 

Model AModel B
SoCBroadcom BCM2835 (CPU, GPU, DSP, and SDRAM)
CPU:700 MHz ARM1176JZF-S core (ARM11 family)
GPU:Broadcom VideoCore IV, OpenGL ES 2.0, 1080p30 h.264/MPEG-4 AVC high-profile decoder
Memory (SDRAM):256 Megabytes (shared with GPU)512 Megabytes (shared with GPU)
USB 2.0 ports:12 (via integrated USB hub)
Video outputs:Composite RCA, HDMI
Audio outputs:3.5 mm jack, HDMI
Onboard storage:SD, MMC, SDIO card slot
Onboard network:None10/100 Ethernet (RJ45)
Low-level peripherals:8 × GPIO, UART, I²C bus, SPI bus with two chip selects, +3.3 V, +5 V, Ground
Power ratings:500 mA (2.5 W)700 mA (3.5 W)
Power source:5 volt via MicroUSB or GPIO header
Size:85.60 × 53.98 mm (3.370 × 2.125 in)
Operating Systems:Debian GNU/Linux, Fedora, Arch Linux

 

 

 

 

 

 

Back to top

Ordering Information

 


 

 

MPNDescription
RASPBERRY PI 8GB BUNDLERASPBERRY PI 8GB BUNDLE  imageBundle: Raspberry Pi Model B (512MB) Board + Case + Pre-Programmed 8GB SD Card (NOOBS: Enjoy all 6 Operating Systems for Raspberry Pi from single SD card)
RASPBERRY-PI/8GB-USDRASPBERRY-PI/8GB-USDBundle: Raspberry Pi Model B (512MB) Board + Case + 8GB SD Card + MicroSD to SD Converter
KIT-STARTER-RPI/CASE/SD/PWR-UKKIT-STARTER-RPI/CASE/SD/PWR-UKBundle: Raspberry Pi Model B (512MB) Board + Case + Pre-Programmed 4GB SD Card (RASPBIAN) + USB Cable + Mains Plug UK
RPI-B-512-BUNDLE/ANZRPI-B-512-BUNDLE/ANZBundle: Raspberry Pi Model B (512MB) Board + Case + Pre-Programmed 4GB SD Card (Debian) + USB Cable + Mains Plug AU
KIT-STARTER-RPI/CASE/SD/PWR-EUKIT-STARTER-RPI/CASE/SD/PWR-EUBundle: Raspberry Pi Model B (512MB) Board + Case + Pre-Programmed 4GB SD Card (RASPBIAN) + USB Cable + Mains Plug EU
RPI-B-512-CASEDRPI-B-512-CASEDRaspberry Pi Model B (512MB) Board Only - with Case
RASPBRRY-MODB-512MRASPBRRY-MODB-512MRaspberry Pi Model B (512MB) Board Only - without Case
RASPBERRY-MODA-256MRASPBERRY-MODA-256MRaspberry Pi Model A Board Only (without Case)

 

 

Back to top

 


  • arm1176jzf-s
  • raspberrypi
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • e14 Contributor
    e14 Contributor over 14 years ago +1
    +1
  • e14 Contributor
    e14 Contributor over 11 years ago

    Documentation!

    cat /proc/cpuinfo returns BCM2708 Revision 0010 (along with other things like processor type).

    Can I get from here to any documentation on the rasp pi that I have? and if so how?

     

    Thanks,

    very much a newbee. Ian D

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    what happens when one of the tiny cheap and designed to be not flush with the pcb connectors breaks

    how easy are they to repair and replace?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    why couldnt the first version have been sold with the ability to add ram to it?

    when can we see the internet bandwidth we are paying for onscreen along with the pathetic 1-10% of what we are paying for that we actually get

    what USB peripherals are compatible with this device is there a list somewhere

    what are the specs of the GPU

     

    thanks

     

    http://www.youtube.com/watch?v=zsjTpFR0oYQ

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    PS the circuit board, for a wide area around both the USB and RJ45 connectors were painted with flux.

    This is a bad...Ive personally seen excess flux crash a 3,85 MHz clock in a VCR...and the signals on the Pi are a much higher frequency, on the order of 12 MHz on up, possibly to high UHF.

     

    http://alphacpmd.com/~/media/Files/CooksonElectronics/TP%20-RF%20Characterization%20of%20No%20Clean%20Solder%20Flux%20ResiduesWWE%20SM000%20CNP%2020100917.PDF

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    There are hardware failures in the Pi due to faulty design. The below is written by a hardware engineer with massive RFI and circuit test./design experience, plus FCC cert and manufacturing.

     

    Those of you noticing USB problems, its not you, the Pis designers ignored the design requirements of SMSC for the LAN9512 IO chip, heres the long list, since there may be EEs floating through here.

     

    Management at Newark need to take notice, your Company and others are selling faulty product that is mis designed and is NOT USB COMPLIANT.

     

    Main problems:

     

    * false rumours of the need to use a powered USB hub - not relevant to failure of a wireless USB receiver drawing 28 mA

    * false rumours of power supply problems in the Pi (there arent, the supplies are clean and stable on an oscilloscope)

    * Numerous and serious design defects in both the circuits and CBA layout of the Pi - the Pis designers refused to adhere to SMSCs design requirements,

      especially inexcusable since SMSCs website offers design evaluation.

     

    Design defects in the Pi B 512: (this is an engineering level R-E and document, non engineers may not understand it)

    Refer to SMSCs documents on the LAN9512 and App notes (engineers will know how to find those)

     

    For non engineers or programmers:

     

    The USB connector on the Pi is too far from the power connector, many of the electronic components

    associated with the USB chip are incorrectly installed, circuit board layout is wrong (these issues are critical on high speed circuit boards)

    and the USB clock circuit is too close to the USB data lines. These design faults can lead to both hardware and software crash or instability.

     

    =============

     

    List of design failures in the Raspberry Pi, 512 Mb B version:

     

    Source documents:

     

    Raspberry-Pi-Schematics-R1.0.pdf  (schematic of the Pi, incorrect in some areas)

    an1920.pdf (from SMSC)            (Ethernet/USB chip)

    9512_sch.pdf (SMSC)               ( " ")

    NCP1117-D.pdf                     (from ON Semiconductor) power supply regulator 

     

      Comparing the Pi schematic, the Pi board itself and the documentation by the component manufacturers

    we see many design mistakes in the Pi that are causing it to violate the USB design standards

    and not work with common wireless Keyboard and mouse sets.

     

      It is absolutely pointless to make and sell a piece of computer equipment that wont even work

    with a mouse and keyboard.

     

     

     

      There are so many serious electrical design mistakes on the Pi B board that it is pointless

    to even consider using it to develop code.

     

      The popular rumour on the Pi Internet Forums is that the Pi requires use of

    a powered hub as the Pi cannot supply enough current to USB devices. This is an admission

    that the Pis design violates the USB standard, and is also false in that the Pi fails with 

    USB devices that are very low power that do not require a powered hub.

     

    Design analysis:

     

    1.) There is nothing wrong with the Pis power supply (RG2, the bulk regulator that drives

    the USB Hub, 3.3V regulated supply- (NCP1117)). Oscilloscope and DVM (lab quality equipment,

    not hobbyist equipment) prove the power supplies are flat and clean. Bulk supply is 4.95V from

    a switching regulator supply (MCM 28-13060), about 100mV noise floor, the 3.3V supply is about 10 mV.

     

    There is no power supply droop when a 28 mA USB receiver is hot plugged. This indicates RFI causing signal corruption

    in the controller, Ive personally seen that and fixed it in a HVAC controller design.

     

        a.) The power supply connector is too small and fragile.

     

        b.) the power supply as on the Pi is correctly designed according to ON Semiconductors data sheet for the

        NCP1117.

     

      That the Pi cannot supply 600 mA to a 3G modem is a separate topic and is not excusable as this violates the USB standard.

     

    2.) The Pis USB ports do not work with an MCM 83-13110 wireless KBD and mouse or a Microsoft set.

    Both sets work fine with two laptops. The MCM wireless receiver plugs directly into the USB port, and has a receiver 

    and a 12MHz clock, which happens to be the same frequency (?) as a low speed USB device bus.

     

      The USB receivers clock at 12 MHz, and the USB signal frequency being 12, with the SMSC device clock at 25 MHz,

    may be allowing interference at 2f especially since the Pis circuit board is improperly designed as in 

    Sect. 3 (B)(5) of this Document.

     

      When the MCM receiver is used on the Pi, the mouse pointer jumps to the bottom of the screen and stays there.

     

      When used with a Microsoft wireless set, the keyboard exhibits a 'stuck key' symptom when the User attempts to input Username

    and PW. This has been reported on a Pi Forum.

     

      The MCM wireless KBD/mouse receiver draws 28 mA DC quiescent current. This is nearly zero and can not be 

    the source of board crash when the receiver is hot plugged. 

     

        a.) This 28 mA figure is well under the limits in SMSCs document AN1920.pdf, Sect. 4.5.1. and far less

        than the test amount in Sect. 4.5.2.2 of 100 mA.

     

      The problem tended to be mitigated (but not totally eliminated) by using a USB extension cable. The cable changes

    the tuning of the USB lines by adding capacitance and inductance, but more importantly, moves the receiver away

    from the USB socket on the board.

     

      The Pi works with an older Logitech wireless set with a 3 foot USB cable in between WITHOUT a powered hub.

     

      The story is that the Pi must be used with a USB hub, the fact that simply using a USB extension tended to mitigate

    the problem indicates the USB hub story is exactly that, a cover story that hides the failure in the Pi

     

    3.) specific design problems in the Pi:

     

     

     

        Being a hardware engineer particularly experienced in RFI and FCC type acceptance, and having the manufacturers

    data sheets and Pi schematic and two Pi boards, I note the following design flaws in the Pi:

     

    (NOTE: the Pi boards I received do not have the Polyfuse port switching circuit, the USB power is direct to the 5V supply

    and the supply is correct and clean)

      

      a.) the USB connector is located in the wrong place, it, if used with a 3/4G modem for example, will draw the highest current

      and/or highest total energy of any device on the board, so it must be located next to the power connector.

     

     

        Other such boards are designed correctly:

     

        https://www.olimex.com/Products/OLinuXino/iMX233/iMX233-OLinuXino-MAXI/ (power and USB and other connectors on the same side of the board,

        power does not traverse the signal paths. Not the best layout because the USB connector is across the board from the power, but its better)

     

      Notice the folk at Olimex know of the failures in the Pi - https://www.olimex.com/Products/OLinuXino/

      People with hardware engineering experience can catch such failures, persons who only write code cannot.

     

      Another example of 5V supply near the USB connector- http://www.embeddedarm.com/products/board-detail.php?product=TS-7800

     

      An example of doing it badly wrong as in the Pi - Beagle Bone - http://beagleboard.org/bone 

    Read the Wiki on their previous release that was absolutely plagued with design failures- http://elinux.org/BeagleBoard (Revisions section)

     

      (get a copy of their Reference manual and read the disclaimers http://beagleboard.org/static/beaglebone/latest/Docs/Hardware/BONE_SRM.pdf

      They admit to serious RF immunity problems.

     

      Why is the connector location wrong?

     

      Code hacks and hardware designers know the USB power source is DC. They do not realize that the USB supply CURRENT is AC and VERY noisy.

      It is not acceptable to route the USB current past or through sensitive, high speed circuits as the noise from the USB current can corrupt signals.

     

      b.) See the SMSC document AN1920 (an1920.pdf)

     

        This documentation sets out REQUIREMENTS (not suggestions) of how the circuits must be designed. The Pis designers

      ignored them and now have a faulty product.

     

        1.) ibid, Sec. 4.3 requires the USB connector shield to ONLY be AC coupled, the shield on the Pi is soldered to DC ground.

        This allows USB device current to mix with USB signal currents and can cause data corruption.

     

        2.) Sect. 2.9.1 forbids using 90 degree turns on circuit traces, one USB trace on the Pi board has a 90 degree turn.

        Sharp corners radiate noise energy from very high frequency signals.   

     

        3.) Sect 2.8.4 requires bias resistors be on the component side, R23,24 and others are not on the component side.

     

        4.) Sect. 2.5.1 requires crystal circuit components be on the top layer, they are on the bottm of the board.

        A corrupted clock signal could crash the entire IO system and maybe even the processor.

     

        5.) Sect. 4.2, requires DP/DM trace isolation, these traces are routed near R39 and C41, IN THE CRYSTAL OSCILLATOR CIRCUIT.

        This fault, by itself, can crash the whole board by the USB port signals corrupting the clock signal in the hub.

     

        6.) Sect 4.5.3, requires at least 150 uF capacitance for the USB connector, the Pi has a 47 uF, only half the required value.

     

        7.) Sect 2.2, requires one decoupling capacitor for each power pin, there is one missing on page 3 of the Pi schematic

        with the group of 7 power pins including pin 5- 7 pins, 6 capacitors is not "one for each pin."

     

        8.) Sect. 2.2.2 requires CALCULATION of individual decoupling capacitor values, this was not done on the Pi,

        the designers apparently assuming that all such caps are 0.001 uF; this is a common mistake made by designers and experimenters.

     

        9.) Sect 2.1 & 4.5.1 require sufficient power supply. If the Pi cannot supply power to operate USB devices, then its design

        violates both SMSCs requirements and the USB standard and is misleading to advertise to sell as USB -operable when it is not.

     

    4.) See Pi schematic P.3 and Document 9512.pdf. GPIO pins were left floating, this violates the first rule of digital design

    that "every pin must go somewhere". If these lines are left tri state or OD in software, they could couple noise into the package.

     

    5.) See Pi schematic P.3 and 9512.pdf Sect. 2.3. PU/PD pins must have external pull up.down resistors, the Pi schematic

    does not show an external resistor on pin 14. Apparently this entire circuit has been omitted as it didnt function properly.

        

    6.) The USB standard requires hot plug-able operation, hot plugging the KBD/mouse wireless receiver from MCM

    into the Pi crashes the entire board back to a hard reset. This is NOT due to power supply bounce, I have tested

    that with an oscillloscope. It is due to signal corruption.

     

    7.) False and misleading information on the Pi Forums on the web:

     

        a.) USB problems are blamed on lack of a powered hub. They are not, as proven by oscilliscope measurements

        and the fact the wireless KBD/mouse receiver draws 28 mA. Tests prove that even a USB extension cable improves

        operation without being powered,

     

     

     

        b.) claims that Poly fuses were use don the USB ports for over current protection are false, the Polyfuses

        according to Document 9512.pdf, Sect. 2.2.2 are for port power switching, not overcurrent protection.

     

     

     

      This Pi device is not suited for the intended purpose, especially as it is advertised /sold as USB compliant and

    is not, and there is nothing that can be done to remedy it without a complete redesign of the circuits and circuit

    board to comply with the USB specification and requirements of SMSC.

     

     

      As a result of the Pis designers negligence, thousands of these units have been sold to Consumers who are being

    deceived into thinking that the Pi works correctly and they must use a USB hub. This is a false premise.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fustini
    fustini over 14 years ago in reply to e14 Contributor

    You can log in with:

     

    Username: pi

    Password: raspberry

     

    Then you can use "sudo" to execute commands as root.  "sudo su -" will give you a root shell.  "passwd" in the root shell should let you change the root password if you really need to.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    I just need to find the root password from the latest wheezy image file.  Please???

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    try type Raspberry pi 3D dimension under google.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    The RPI-B is bit too slow, wish the RPI-C CPU can up to 1.2GHz and SDRAM up to 1GHz, otherwise, better to overclock it, anyway, it's good for command prompt type, don't expect too much for graph mode when tablet all more then 1GHz CPU. Also, don't expect chinese language on it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    I'd like to see a few goodies posted:

     

    1. Schematics. Most of the stuff I'd like to do involve hardware (adding FPGA peripherals, drivers, etc.). I can back-engineer all this stuff if I have to, but having an official set of documents would be great. I'd also like to add some memory, but that doesn't look like it's feasible.

     

    2. Docs on drivers for peripherals such as USB disks

     

    Raspberry PI is a great platform for teaching, but it could make a good platform for more serious development because it has a relatively stable OS.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>