Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE Support (Deutsch) Error when using UltraLib to exporting Library to Eagle 6.5.0
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 187 subscribers
  • Views 851 views
  • Users 0 members are here
  • eagle
  • librarian
  • ultra
Related

Error when using UltraLib to exporting Library to Eagle 6.5.0

e14 Contributor
e14 Contributor over 12 years ago

Hello,

I am using eagleCAD for the first time (normally use Target 3001).

When I download libraries using Ultra Librarian 5.3.409, and export the .bxl to Eagle compatible .src and run the script to create a new library, the following error occurs:

 

Line 176:

Layer 93:Pins not available!

 

Line 449:

Layer 93:Pins not available!

 

Line 772:

Layer 93:Pins not available!

 

What does this mean? Should I replace layer 93 with another layer (eg 101) in script file? Please find the script file for ADS8331 attached as example.

Attachments:
2014-05-18_18-08-14_Library.scr.zip
  • Sign in to reply
  • Cancel
Parents
  • Richard_H
    Richard_H over 12 years ago

    Hi,

     

    please change the layer selection here. I did a test with layer 37 instead of 93. The packages will then contain a lot of objects that can be simply deleted after importing it into EAGLE. This seems to be a problem of the source file....

    By the way: Layer 93 is only used in schematics or in symbols but not in the layout or package editor. that's the reason why EAGLE complains.

     

    HTH

    Regards,
    Richard

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Richard_H
    Richard_H over 12 years ago

    Hi,

     

    please change the layer selection here. I did a test with layer 37 instead of 93. The packages will then contain a lot of objects that can be simply deleted after importing it into EAGLE. This seems to be a problem of the source file....

    By the way: Layer 93 is only used in schematics or in symbols but not in the layout or package editor. that's the reason why EAGLE complains.

     

    HTH

    Regards,
    Richard