I have a new lib design but i have 3 pins and 4 pad two of which are common
ground. Anyway to connect two common pads to one pin?
I have a new lib design but i have 3 pins and 4 pad two of which are common
ground. Anyway to connect two common pads to one pin?
On 2/7/2011 3:47 PM, Brian wrote:
I have a new lib design but i have 3 pins and 4 pad two of which are common
ground. Anyway to connect two common pads to one pin?
>
Short answer: no. but you can name them gnd@1 and gnd@2 and whatever
appears after the @ will not be shown, which makes it a little better.
On 2/7/2011 3:47 PM, Brian wrote:
I have a new lib design but i have 3 pins and 4 pad two of which are common
ground. Anyway to connect two common pads to one pin?
>
Short answer: no. but you can name them gnd@1 and gnd@2 and whatever
appears after the @ will not be shown, which makes it a little better.
Brian wrote:
I have a new lib design but i have 3 pins and 4 pad two of which are
common ground. Anyway to connect two common pads to one pin?
As Gary said, "no". It is expected in version6
You could fake it the following way but as with all work-arounds, there is a
nasty element to it .
Add a 4th pin to the symbol. For the two pins that will be commoned, make
one the 'medium' length and the second one a 'point' length pin. Place this
point pin 0.1" closer to the body of your device. Turn off the display of
the Pad and Pin names for this 'point' pin.(I also rotate it to prevent the
names from colliding with the other pin)
When using this part on the schematic you need to remember to run the NET
wire to both pins.
Click to on the end of the stub that represents the pin, then click 0.1"
close to the body. The airwires on the board will confirm if you have
succeeded in doing this.
The attached is a three pin version of what I am describing to show you how
it looks - Symbol, Board and Schematic
A compromise but it works.
HTH
Warren
begin 666 Co-Joined-Pins.png
MB5!.1PT*&@H````-24A$4@```84```'," ,````-JD3>````-E!,5$4```!
M@ ! P$"@P("FRO"@H*3@P$#___^@0$! H$# X$# W,#@X$# P$# P,# H(!
M@$# 0$"F8MNQ```0@$E$051XG.V=BYJC*!"%LYFD7;<WSL[[O^RVX@6T0% N
M1SQGOQT3LKE3U& Q'XTHK[EY C6A)<N93U_Z4>BZZ8Y&=-"@A64D"PD@*"
ME100K2 8"4%!"LI(%A)`<%"@C6*UX_;=H%9WE:Y'`;6==ZS)VD-1^!;5
MR<GGK;]_=[]=0K6F:@]ES>T+N-]VMS55>Y3ID?9JA!A_20'!2@H(5E) L)("
M@I44$RD@& E!00K2!820'!2@H(5E) L)("@I44$RD@& E!00K2!820'!
M2@H(5E) L)("@I44$RD@& E!00K2!820'!2@H(5E) L-:Y9SO1I9-9Z]RS
MG>C25_:%1->UB10DRGL6TD!P4H"%920+"2`H5%!"LI(!@)04$RD@6$D!
MP4H"%920+"2`HU#(6VM[7]BUY+\OR&%(23V^F?=:O]:N6SM'-=%-KIW7)L
M=XM\>PJ;5OMN7!B<%-I5\VNY]'1;VX7=UAHI3#4>W$!JM004A@;^'EZ))7)9
M>]5&P:QQ'@JMWB-M6MIM53I"X>VTNL\5K6^G=2-[F?4:C_X0D\*O1KI>NXH+
M[?HTAW74#H5W]YXT)VEOOE6"Y621X*Q.NN#\[A %H\8C@>049M+?C6DR7XO6
M2?X45$N94$Y1D"XXOSU"P:QQJUPC-86%]?^T<TKR3IKE\\:FJTH0,9WWVK
M9K.<%.87G72!>=#)YR[495C<>(B*%=AE[9?-2T$UT-!(P_\CA?=A"M_"
M!1>7B$&AC3Q2;:<(JPTZ6W'6MD)OL2[RI] 8C:;4]U>A/=)BW5YPMAZ@L*[Q
M,E:-,VMKQ JYVSD;A>"XL%B%"TKY>I;9M\91UY%:B[7UL&H*IO#>C%1/4G@+
M% Y$9\:7YO">JYWY$H2!><$RY(07\0[U_:O]O'].KI/L_IW8R1&F/R<(9"
M)UUP?K]'82.CQMJ'CU'PW6?\2]O#K#4JW]NWUDM9[N
SJ3I.9N!2KLVV"
MEM)WKBD. HE/H7;J'VX5;TV/NV<[5(VWFSJOYPOFYLW[!69WMHK8RE^1
M\D3G);%9Y@O-B>@L7' 6*6@BA9TSL
7AO?KN7-SDL)Z[CQ9@RF4F2\X2%.DNC]\=E=@4YDR5]G
MCV@EJZ&J[GC:VB.X6&&[PFQWEH7H?O$I-#N[.Z!-HQN$[)+D?
MR=1>C=-0.&>MCT,C$EAWTH"%920+!>AD(K[]#8BA0D:QP^AR:%,M42BT
MQ@M2";61,$M4EB4DH*EJ>O3 HA5K=(81%]0;+6-$9RJWX*&/.%N_N"OY6^
M(%GCQ(76935$7Y"L\7HDOW/I"Y(U7H_$N'#<&O4YV[]^[9X;_SG;/XV__2_*
ME2?Q.=LAU@O[0HSKMJV^"8-Q(=A7]BWDD(U2U26$1?D*PU47"+%!;1%R1K
M313<(H5%] 7)6A,%MTAA$?=@2%92V+>2`H5%!"LI(!@)04$RD@6$D!P4H*
M"%920+"2`H5%!"LI(!@)04$RD@6$D!P4H"-8Z;B$:DW5'J008DW5'B.%
M1N0;1*?66UY2#>2-55[E-FSW<!^V]W69.U1I$?"C^EJT0*YZVD@& E!00K
M2!820'!2@H(5E) L)("@I44$RD@& E!00K2!8DU&@LHH4$$0""(%!)$"
M@D@!0:2 (%) $"D@B!00]"BB3YEL,^B/E-AUG>7CG5+"`CE4/84_QMNN:QY2
MJ-K!@2%FJ-Z"J:LW_;N]:-/J=:HFL+J_YS5!3,],_GG\_KU5M$<#E4-86M
M5K[PZ?48@T64EE4+09W7/CY_BL`?U1R5VAT-IV"J9^FOLS.8"97-05JJ:P
MB@M#__]Z"/&B,-%?M5,8=9'"P#29QD74FD<`!G]OW6T/7SA;SE,U4KAG^$
M_M\Q7R@Z=ZZ1@NI_O.<+ZM@C*.@/-5'0QS!ZT@/L)Y;<>?8>M(RD](X:BD
M\7^O4%\HJPM3L2_4F!<T(\E=$4,-@?0!.HG44OFP%2K_WV5PJ."WEDK5?.
M1CRAUR#O[W@_85C;1HN:^TRMN0QC>VOY%O=HC095M'LM4`.2ZL^_\P"EM9
MS@_">T[6C" QR/$WG()?7,@W;[X*!=?X)Y$O9%Q'PJ>P/_Y,%1?RK2,A4_ 8
M_P]*Y@O9UI% ?B._P>EB@OYUI'@/@Z@*:$OI!)]A)DQW"@_972Q07]F%(0
M% ZWOQ)]X:1.MK]2RKB01\4H1&E_)?K"`45L?Z6:X\+7<U#,S*WOUUOM"W
M_XAA!G&FJ(G:7ZG6N/ T#S'3Q[(&G[*]7I"V/;_U!0/^L:..B32+]"9VA_
MI2KCPG.F,/VZ[N>-OKJX7E<[:]4HR
=0K]<?AW(67^K"ST-D<0%.-<6&)
M!I\?VTBA4;S4__+E2[1_DH5H(6D3^#;:30S-W1YI1R[:]47US0AT6*PD/U
M2*,WJ'.F3Y=N?Z7Z?$$?FXX4NH7"$ITQVEIOKB@S],TWW7(:T9H_/G4_ W
MP*J\X6GC4+SXPU3^Q<O]$K5Q05S[6C>\_8U/I1C[(N3>'4^8FT1T'U_VH6
MW7732#7??BD?51<75A1>GRFY:>8I0P44#I^?2$X'SVYU&."]E5Y7B2PJGS
M$\DU1IHIFEPJBXN/!P4,I4H7-7YPFK"(0!JKJX8*PCC12>=5$X=7XBN=94
M%05X"!7&!?W0D_AB0A1E]8VEV__U\1A2O$A8>.X>L2$*KT!>/.\Q4@5!D7
M>JTH9"K4=7I"X\)0X)-DBE495P8-5(4(8YOX/(J_4%I7SW-9^ZQC3OIJDU
MHS*1N'YW&P;UKZ@JC -?"Y]>?]F.:V+U[2C7'A4<N"BL(ZWVQ_?VZ NB
M@B@\-0HCBVE'YK(A,S%6\2%8Q2&1G].V)7<8&$P0"EI$5D59[8L=%8^"
MRH](4]&'16)3-OEAIA[N:+X@7RB#IX!0&,NB#MM]L>YVCA47^N>_
M;.TY^BL,"G-9YAV9X[Y8KV)&\@49=I:M5X4I/"4*0XB>`_2R3]RF.'&A&2EL
M_.0N%.:RS,EJ7ZPV1DWN"_L9\SC"10"LN.S"2SMFU<4'FLXT*3!T(\"L?^
M_*))X37],$6G\-B#$,,7.IEU)@A0OJ#R[/7U]16P(S-"7!C\8!L7^I0;K"-9
M[BGT]S;Z7ZWX_6@KDB\(W_Q;<(:@Y[Z>S^A"Y"7!@#M!07?"]]1DCS!6>B
M`T847WA(W_R;^(H#*#C$42:,2("_IQL=\DDC[X6DK70:D>;.-_:%;9M[
M09C5DWC-O_S:5> ZTEWBPGHG[#,,PJ"^#OLQ?!!]P:*GK( K:'78&U$Y[R_8
MXD+UZTB]SD0ZF"C<<07ZE_-&W02@JL.:QH'XD.3@F!@KP?R5\>[33!.. +
MEZ40KC,0`D:J_1S_6=T#=X4/;^PK/B?:IF1P7K"ZI%S#W;I;>+6'5\'4G]
MH>'7RQT7(A73(3F3IT'AU/-4,^C\W%G]U;V7[ OG"N<E*9>Y@_Z2GZ>::R[C
MJPCK2.K83\+8]'K-8:-47'CJ%*9_
MF_EYJC.Y$7SUO&XH-]?&,=#XW$P]'[1_X'$J65Y* P/*7J>6#?:&Y%]P7C
M@D5\01T#T]L"]\WFEL1XD*W]@?-7H"",7-2S\W;[AN]?(]T/Q$LE!0;\:_
M&*OM&WDL\HJ0EQX2.GE?K]@S-.FO]NK0G4W?Q@+0GV\%Q1F%.'?:./>9M6
MUC+N=9\89UN'E-I#"]FYGM2?IXH&H59?F-XM%&I_GNIFOF <8Q=XHT *
MVN Z>=&\E6^8)D\))3@I%<RY,\_>8QC%^D5>Z'P5$.<=([E08G8T9$18=]H;B7VA0R5EVIP,0A)XT>VLLUN!#E+Z0J_Z6&EP)0KJX
M,-3WW(4'OASM46I?"'?UQ!JB?J@$L4%Y0>DX*DTOI"S2[X?!<X,/E!X;AP
M':7PA;S#DWM2V/6'Q0](P5,)?"'S?.E%'SB@N8'SW\CE=*EU'P4>XYZSTI
M[/E#SO%1KWM2V%'VU9O[40A8/QHH%+J_<#DE](7#90K3[N[ :\BWNGYQ(>OX
MJ%?IYHLDWK2%U+M[JA<>&1)R[<3"<#.%Q@5B2"'0^<-%Z.Q+@07Z#K
M2#=3#H2,<07Z/V%F\GWOK-?X$48@OTOO/-Y+\?25M7)87(`MV/=#.%[%-E
M7$BE@_M4K7^ B\HG4D 0*2"(%!!$"@@B!021`H)((9;:]OBYI!!+I( @4D 0
M2"(%!!$"@@B!021`H)(`4&D@"!20! I((@4$$0""(%!)$"@D@!0:2 (%)
M$"D@B!001 H(
]@((5(:ML3&$@ACMKV# 8("G\74KP:M,<TG8Y H10$4M 5
MLSD9;MIUS"10AQ=/R[40.'Z8Z0J%Q^OE A>/GDD(LD0)"MJ2 D"TI(&1
M"@C9D@)"MJ2 D"TI(&1"@C9D@)"MJ2 D"TI(&1"@C9D@)"MJ2 D"TI(&1+
M"@C9D@)"MM 4WOL?@:'@45:[P"B\!VFO9X/EA((4]+(VEF)["HV"\>][;GUK
MO4I2&%YMROI>4KT%26$XO.?#6$E1Q2FLRZJE@N>0F.7 N@J;Z&A?L8U(
M(9LO-.@4-EUF-7$!?XRD7HXQ62]K36.D=6@0M4\A?"#O.4VQEC4\4S0*&P?8
M&7.4I& K:WBN:!2,EP<I!$_]WI8S[/,OK4=:E;6BD>KX\F"/%#SU,T^80ZUC
M_K6BH&5C]E.>@J70MO]-7\7WVUZOR8[A<W4;X"_G7>U:O*=2U@C%K'F+
M9P>]EF6X:Y^ ;RELC7O9AH<?3: 4U"]_MO_H#%[<S<LU*1S\Q:A-?PGR
M\EK\-3/G'MNAKQ#*D@?T5N@!W)%")G(D$(I[!:?O:@L!I56;IX"0((!4L=
M#VB3E57VD:K>]#O#QU7P]W @V'MM,2GX_P38X0O:NST*F[>D,%[-"\(>!;^I
MWZK-/4>J$85*P?<GP%X4/./"^HR=65M$P5+PU%Z/M'3XCJG?9OZE3<#\LSVA
M&BF8"A_('YPLGA I'#J#% S![$<Z)5) R)84$(E!81L20$A6U) R)84$*]
M,X4SIY*"+E(@A5@BA>S9"KHKA9-/:B8%0_0%4H@E4LB>K2!2R)ZMH#M3P,F6
M%!"R)06$;$D!(5M20,B6%!"R)06$;$D!(5M20,B6%!"R)06$;$D!(5M20,B6
M%!"RO3Z%0HI:"U(@!4J)%!!$"@@B!021`H)(`4&D@"!20! I((@4$$0*""(%
M!)$"@D@!0:2 (%) $"D@B!001 H((@4$D0"2 %!I( @4D 02"(%!!$"@@B
M!021`H)(`4&D@"!20! I((@4$$0*""(%!)$"@D@!0:2 (%) $"D@B!00%(\"
;54:D@#_`7 #6[7,PR\`````$E%3D2N0F""
`
end
On 2/7/2011 3:57 PM, Brian wrote:
Have that done but only the one labeled GND gets connected to ground. The
other has no pin connected to it so it reamins floating.
"Gary Gofstein"<nospam@use.forum.net> wrote in message
news:iiq0hh$epp$1@cheetah.cadsoft.de...
>> On 2/7/2011 3:47 PM, Brian wrote:
>>> I have a new lib design but i have 3 pins and 4 pad two of which are
>>> common
>>> ground. Anyway to connect two common pads to one pin?
>>>
>>>
>> Short answer: no. but you can name them gnd@1 and gnd@2 and whatever
>> appears after the @ will not be shown, which makes it a little better.
>
yes, each must have a pin in the schematic and you must connect it there..