EAGLE User Chat (English) Pins to pads
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
  • Replies 5 replies
  • Subscribers 179 subscribers
  • Views 547 views
  • Users 0 members are here
Related

Pins to pads

Former Member
Former Member over 14 years ago

I have a new lib design but i have 3 pins and 4 pad two of which are common

ground. Anyway to connect two common pads to one pin?

 

 

 

  • Sign in to reply
  • Cancel
Parents
  • Former Member
    Former Member over 14 years ago

    On 2/7/2011 3:47 PM, Brian wrote:

    I have a new lib design but i have 3 pins and 4 pad two of which are common

    ground. Anyway to connect two common pads to one pin?

     

    >

    Short answer: no. but you can name them gnd@1 and gnd@2 and whatever

    appears after the @ will not be shown, which makes it a little  better.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    Brian wrote:

    I have a new lib design but i have 3 pins and 4 pad two of which are

    common ground. Anyway to connect two common pads to one pin?

     

    As Gary said, "no". It is expected in version6

    You could fake it the following way but as with all work-arounds, there is a

    nasty element to it .

     

    Add a 4th pin to the symbol. For the two pins that will be commoned, make

    one the 'medium' length and the second one a 'point' length pin. Place this

    point pin 0.1" closer to the body of your device. Turn off  the display of

    the Pad and Pin names for this 'point' pin.(I also rotate it to prevent the

    names from colliding with the other pin)

     

    When using this part on the schematic you need to remember to run the NET

    wire to both pins.

    Click to on the end of the stub that represents the pin, then click 0.1"

    close to the body.  The airwires on the board will confirm if  you have

    succeeded in doing this.

     

    The attached is a three pin version of what I am describing to show you how

    it looks - Symbol, Board and Schematic

    A compromise but it works.

     

    HTH

    Warren

     

     

    begin 666 Co-Joined-Pins.png

    MB5!.1PT*&@H````-24A$4@```84```'," ,````-JD3>````-E!,5$4```!

    M@ ! P$"@P("FRO"@H*3@P$#___^@0$! H$# X$# W,#@X$# P$# P,# H(!

    M@$# 0$"F8MNQ```0@$E$051XG.V=BYJC*!"%LYFD7;<WSL[[O^RVX@6T0% N

    M1SQGOQT3LKE3U& Q'XTHK[EY C6A)<N93U_Z4>BZZ8Y&=-"@A64D"PD@*"

    ME100K2 8"4%!"LI(%A)`<%"@C6*UX_;=H%9WE:Y'`;6==ZS)VD-1^!;5

    MR<GGK;]_=[]=0K6F:@]ES>T+N-]VMS55>Y3ID?9JA!A_20'!2@H(5E) L)("

    M@I44$RD@& E!00K2!820'!2@H(5E) L)("@I44$RD@& E!00K2!820'!

    M2@H(5E) L)("@I44$RD@& E!00K2!820'!2@H(5E) L-:Y9SO1I9-9Z]RS

    MG>C25_:%1->UB10DRGL6TD!P4H"%920+"2`H5%!"LI(!@)04$RD@6$D!

    MP4H"%920+"2`HU#(6VM[7]BUY+\OR&%(23V^F?=:O]:N6SM'-=%-KIW7)L

    M=XM\>PJ;5OMN7!B<%-I5\VNY]'1;VX7=UAHI3#4>W$!JM004A@;^'EZ))7)9

    M>]5&P:QQ'@JMWB-M6MIM53I"X>VTNL\5K6^G=2-[F?4:C_X0D\*O1KI>NXH+

    M[?HTAW74#H5W]YXT)VEOOE6"Y621X*Q.NN#\[A %H\8C@>049M+?C6DR7XO6

    M2?X45$N94$Y1D"XXOSU"P:QQJUPC-86%]?^T<TKR3IKE\\:FJTH0,9WWVK

    M9K.<%.87G72!>=#)YR[495C<>(B*%=AE[9?-2T$UT-!(P_\CA?=A"M_"

    M!1>7B$&AC3Q2;:<(JPTZ6W'6MD)OL2[RI] 8C:;4]U>A/=)BW5YPMAZ@L*[Q

    M,E:-,VMKQ JYVSD;A>"XL%B%"TKY>I;9M\91UY%:B[7UL&H*IO#>C%1/4G@+

    M% Y$9\:7YO">JYWY$H2!><$RY(07\0[U_:O]O'].KI/L_IW8R1&F/R<(9"

    M)UUP?K]'82.CQMJ'CU'PW6?\2]O#K#4JW]NWUDM9[N
    SJ3I.9N!2KLVV"

    MEM)WKBD. HE/H7;J'VX5;TV/NV<[5(VWFSJOYPOFYLW[!69WMHK8RE^1

    M\D3G);%9Y@O-B>@L7' 6*6@BA9TSL
    7AO?KN7-SDL)Z[CQ9@RF4F2\X2%.DNC]\=E=@4YDR5]G

    MCV@EJZ&J[GC:VB.X6&&[PFQWEH7H?O$I-#N[.Z!-HQN$[)+D?

    MR=1>C=-0.&>MCT,C$EAWTH"%920+!>AD(K[]#8BA0D:QP^AR:%,M42BT

    MQ@M2";61,$M4EB4DH*EJ>O3 HA5K=(81%]0;+6-$9RJWX*&/.%N_N"OY6^

    M(%GCQ(76935$7Y"L\7HDOW/I"Y(U7H_$N'#<&O4YV[]^[9X;_SG;/XV__2_*

    ME2?Q.=LAU@O[0HSKMJV^"8-Q(=A7]BWDD(U2U26$1?D*PU47"+%!;1%R1K

    M313<(H5%] 7)6A,%MTAA$?=@2%92V+>2`H5%!"LI(!@)04$RD@6$D!P4H*

    M"%920+"2`H5%!"LI(!@)04$RD@6$D!P4H"-8Z;B$:DW5'J008DW5'B.%

    M1N0;1*?66UY2#>2-55[E-FSW<!^V]W69.U1I$?"C^EJT0*YZVD@& E!00K

    M2!820'!2@H(5E) L)("@I44$RD@& E!00K2!8DU&@LHH4$$0""(%!)$"

    M@D@!0:2 (%) $"D@B!00]"BB3YEL,^B/E-AUG>7CG5+"`CE4/84_QMNN:QY2

    MJ-K!@2%FJ-Z"J:LW_;N]:-/J=:HFL+J_YS5!3,],_GG\_KU5M$<#E4-86M

    M5K[PZ?48@T64EE4+09W7/CY_BL`?U1R5VAT-IV"J9^FOLS.8"97-05JJ:P

    MB@M#__]Z"/&B,-%?M5,8=9'"P#29QD74FD<`!G]OW6T/7SA;SE,U4KAG^$

    M_M\Q7R@Z=ZZ1@NI_O.<+ZM@C*.@/-5'0QS!ZT@/L)Y;<>?8>M(RD](X:BD

    M\7^O4%\HJPM3L2_4F!<T(\E=$4,-@?0!.HG44OFP%2K_WV5PJ."WEDK5?.

    M1CRAUR#O[W@_85C;1HN:^TRMN0QC>VOY%O=HC095M'LM4`.2ZL^_\P"EM9

    MS@_">T[6C" QR/$WG()?7,@W;[X*!=?X)Y$O9%Q'PJ>P/_Y,%1?RK2,A4_ 8

    M_P]*Y@O9UI% ?B._P>EB@OYUI'@/@Z@*:$OI!)]A)DQW"@_972Q07]F%(0

    M% ZWOQ)]X:1.MK]2RKB01\4H1&E_)?K"`45L?Z6:X\+7<U#,S*WOUUOM"W

    M_XAA!G&FJ(G:7ZG6N/ T#S'3Q[(&G[*]7I"V/;_U!0/^L:..B32+]"9VA_

    MI2KCPG.F,/VZ[N>-OKJX7E<[:]4HR
    =0K]<?AW
    (67^K"ST-D<0%.-<6&)

    M!I\?VTBA4;S4__+E2[1_DH5H(6D3^#;:30S-W1YI1R[:]47US0AT6*PD/U

    M2*,WJ'.F3Y=N?Z7Z?$$?FXX4NH7"$ITQVEIOKB@S],TWW7(:T9H_/G4_ W

    MP*J\X6GC4+SXPU3^Q<O]$K5Q05S[6C>\_8U/I1C[(N3>'4^8FT1T'U_VH6

    MW7732#7??BD?51<75A1>GRFY:>8I0P44#I^?2$X'SVYU&."]E5Y7B2PJGS

    M$\DU1IHIFEPJBXN/!P4,I4H7-7YPFK"(0!JKJX8*PCC12>=5$X=7XBN=94

    M%05X"!7&!?W0D_AB0A1E]8VEV__U\1A2O$A8>.X>L2$*KT!>/.\Q4@5!D7

    M>JTH9"K4=7I"X\)0X)-DBE495P8-5(4(8YOX/(J_4%I7SW-9^ZQC3OIJDU

    MHS*1N'YW&P;UKZ@JC -?"Y]>?]F.:V+U[2C7'A4<N"BL(ZWVQ_?VZ NB

    M@B@\-0HCBVE'YK(A,S%6\2%8Q2&1G].V)7<8&$P0"EI$5D59[8L=%8^"

    MRH](4]&'16)3-OEAIA[N:+X@7RB#IX!0&,NB#MM]L>YVCA47^N>_

    M;.TY^BL,"G-9YAV9X[Y8KV)&\@49=I:M5X4I/"4*0XB>`_2R3]RF.'&A&2EL

    M_.0N%.:RS,EJ7ZPV1DWN"_L9\SC"10"LN.S"2SMFU<4'FLXT*3!T(\"L?^

    M_*))X37],$6G\-B#$,,7.IEU)@A0OJ#R[/7U]16P(S-"7!C\8!L7^I0;K"-9

    M[BGT]S;Z7ZWX_6@KDB\(W_Q;<(:@Y[Z>S^A"Y"7!@#M!07?"]]1DCS!6>B

    M`T847WA(W_R;^(H#*#C$42:,2("_IQL=\DDC[X6DK70:D>;.-_:%;9M[

    M09C5DWC-O_S:5> ZTEWBPGHG[#,,PJ"^#OLQ?!!]P:*GK( K:'78&U$Y[R_8

    MXD+UZTB]SD0ZF"C<<07ZE_-&W02@JL.:QH'XD.3@F!@KP?R5\>[33!.. +

    MEZ40KC,0`D:J_1S_6=T#=X4/;^PK/B?:IF1P7K"ZI%S#W;I;>+6'5\'4G]

    MH>'7RQT7(A73(3F3IT'AU/-4,^C\W%G]U;V7[ OG"N<E*9>Y@_Z2GZ>::R[C

    MJPCK2.K83\+8]'K-8:-47'CJ%*9_

    MF_EYJC.Y$7SUO&XH-]?&,=#XW$P]'[1_X'$J65Y* P/*7J>6#?:&Y%]P7C

    M@D5\01T#T]L"]\WFEL1XD*W]@?-7H"",7-2S\W;[AN]?(]T/Q$LE!0;\:_

    M&*OM&WDL\HJ0EQX2.GE?K]@S-.FO]NK0G4W?Q@+0GV\%Q1F%.'?:./>9M6

    MUC+N=9\89UN'E-I#"]FYGM2?IXH&H59?F-XM%&I_GNIFOF <8Q=XHT *

    MVN Z>=&\E6^8)D\))3@I%<RY,\_>8QC%^D5>Z'P5$.<=([E08G8T9$18=]H;B7VA0R5EVIP,0A)XT>VLLUN!#E+Z0J_Z6&EP)0KJX

    M,-3WW(4'OASM46I?"'?UQ!JB?J@$L4%Y0>DX*DTOI"S2[X?!<X,/E!X;AP

    M':7PA;S#DWM2V/6'Q0](P5,)?"'S?.E%'SB@N8'SW\CE=*EU'P4>XYZSTI

    M[/E#SO%1KWM2V%'VU9O[40A8/QHH%+J_<#DE](7#90K3[N[ :\BWNGYQ(>OX

    MJ%?IYHLDWK2%U+M[JA<>&1)R[<3"<#.%Q@5B2"'0^<-%Z.Q+@07Z#K

    M2#=3#H2,<07Z/V%F\GWOK-?X$48@OTOO/-Y+\?25M7)87(`MV/=#.%[%-E

    M7$BE@_M4K7^ B\HG4D 0*2"(%!!$"@@B!021`H)((9;:]OBYI!!+I( @4D 0

    M2"(%!!$"@@B!021`H)(`4&D@"!20! I((@4$$0""(%!)$"@D@!0:2 (%)

    M$"D@B!001 H(image]@((5(:ML3&$@ACMKV# 8("G\74KP:M,<TG8Y H10$4M 5

    MLSD9;MIUS"10AQ=/R[40.'Z8Z0J%Q^OE A>/GDD(LD0)"MJ2 D"TI(&1

    M"@C9D@)"MJ2 D"TI(&1"@C9D@)"MJ2 D"TI(&1"@C9D@)"MJ2 D"TI(&1+

    M"@C9D@)"MM 4WOL?@:'@45:[P"B\!VFO9X/EA((4]+(VEF)["HV"\>][;GUK

    MO4I2&%YMROI>4KT%26$XO.?#6$E1Q2FLRZJE@N>0F.7 N@J;Z&A?L8U(

    M(9LO-.@4-EUF-7$!?XRD7HXQ62]K36.D=6@0M4\A?"#O.4VQEC4\4S0*&P?8

    M&7.4I& K:WBN:!2,EP<I!$_]WI8S[/,OK4=:E;6BD>KX\F"/%#SU,T^80ZUC

    M_K6BH&5C]E.>@J70MO]-7\7WVUZOR8[A<W4;X"_G7>U:O*=2U@C%K'F+

    M9P>]EF6X:Y^ ;RELC7O9AH<?3: 4U"]_MO_H#%[<S<LU*1S\Q:A-?PGR

    M\EK\-3/G'MNAKQ#*D@?T5N@!W)%")G(D$(I[!:?O:@L!I56;IX"0((!4L=

    M#VB3E57VD:K>]#O#QU7P]W @V'MM,2GX_P38X0O:NST*F[>D,%[-"\(>!;^I

    MWZK-/4>J$85*P?<GP%X4/./"^HR=65M$P5+PU%Z/M'3XCJG?9OZE3<#\LSVA

    M&BF8"A_('YPLGA I'#J#% S![$<Z)5) R)84$(E!81L20$A6U) R)84$*]

    M,X4SIY*"+E(@A5@BA>S9"KHKA9-/:B8%0_0%4H@E4LB>K2!2R)ZMH#M3P,F6

    M%!"R)06$;$D!(5M20,B6%!"R)06$;$D!(5M20,B6%!"R)06$;$D!(5M20,B6

    M%!"RO3Z%0HI:"U(@!4J)%!!$"@@B!021`H)(`4&D@"!20! I((@4$$0*""(%

    M!)$"@D@!0:2 (%) $"D@B!001 H((@4$D0"2 %!I( @4D 02"(%!!$"@@B

    M!021`H)(`4&D@"!20! I((@4$$0*""(%!)$"@D@!0:2 (%) $"D@B!00%(\"

    ;54:D@#_`7 #6[7,PR\`````$E%3D2N0F""

    `

    end

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    Brian wrote:

    I have a new lib design but i have 3 pins and 4 pad two of which are

    common ground. Anyway to connect two common pads to one pin?

     

    As Gary said, "no". It is expected in version6

    You could fake it the following way but as with all work-arounds, there is a

    nasty element to it .

     

    Add a 4th pin to the symbol. For the two pins that will be commoned, make

    one the 'medium' length and the second one a 'point' length pin. Place this

    point pin 0.1" closer to the body of your device. Turn off  the display of

    the Pad and Pin names for this 'point' pin.(I also rotate it to prevent the

    names from colliding with the other pin)

     

    When using this part on the schematic you need to remember to run the NET

    wire to both pins.

    Click to on the end of the stub that represents the pin, then click 0.1"

    close to the body.  The airwires on the board will confirm if  you have

    succeeded in doing this.

     

    The attached is a three pin version of what I am describing to show you how

    it looks - Symbol, Board and Schematic

    A compromise but it works.

     

    HTH

    Warren

     

     

    begin 666 Co-Joined-Pins.png

    MB5!.1PT*&@H````-24A$4@```84```'," ,````-JD3>````-E!,5$4```!

    M@ ! P$"@P("FRO"@H*3@P$#___^@0$! H$# X$# W,#@X$# P$# P,# H(!

    M@$# 0$"F8MNQ```0@$E$051XG.V=BYJC*!"%LYFD7;<WSL[[O^RVX@6T0% N

    M1SQGOQT3LKE3U& Q'XTHK[EY C6A)<N93U_Z4>BZZ8Y&=-"@A64D"PD@*"

    ME100K2 8"4%!"LI(%A)`<%"@C6*UX_;=H%9WE:Y'`;6==ZS)VD-1^!;5

    MR<GGK;]_=[]=0K6F:@]ES>T+N-]VMS55>Y3ID?9JA!A_20'!2@H(5E) L)("

    M@I44$RD@& E!00K2!820'!2@H(5E) L)("@I44$RD@& E!00K2!820'!

    M2@H(5E) L)("@I44$RD@& E!00K2!820'!2@H(5E) L-:Y9SO1I9-9Z]RS

    MG>C25_:%1->UB10DRGL6TD!P4H"%920+"2`H5%!"LI(!@)04$RD@6$D!

    MP4H"%920+"2`HU#(6VM[7]BUY+\OR&%(23V^F?=:O]:N6SM'-=%-KIW7)L

    M=XM\>PJ;5OMN7!B<%-I5\VNY]'1;VX7=UAHI3#4>W$!JM004A@;^'EZ))7)9

    M>]5&P:QQ'@JMWB-M6MIM53I"X>VTNL\5K6^G=2-[F?4:C_X0D\*O1KI>NXH+

    M[?HTAW74#H5W]YXT)VEOOE6"Y621X*Q.NN#\[A %H\8C@>049M+?C6DR7XO6

    M2?X45$N94$Y1D"XXOSU"P:QQJUPC-86%]?^T<TKR3IKE\\:FJTH0,9WWVK

    M9K.<%.87G72!>=#)YR[495C<>(B*%=AE[9?-2T$UT-!(P_\CA?=A"M_"

    M!1>7B$&AC3Q2;:<(JPTZ6W'6MD)OL2[RI] 8C:;4]U>A/=)BW5YPMAZ@L*[Q

    M,E:-,VMKQ JYVSD;A>"XL%B%"TKY>I;9M\91UY%:B[7UL&H*IO#>C%1/4G@+

    M% Y$9\:7YO">JYWY$H2!><$RY(07\0[U_:O]O'].KI/L_IW8R1&F/R<(9"

    M)UUP?K]'82.CQMJ'CU'PW6?\2]O#K#4JW]NWUDM9[N
    SJ3I.9N!2KLVV"

    MEM)WKBD. HE/H7;J'VX5;TV/NV<[5(VWFSJOYPOFYLW[!69WMHK8RE^1

    M\D3G);%9Y@O-B>@L7' 6*6@BA9TSL
    7AO?KN7-SDL)Z[CQ9@RF4F2\X2%.DNC]\=E=@4YDR5]G

    MCV@EJZ&J[GC:VB.X6&&[PFQWEH7H?O$I-#N[.Z!-HQN$[)+D?

    MR=1>C=-0.&>MCT,C$EAWTH"%920+!>AD(K[]#8BA0D:QP^AR:%,M42BT

    MQ@M2";61,$M4EB4DH*EJ>O3 HA5K=(81%]0;+6-$9RJWX*&/.%N_N"OY6^

    M(%GCQ(76935$7Y"L\7HDOW/I"Y(U7H_$N'#<&O4YV[]^[9X;_SG;/XV__2_*

    ME2?Q.=LAU@O[0HSKMJV^"8-Q(=A7]BWDD(U2U26$1?D*PU47"+%!;1%R1K

    M313<(H5%] 7)6A,%MTAA$?=@2%92V+>2`H5%!"LI(!@)04$RD@6$D!P4H*

    M"%920+"2`H5%!"LI(!@)04$RD@6$D!P4H"-8Z;B$:DW5'J008DW5'B.%

    M1N0;1*?66UY2#>2-55[E-FSW<!^V]W69.U1I$?"C^EJT0*YZVD@& E!00K

    M2!820'!2@H(5E) L)("@I44$RD@& E!00K2!8DU&@LHH4$$0""(%!)$"

    M@D@!0:2 (%) $"D@B!00]"BB3YEL,^B/E-AUG>7CG5+"`CE4/84_QMNN:QY2

    MJ-K!@2%FJ-Z"J:LW_;N]:-/J=:HFL+J_YS5!3,],_GG\_KU5M$<#E4-86M

    M5K[PZ?48@T64EE4+09W7/CY_BL`?U1R5VAT-IV"J9^FOLS.8"97-05JJ:P

    MB@M#__]Z"/&B,-%?M5,8=9'"P#29QD74FD<`!G]OW6T/7SA;SE,U4KAG^$

    M_M\Q7R@Z=ZZ1@NI_O.<+ZM@C*.@/-5'0QS!ZT@/L)Y;<>?8>M(RD](X:BD

    M\7^O4%\HJPM3L2_4F!<T(\E=$4,-@?0!.HG44OFP%2K_WV5PJ."WEDK5?.

    M1CRAUR#O[W@_85C;1HN:^TRMN0QC>VOY%O=HC095M'LM4`.2ZL^_\P"EM9

    MS@_">T[6C" QR/$WG()?7,@W;[X*!=?X)Y$O9%Q'PJ>P/_Y,%1?RK2,A4_ 8

    M_P]*Y@O9UI% ?B._P>EB@OYUI'@/@Z@*:$OI!)]A)DQW"@_972Q07]F%(0

    M% ZWOQ)]X:1.MK]2RKB01\4H1&E_)?K"`45L?Z6:X\+7<U#,S*WOUUOM"W

    M_XAA!G&FJ(G:7ZG6N/ T#S'3Q[(&G[*]7I"V/;_U!0/^L:..B32+]"9VA_

    MI2KCPG.F,/VZ[N>-OKJX7E<[:]4HR
    =0K]<?AW
    (67^K"ST-D<0%.-<6&)

    M!I\?VTBA4;S4__+E2[1_DH5H(6D3^#;:30S-W1YI1R[:]47US0AT6*PD/U

    M2*,WJ'.F3Y=N?Z7Z?$$?FXX4NH7"$ITQVEIOKB@S],TWW7(:T9H_/G4_ W

    MP*J\X6GC4+SXPU3^Q<O]$K5Q05S[6C>\_8U/I1C[(N3>'4^8FT1T'U_VH6

    MW7732#7??BD?51<75A1>GRFY:>8I0P44#I^?2$X'SVYU&."]E5Y7B2PJGS

    M$\DU1IHIFEPJBXN/!P4,I4H7-7YPFK"(0!JKJX8*PCC12>=5$X=7XBN=94

    M%05X"!7&!?W0D_AB0A1E]8VEV__U\1A2O$A8>.X>L2$*KT!>/.\Q4@5!D7

    M>JTH9"K4=7I"X\)0X)-DBE495P8-5(4(8YOX/(J_4%I7SW-9^ZQC3OIJDU

    MHS*1N'YW&P;UKZ@JC -?"Y]>?]F.:V+U[2C7'A4<N"BL(ZWVQ_?VZ NB

    M@B@\-0HCBVE'YK(A,S%6\2%8Q2&1G].V)7<8&$P0"EI$5D59[8L=%8^"

    MRH](4]&'16)3-OEAIA[N:+X@7RB#IX!0&,NB#MM]L>YVCA47^N>_

    M;.TY^BL,"G-9YAV9X[Y8KV)&\@49=I:M5X4I/"4*0XB>`_2R3]RF.'&A&2EL

    M_.0N%.:RS,EJ7ZPV1DWN"_L9\SC"10"LN.S"2SMFU<4'FLXT*3!T(\"L?^

    M_*))X37],$6G\-B#$,,7.IEU)@A0OJ#R[/7U]16P(S-"7!C\8!L7^I0;K"-9

    M[BGT]S;Z7ZWX_6@KDB\(W_Q;<(:@Y[Z>S^A"Y"7!@#M!07?"]]1DCS!6>B

    M`T847WA(W_R;^(H#*#C$42:,2("_IQL=\DDC[X6DK70:D>;.-_:%;9M[

    M09C5DWC-O_S:5> ZTEWBPGHG[#,,PJ"^#OLQ?!!]P:*GK( K:'78&U$Y[R_8

    MXD+UZTB]SD0ZF"C<<07ZE_-&W02@JL.:QH'XD.3@F!@KP?R5\>[33!.. +

    MEZ40KC,0`D:J_1S_6=T#=X4/;^PK/B?:IF1P7K"ZI%S#W;I;>+6'5\'4G]

    MH>'7RQT7(A73(3F3IT'AU/-4,^C\W%G]U;V7[ OG"N<E*9>Y@_Z2GZ>::R[C

    MJPCK2.K83\+8]'K-8:-47'CJ%*9_

    MF_EYJC.Y$7SUO&XH-]?&,=#XW$P]'[1_X'$J65Y* P/*7J>6#?:&Y%]P7C

    M@D5\01T#T]L"]\WFEL1XD*W]@?-7H"",7-2S\W;[AN]?(]T/Q$LE!0;\:_

    M&*OM&WDL\HJ0EQX2.GE?K]@S-.FO]NK0G4W?Q@+0GV\%Q1F%.'?:./>9M6

    MUC+N=9\89UN'E-I#"]FYGM2?IXH&H59?F-XM%&I_GNIFOF <8Q=XHT *

    MVN Z>=&\E6^8)D\))3@I%<RY,\_>8QC%^D5>Z'P5$.<=([E08G8T9$18=]H;B7VA0R5EVIP,0A)XT>VLLUN!#E+Z0J_Z6&EP)0KJX

    M,-3WW(4'OASM46I?"'?UQ!JB?J@$L4%Y0>DX*DTOI"S2[X?!<X,/E!X;AP

    M':7PA;S#DWM2V/6'Q0](P5,)?"'S?.E%'SB@N8'SW\CE=*EU'P4>XYZSTI

    M[/E#SO%1KWM2V%'VU9O[40A8/QHH%+J_<#DE](7#90K3[N[ :\BWNGYQ(>OX

    MJ%?IYHLDWK2%U+M[JA<>&1)R[<3"<#.%Q@5B2"'0^<-%Z.Q+@07Z#K

    M2#=3#H2,<07Z/V%F\GWOK-?X$48@OTOO/-Y+\?25M7)87(`MV/=#.%[%-E

    M7$BE@_M4K7^ B\HG4D 0*2"(%!!$"@@B!021`H)((9;:]OBYI!!+I( @4D 0

    M2"(%!!$"@@B!021`H)(`4&D@"!20! I((@4$$0""(%!)$"@D@!0:2 (%)

    M$"D@B!001 H(image]@((5(:ML3&$@ACMKV# 8("G\74KP:M,<TG8Y H10$4M 5

    MLSD9;MIUS"10AQ=/R[40.'Z8Z0J%Q^OE A>/GDD(LD0)"MJ2 D"TI(&1

    M"@C9D@)"MJ2 D"TI(&1"@C9D@)"MJ2 D"TI(&1"@C9D@)"MJ2 D"TI(&1+

    M"@C9D@)"MM 4WOL?@:'@45:[P"B\!VFO9X/EA((4]+(VEF)["HV"\>][;GUK

    MO4I2&%YMROI>4KT%26$XO.?#6$E1Q2FLRZJE@N>0F.7 N@J;Z&A?L8U(

    M(9LO-.@4-EUF-7$!?XRD7HXQ62]K36.D=6@0M4\A?"#O.4VQEC4\4S0*&P?8

    M&7.4I& K:WBN:!2,EP<I!$_]WI8S[/,OK4=:E;6BD>KX\F"/%#SU,T^80ZUC

    M_K6BH&5C]E.>@J70MO]-7\7WVUZOR8[A<W4;X"_G7>U:O*=2U@C%K'F+

    M9P>]EF6X:Y^ ;RELC7O9AH<?3: 4U"]_MO_H#%[<S<LU*1S\Q:A-?PGR

    M\EK\-3/G'MNAKQ#*D@?T5N@!W)%")G(D$(I[!:?O:@L!I56;IX"0((!4L=

    M#VB3E57VD:K>]#O#QU7P]W @V'MM,2GX_P38X0O:NST*F[>D,%[-"\(>!;^I

    MWZK-/4>J$85*P?<GP%X4/./"^HR=65M$P5+PU%Z/M'3XCJG?9OZE3<#\LSVA

    M&BF8"A_('YPLGA I'#J#% S![$<Z)5) R)84$(E!81L20$A6U) R)84$*]

    M,X4SIY*"+E(@A5@BA>S9"KHKA9-/:B8%0_0%4H@E4LB>K2!2R)ZMH#M3P,F6

    M%!"R)06$;$D!(5M20,B6%!"R)06$;$D!(5M20,B6%!"R)06$;$D!(5M20,B6

    M%!"RO3Z%0HI:"U(@!4J)%!!$"@@B!021`H)(`4&D@"!20! I((@4$$0*""(%

    M!)$"@D@!0:2 (%) $"D@B!001 H((@4$D0"2 %!I( @4D 02"(%!!$"@@B

    M!021`H)(`4&D@"!20! I((@4$$0*""(%!)$"@D@!0:2 (%) $"D@B!00%(\"

    ;54:D@#_`7 #6[7,PR\`````$E%3D2N0F""

    `

    end