Is uninstalling 5.10.0 necesary or can i overinstall 5.11 on 5.10 ?
what about the projects I already have ?
Is uninstalling 5.10.0 necesary or can i overinstall 5.11 on 5.10 ?
what about the projects I already have ?
Joern Paschedag schrieb:
Am 03.09.2011 12:42, schrieb bob:
>> Is uninstalling 5.10.0 necesary or can i overinstall 5.11 on 5.10 ?
>> what about the projects I already have ?
You can do that. Eagle asks you if you want to create backups.
I generally install into a new folder and adjust the paths of the
directories and my libraries . Then copy the current project to the new
version and continue work. If everything runs smooth I move all projects
over and uninstall the old eagle.
Generally I keep my backups up to date.
It is generally a good advice to strictly separate programs and data.
The libraries, projects etc. never belong in the path of the program
installation - even if that's the (unlucky) default after installation.
Move all your data to a complete different path, ideally at another
drive (I strongly second that suggestion made by Alfred Zaffran a few
days ago) or at least a separate root directory. Set the directory paths
in EAGLE accordingly.
After that, you can seamlessly update EAGLE any time, without moving or
correcting any data - regardless of using the same or another directory
for the program.
Tilmann
On 09/03/2011 06:42 AM, bob wrote:
Is uninstalling 5.10.0 necesary or can i overinstall 5.11 on 5.10 ?
what about the projects I already have ?
Not sure about an overwrite. I've never done it. I generally take
eagle's default of /opt/eagle-5.11-0 and change the symlink /opt/eagle
to point to it. That way if there's any problems with the new rev, all
I have to do is change the symlink back to what it was.
By using a symlink, I don't have to mess around with changing all the
paths on each workstation.
Enjoy,
- Chuck
Am 03.09.2011 12:42, schrieb bob:
Is uninstalling 5.10.0 necesary or can i overinstall 5.11 on 5.10 ?
what about the projects I already have ?
You can do that. Eagle asks you if you want to create backups.
I generally install into a new folder and adjust the paths of the
directories and my libraries . Then copy the current project to the new
version and continue work. If everything runs smooth I move all projects
over and uninstall the old eagle.
Generally I keep my backups up to date.
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag