EAGLE User Chat (English) Eagle Software
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
  • Replies 45 replies
  • Subscribers 184 subscribers
  • Views 4215 views
  • Users 0 members are here
  • eagle
  • software
Related

Eagle Software

Former Member
Former Member over 12 years ago

Greetings

 

My name is Brian, and I am a new user of Eagle, for right now the free version.

 

First question, is there any way to stop Eagle from carrying on point to point connections.   I am sure at times this is a very useful feature, but I need it to stop after automatically after it connects 2 points.   I hope this is possible, as if this is a persistent feature, it will really turn me off to Eagle.

 

But more importantly, I did a practice design and have a problem.

 

I am using a XF2H-3415 surface mount connector, .5 mm spacing.   I have a bit of a problem with the datasheet, as it doesn't clearly state the measurement units, but since the first page notes a measurement in mm, I'm assuming they are smart enough to carry those units throughout the datasheet.

 

Let me describe what I did, and perhaps did not do.

 

I have my board layout done, I have two 12 pin single row headers on each side of the board, and the other connector on the other side.   And I see the Ratsnest.

 

I think the pad color denotes side of board, but I'm not sure how to check or change that.

 

This is where the confusion starts.

 

I can't get the autorouter to start, and I come up with 34 DRC errors.

 

I'm a beginner, probably making a silly mistake, but Eagle also has a much more complicated set of DRC rules than I'm used to.

 

I have attached an image.

 

Help is most appreciated.

 

Thanks

 

Brian K

BKM Engineering

Attachments:
image
  • Sign in to reply
  • Cancel

Top Replies

  • AnalogNotes
    AnalogNotes over 12 years ago in reply to Former Member +2
    Brian Mcclung wrote: You don't have to act like you are the defenders of eagle. LOL, but this is the EAGLE forum - we *ARE* the defenders of EAGLE! * AnalogNotes dons his EAGLE cape and stands on the…
  • AnalogNotes
    AnalogNotes over 12 years ago in reply to Former Member +2
    In that case, I hope at least the first 3/4 of my messages were useful to you... Best of luck, sir!
  • mcb1
    mcb1 over 12 years ago in reply to AnalogNotes +2
    I'm always amazed by some people for whom the HELP section included in most software in unused. The same people expect others to guide them through a learning process, but then bite the hand that feeds…
  • dukepro
    dukepro over 12 years ago in reply to Former Member

    On 03/13/2014 08:26 PM, Brian Mcclung wrote:

    Hi Chuck

     

    I'm still having the same problem, but other questions first.

     

    How do you change the units.

    How do you define the grid in such a way that your measurement steps are

    smaller than the area to be measured.

    As Doug mentioned, you can use the grid command.  Try "grid mil 5" to

    set the snap to every 5 mils, or "grid mil 1" to set it to 1 mil.  You

    can go smaller or larger to suit your needs.  You can also append a

    second integer to this that affects the display of the grid.  Try "grid

    mil 1 5".  This will set your snap to 1 mil, and the grid display to

    every 5 snaps (5 mils).  "grid mil 5 5" will set the snap to 5 mils, and

    the display to 5 snaps (25 mils).

     

    You can also specify other units, such as mm or in.

    Back to my original problem.

     

    I checked the parameter I think you specified, and the size is already

    set to 10 mils.

     

    Well, that's the source of the DRC problems.  If the pads are on .5mm

    spacing, and each pad is .25mm wide, that leaves only .25mm of spacing.

    That converts to 9.8 mils.  Try setting the size to 9 mils.

     

    This also means that the wire coming off the pad must be less than 9.8

    mils - a 10 mil trace will create a DRC clearance error.

     

    What I want to know is if these errors are caused by a design rule, why

    is Eagle not self adjusting to what is a standard part.

    That would be making assumptions about the capabilities of the board fab

    house, and your design limitations.

    Why is Eagle not self adjusting, and is this going to be a persistent

    feature when using Eagle.  Is this something that every time I do a

    board, I am going to have to go in adjust my design rules?

    Basically, yes.  If you are using all PTH components, there's no need

    for such tight tolerances.  For SMD designs, obviously the fab

    requirements have small tolerances.  I'm sure you can change the default

    design rules for new designs, but I don't know where that would be done.

     

    HTH,

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • AnalogNotes
    AnalogNotes over 12 years ago in reply to Former Member

    What exactly are you trying to do with the dimensioning tool?  I've never thought of it as anything more than icing on the cake, just a way to put measurements on a page for a human to read...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to dukepro

    Here is where I'm having a problem with the design rules.

     

    This particular part that was giving me problems was obsolete 7 years ago.  It has been replaced with the M model, but the spacing is the same.   This particular obsolete part has been around 10 years.

     

    What legitimate board house could not handle that spacing.

     

    So let me retract my question, why are the DRC rules not self adjusting.   I could further debate the point, but I wont.

     

    I never changed the DRC rules.

     

    Now my question is this.

     

    Why would Eagle default to parameters that don't reflect current manufacturing capabilities.

     

    Is that spacing really beyond typical manufacturing capability?

     

    If it isn't, I was caused unnecessary trouble by the parameters it defaulted to.

     

    Thank you for your response.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to AnalogNotes

    Maybe to aid placement, a quick check of board or edge-part spacing.

     

    I just don't see how it can be used for a quick a-b measurement.

     

    It seems to pick its own points automatically, or at least one of them.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 12 years ago in reply to Former Member

    On 14/03/14 11:23, Brian Mcclung wrote:

    Yes Rob, I agree, how stupid of me.

     

    Why would I not expect Eagle to impose a limit on me based upon an

    action I have never performed: Adjusting the rules you carefully worked

    out to suit a component you picked on a whim.

     

    Do me a favor!

     

    Do yourself a favour and READ THE ADVICE YOU ARE GIVEN.

     

    We are not here to waste our time on your personal whinge-fest. If you

    want to know why things are as they are, and somebody answers that

    question, rejecting an answer you don't like with sarcasm is incredibly

    rude and obnoxious. Please grow up.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • AnalogNotes
    AnalogNotes over 12 years ago in reply to Former Member

    Brian Mcclung wrote:

    Maybe to aid placement, a quick check of board or edge-part spacing.

     

    I just don't see how it can be used for a quick a-b measurement.

     

    When I want to do a quick measurement, I just use the "mark" command.  When you place a mark, you get a display of relative coordinates right next to the cursor location display.  Read: MARK command You can use the "assign" command or the options-assign menu to tie the mark command to a particular key that you like.  For example:

     

    ASSIGN F12 'mark';

     

    If you want, you can even assign a key to stop marking:

     

    ASSIGN F11 'mark;';

     

    (Notice additional semicolon inside quotes.)

     

    It seems to pick its own points automatically, or at least one of them.

     

    If you read the help on dimension DIMENSION command you'll see that if you click on an object, EAGLE will try to guess what to do...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to autodeskguest

    I'm going to make this really simple for you.

     

    The next time anybody refers to anything I'm questioning, wanting to do, or thinking you should be allowed to do as catastrophically stupid, they will get an attitude from me.

     

    You don't have to act like you are the defenders of eagle.

     

    Everything about Eagle is not the greatest.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to AnalogNotes

    I may be kind of unique, but I would actually prefer a little less thinking for me.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 12 years ago in reply to autodeskguest

    I want to clarify.

     

    I have been reading the advice given.   I have not rejected anything.   I'm here to learn how to do things.

     

    And I have tried to thank everybody who has helped me.

     

    None of these 4 things requires me to like Eagle.

     

    And I don't have to justify anything I would like to do.

     

    Now that we have that straightened out, if you don't want to help, don't!!!!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • AnalogNotes
    AnalogNotes over 12 years ago in reply to Former Member

    Brian Mcclung wrote:

    You don't have to act like you are the defenders of eagle.

     

    LOL, but this is the EAGLE forum - we *ARE* the defenders of EAGLE!

     

     * AnalogNotes dons his EAGLE cape and stands on the roof, hands on hips, gazing into the distance with his hair and cape billowing behind him in the wind while patriotic music plays...

     

    Everything about Eagle is not the greatest.

     

    In some circles, that comment would be worthy of the title "troll"...

     

    Troll (Internet) - Wikipedia, the free encyclopedia

     

    Seriously though, what other EDA products have you used, why are they better than EAGLE, and why aren't you using them?

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
<>