Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) restricting inner layers
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 187 subscribers
  • Views 1532 views
  • Users 0 members are here
Related

restricting inner layers

autodeskguest
autodeskguest over 16 years ago

I have a 4 layer design with power and ground filling both internal layers

with no internal routing just vias.  I want to set up a restriction to

prevent the power plane filling an area.  How do I set up the internal

restriction?

 

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 16 years ago

    Tony wrote:

    I have a 4 layer design with power and ground filling both internal layers

    with no internal routing just vias.  I want to set up a restriction to

    prevent the power plane filling an area.  How do I set up the internal

    restriction?

     

    Besides using multiple polygons to cover the area (as Gary already

    suggested), have a look at the attached board file for an alternative.

     

    Also a closed wire frame will keep the polygon pour out of it's area.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 16 years ago

    On 5/26/2010 7:22 AM, Tony wrote:

    I have a 4 layer design with power and ground filling both internal

    layers with no internal routing just vias. I want to set up a

    restriction to prevent the power plane filling an area. How do I set up

    the internal restriction?

    if I understand your question correctly, you want some areas with no

    fill, open in other words, on your internal planes.

     

    if this is the case, use polygons on the inner layers to make the planes

    and simply don't draw them over the areas where you want it to be open.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 16 years ago

    On 5/26/2010 9:22 AM, Tony wrote:

    I have a 4 layer design with power and ground filling both internal

    layers with no internal routing just vias. I want to set up a

    restriction to prevent the power plane filling an area. How do I set up

    the internal restriction?

     

    Hi Tony,

     

    You might be better off just turning the inner layers into supply

    layers. Since you're not running any traces through those layers then

    you can use this option.

     

    Using the DISPLAY command select your inner layers and using the change

    button you can set them to supply layers. Remeber that these are

    negative layers so if you route any tracks on them they will be removed.

     

    If you don't want the autorouter to touch those layers you can turn them

    off on the autorouter setup the first tab. Where you see the layer

    preferred directions you can set the layer to N/A not available and the

    autorouter won't route to it.

     

    If you just want the vias placed and routed then you can use this little

    trick. First Disable your optimize runs, then set your via cost to zero,

    and finally type 9999 in the field that allows you to limit the number

    of vias per connection.

     

    When you run the autorouter EAGLE will automatically run vias near all

    ground and power pins.

     

    hth,

     

    Jorge Garcia

    Cadsoft Computer

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 16 years ago

    There is no direct way to do this.

    All restrictions works on top and bottom layers, only.

     

    I have a pcb antenna myself with same problem. I did make signals on all

    4 layers, and then made 2=polygon fill gnd and 15=polygon fill with vcc

     

    Christen