Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) >$1000 for a simple 8"x8" PCB???
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 12 replies
  • Subscribers 183 subscribers
  • Views 1457 views
  • Users 0 members are here
  • eagle
  • pcb
Related

>$1000 for a simple 8"x8" PCB???

Former Member
Former Member over 11 years ago

I want to make a simple PCB, so I'm looking at Eagle as it seems to be what other hobbiests use.

The board is 8" x 8", and will have only a few LEDs and chip resistors on it. I don't need multiple layers, libraries, autorouting, or even drilled holes. I could make the PCB by hand with a utility knife, but I thought using a PCB program would be neater and cause less hand stress. BUT it seems the Eagle program is more than $1000 to do this! Do other hobbiests really spend this? (I was hoping for free...)

My question: Is there another program out there cheaper, Eagle just seems unreasonably priced.

  • Sign in to reply
  • Cancel

Top Replies

  • Problemchild
    Problemchild over 11 years ago in reply to johnbeetem +1
    Indeed John 1 PCB is basically the same as 10 from a small run organisation which is only marginally less than 100 off. um PCBPOOL wants around £100 for a 1 off 2 layer 200mmx200mm i.e. 8" on side!
  • vsluiter
    vsluiter over 11 years ago +1
    Hi Steve, At work I'm using a design package that costs 1k anually for maintenance... It does however work very well, with very little frustration during routing. For private projects I used to work with…
  • rea5245
    rea5245 over 11 years ago +1
    Steve, I've assembled a list of free PCB CAD software. Since some of the packages are crippled versions of commercial software, I include details of what the limitations are. You can see the list at http…
  • autodeskguest
    0 autodeskguest over 11 years ago

    On 05/05/14 22:27, Steve Ins wrote:

    I want to make a simple PCB, so I'm looking at Eagle as it seems to be

    what other hobbiests use.

    The board is 8" x 8", and will have only a few LEDs and chip resistors

    on it. I don't need multiple layers, libraries, autorouting, or even

    drilled holes. I could make the PCB by hand with a utility knife, but I

    thought using a PCB program would be neater and cause less hand stress.

    BUT it seems the Eagle program is more than $1000 to do this! Do other

    hobbiests really spend this? (I was hoping for free...)

    My question: Is there another program out there cheaper, Eagle just

    seems unreasonably priced.

     

     

    Eagle is free if you want to design simple and small. If you want to

    design something really complex that justifies 8"x8" then the $1000

    price tag is actually quite reasonable. If you're merely hell-bent on

    wasting PCB space...

     

    Yes there are cheaper programs. There are free ones, both as in beer and

    as in speech. Some of them are even tolerably usable apparently.

     

    Of course, if you had the cunning to work around things instead of

    whingeing about the price of something that's worth every penny, then

    there are ways to achieve what you need for your trivial case without

    needing any expensive options, but since this is an Eagle discussion

    group hosted by CadSoft / Element14 then I'm most certainly not going to

    give you any clues there.

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • mcb1
    0 mcb1 over 11 years ago

    Steve

    You're correct that for a simple project the price is high.

     

    For your application there are several others available and PCB manufacturers accept output from these as well.

     

    Obviously Cad Soft Guest is a little biased but it doesn't translate in rudeness.

    Because it is a single board with a few parts on doesn't mean its trivial to the poster.

     

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago

    Hi Steve you have obviously exceeded the limitations of the Free Eagle (I never remember what they are).

    If I remember right it was something like 100x100mm which is 1/4 of the size you mention. Best idea would be to

    reduce the size of your board but not knowing how dense your board is it may not be practical even if it's not complicated.

    You could however try designing the board in 4 parts then stitching them together using some graphics  package presuming you are

    going to etch this board your self. Failing that you can look on the net Google is your friend here for Free PCB tools or look to see what

    folk are using on sites such as Hackaday or what ever.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • johnbeetem
    0 johnbeetem over 11 years ago

    There may be some suggestions that could work for you in this discussion: Software is too expensive!

     

    But first you might what to find out how much it costs to make an 8" x 8" PCB.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    If I had a Windows PC I would check out DesignSPark PCB

    or Kicad which runs on Windows, Linux and Apple OS X

     

    HTH

    Warren

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to johnbeetem

    Indeed John 1 PCB is basically the same as 10  from a small run organisation which is only marginally less than 100 off.

     

    um PCBPOOL wants around £100 for a 1 off 2 layer 200mmx200mm i.e. 8" on side!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • vsluiter
    0 vsluiter over 11 years ago

    Hi Steve,

     

    At work I'm using a design package that costs 1k anually for maintenance... It does however work very well, with very little frustration during routing.

    For private projects I used to work with Eagle, but as I got more and more fed up with the illogical way it is routing (no live DRC, no dynamic routing, no way to easily shift segments while keeping 45 degree angles) I recently migrated to KiCad. It has its quirks, and a very limited amount of DRC rules, but it works, and is more consistent in operation than Eagle if you ask me. Anyway, I don't want to start a tool-war, just saying that a free alternative exists!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Former Member
    0 Former Member over 11 years ago in reply to Problemchild

    I agree with John,

    Unless there is some demand of form over function; the area needed to perform "only a few LEDs and chip resistors" does not require 8"x8" space. Free Eagle is capable of up to ~100mm if i remember correctly.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    Hi Steve,

    If you have any new PCB project feel free to contact me,you can get good

    price wiht best quality.

     

    Waiting for your contact.

     

    Monster@shiyupcb.com (mailto:Monster@shiyupcb.com)

    Skype: monster.cheung

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/112527

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 11 years ago

    OK as a reference how much for a 200x200mm Double sided PCB with

    Resist/Silkscreen and I'm presuming HASL is the cheapest finish?!

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/112551

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>