Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Chat (English) Eagle and Laser cutter
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 18 replies
  • Answers 1 answer
  • Subscribers 190 subscribers
  • Views 4874 views
  • Users 0 members are here
  • eagle
  • pcb
  • laser
Related

Eagle and Laser cutter

e14 Contributor
e14 Contributor over 12 years ago

Has anyone here used a laser cutter in conjunction with eagle to make pcbs?

 

im using pcb-gcode to create the code to use with a milling machine (modding it to turn the laser on and off once it generates the code), then running it through EMC2 that controls our 40w cutter. I spray paint the side of the copper board I intend to use and vaporize the traces with the laser...

 

im just curious if anyone else has a similar workflow, the only real problem I'm having is spotting/marking the holes so enough copper gets etched away so my hand drilling is a bit more accurate (yes I could completely use a drill press but I don't have one image )

 

MAybe a modified method that results in bigger holes being marked?

 

 

 

thanks for reading!

  • Sign in to reply
  • Cancel
Parents
  • Problemchild
    0 Problemchild over 12 years ago

    You said here you are using the Toner transfer method I assume you haven't tried the laser yet then . If that is the Laser then I'm pretty impressed. I would also say stay with vector formats and avoid raster like the plague as although you have enough accuracy you do cannot switch off the beam fast enough for a clean edge as it takes several ms to stop lasing and just messes up the etch resist.

     

    Most of the laser software don't take GCode at least the Chinese variety if you can create a DXF then you can import that into almost all the Software. BTW eagle provided a load of tools to do this but I've not tried as it was windows only..

     

    Good luck ....Do you have a link to the pcb-gcode thing BTW?????

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 12 years ago in reply to Problemchild

    Previously I was using toner transfers to do PCBs. The images posted here are from my first attempt at lasered PCB's (which still need to be etched afterwards anyway image )

     

    The original place for the pcb-gcode plugin is pcbgcode.org, which is meant for milling the board using a mechanical cutter.

     

     

    My modified version can be found https://www.dropbox.com/s/jsx7z02rd623boq/pcb-gcode3.6.2.4-laser.zip  and should have a bunch of warnings attached to it but doesn't image

    (My cutter is setup to where that spindle on/off turns the laser on/off; the modified code turns the laser on when the Z is negative and off when the Z is positive)

    I would dry run any output from this first...

     

    Here's a board from the newer code, its not perfect but my hand drilled holes are a little better since I had better markers...

    image

     

     

    Perhaps later I can try putting the board back after etching and have the laser cut the holes since theres no copper protecting them now image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to e14 Contributor

    That's a good result then. I'm sure you can remove the resist at least as accurately as any hope process can remove the underlying copper so you are good there. The laser hole thing may well be a pain as you will need some lugs or some such on the bed to align the board again to get the correct registration. Another issue I find is that the FR4 has a tendency to char, maybe that wont be such an issue for just the holes and after all you will be soldering over them any way image

     

    Thanks for the links BTW!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to dragonstyne

    Obviously you need good insulation on the 20KV out put but other than that all you need to control it is either the PWM 5V or an analog 0-5 V control that goes on the pin of the PSU ...all very simple stuff!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dragonstyne
    0 dragonstyne over 11 years ago in reply to dragonstyne

    John, Do you have docs on what you have?

    I don't think we should hijack his blog, so if you could PM me we can go from there.

     

    Thanks John,

     

    -Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dragonstyne
    0 dragonstyne over 11 years ago in reply to Problemchild

    Sounds fun, I built a helium neon laser early on. It looked sharp when it fired.

    An X Y Drive shouldn't be too difficult.

    And no, I don't think 20KV would taste very good. image

     

    -Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to dragonstyne

    Most of the parts are available from EBAY. If you feel confident of making an X-Y mechanism with a head on it then you are a winner for the rest.

    Even the Laser part aint too bad as long as you don't stick your tongue on the 20KV line image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dragonstyne
    0 dragonstyne over 11 years ago in reply to Problemchild

    Thst sounds interesting.

     

    -Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 11 years ago in reply to dragonstyne

    Steve if you are interested we can do something with my spare one so that you can get the electronics then the mechanics sounded out with out too many dependencies !

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dragonstyne
    0 dragonstyne over 11 years ago in reply to Problemchild

    John, you can answer your own questions you just don't receive the points.

     

    Good luck truehbridx,  a laser cutter is one of projects I plan attacking later.

    By the way, nice Sinistar icon. I haven't seen that in a while.

     

    -Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Problemchild
    0 Problemchild over 12 years ago in reply to Problemchild

    O BTW I was watching Ian from Dangerous Prototypes and he did a laser PCB but his was rather chared around the edge and where the holes are so it's obviously possible...Just needs a bit of finessing image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • Problemchild
    0 Problemchild over 12 years ago in reply to Problemchild

    O BTW I was watching Ian from Dangerous Prototypes and he did a laser PCB but his was rather chared around the edge and where the holes are so it's obviously possible...Just needs a bit of finessing image