Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Chat (English) Help?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 19 replies
  • Subscribers 187 subscribers
  • Views 2357 views
  • Users 0 members are here
Related

Help?

autodeskguest
autodeskguest over 10 years ago

Hi, I am new to this program. I have tried everything and can't figure out

why nothing I do is working.

 

I need a simple adapter board. I watched videos and everything. I am trying

to simply make a small board that has 42 holes for a m27c160 eprom to fit a

36 hole board.

 

I have went here http://schematicpal.com/ and downloaded the eprom

M27C801-100B1 it shows two boxes the left red box and the right green

circles in the black box. I can only place the red box in the schematic

when I need the other one to just place the holes for me. When I click on

circles they are not circles but pads, I need holes!

 

Plus the eprom clearly has 42 legs yet the only Library file you can place

in is missing majority of pins. This blows my mind it's not even accurate?

You go to the board view and magically it shows the entire chip but

completely useless as it will not let you run traces, that has to be done

in the schematic where they don't exist!!!

 

I have tried drawing circles "holes" manually but when I switch to board

view it does not bring them in? I tried grouping the 42 circles together as

that is what I need for the 27c160 eprom but it does nothing.

 

I can't believe how difficult this is. I want to order these boards but I

need a gerber file. I could whip this thing out in paint in like 10

minutes, here I have wasted countless hours trying to decipher this program

that will not do anything I want it to.

 

I think learning a new language would be easier them deciphering this

program.

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    Well it has pads on both sides. I used a "header pin" layout remember.

    Trust me I barely understand what I did. I just dropped the library file

    and sent it out. I actually got some boards in today. I only ordered 10 to

    make sure they will work.

     

    I need the 1/4" hole as the case it goes into has a 3/16" peg that pushes

    against the main pcb that this will be sitting atop of.

     

    The only thing I did not do that I have heard mixed feelings about is

    ground the unused pins. I guess I could do that before I order the bulk of

    the load, but I made a test board and ran like 35 wires by hand and just

    bent up the pins to nothing and it works fine, that was months ago I did

    that and it still works fine?

     

    http://s14.photobucket.com/user/icemanxp300/media/100_1030_zps9sraditr.jpg.html

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    Quote:

    M27C801-100B1

     

    Except for the mounting hole, you need PADS not holes. A pad is a hole with

    copper around it. You cannot connect copper traces to holes. You can only

    connect traces to pads. According the the drill symbols, your mounting hole

    is actually the same diameter as the drill for the pads. To make it 1/4",

    click on "i", then click on the hole. In the dialog box you can edit the

    drill size of the hole. BTW, 1/4" is HUGE. You will then have to re-route

    your board. First, you need to rip-up the traces. Type "RIP *" (without the

    quotes) into the command line. Then route the board.

    I see that there are several pins that aren't connected to anything. All

    CMOS inputs *MUST* be connected to either +V via a resistor (i.e. 10K) or

    directly to ground. CMOS inputs will act erratically (bounce between '0'

    and '1') if left floating (unconnected), and your board will act

    erratically, too. Floating inputs also draw more power. You may be able to

    get away with leaving them float, but then you will have failures in the

    field.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    I sure do hope this is correct. I just ran connections all in schematic. I

    went into net classes and made width .5mm, drill 1mm, and clearance .5mm I

    then ran auto router and this is end result?

     

    I have that hole on bottom that is suppose to be 1/4" but it doesn't look

    like a 1/4" hole in the green pic. I had only shown layers, pads, holes,

    drills, and vias.

     

     

    http://s14.photobucket.com/user/icemanxp300/media/Finished%20board%20%20segments_zpsc3hbnbnn.jpg.html

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    I finally got a wire to show I want a cookie! I can not believe this

    program is sooooo anal that it required my net wire to attach to the very

    end of the pin lead it shows in schematic view, unbelievable. Further more

    unless you have the grid size adjusted small enough you can never place the

    wire on the exact end spot that it needs.

     

    This is absolutely a horrific experience and very poor programming. I took

    some programming courses a bit awhile ago and every time I go to a webpage

    and it ask to input data such as a birthdate and I have to manually click

    each box, that is the same principle here. All it takes is a simple line of

    code so when you enter your data in box a it automatically goes to box b

    for you.

     

    This program is very picky and not user friendly one bit!

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    Thanks lol. At this point it has zero to do with $$, and is more so

    principal now. I generally don't have too many problems learning stuff and

    I can pick stuff up pretty quick, not this. I even took cad in high

    school.

     

    It is driving me nuts. I watched the tutorial on youtube from Jeremy Blum.

    That helped like crazy, however For the life of me I can't figure out how

    to draw a simple freaking trace from a to b!

     

    The header pin I upload has 7 spots for holes but in schematic view it is

    one entire structure, you can't define the individual holes or I don't know

    how. I can run wires, net wires, buses, and all in schematic but once I go

    to board view not a single one transfers with the components like he did in

    the video.

     

    Once in board view it will not let me run any wires as it says that needs

    to be done in schematic, seriously I want to punch the person who wrote

    this damn thing! You can do this but nothing happens and if you don't do

    that you can't do it later.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    On 27/09/2015 18:21, Greg wrote:

     

    Yes this program sucks! Must have to buy the real version in order for it

    to be a useful program. It's kind of like this website. Their is NO edit

    available anywhere, so you have to make a new post every time.

     

    Wow I will never ever recommend this program to anyone it is completely

    useless.

     

    I truly sympathize with you because I've been where you are not long

    ago. I still struggle, but not as much because after a lot of

    frustrations and learning I finally have a general overview and grasp of

    how it all works. That makes it easier to learn more.

    Eagle is (even the free version, which I use as well), like most other

    professional and specialized tools, an advanced application which isn't

    self-explanetory like a web browser, word processor or email program or

    whatever but takes a lot of time and effort to learn.

     

    I suggest you either hang in there to get an overview and understanding

    of the software by reading web tutorials, tutorial videos on Youtube

    etc. and of course practising yourself, but if you only need to have a

    single PCB done I agree with what others have said: pay someone to get

    the job done, because for that alone I would say the learning curve

    isn't worth it.

     

    L.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to shabaz

    Yes I am going to have to pay someone. Maybe pads was the wrong term to

    use. I am simply talking about the round rings on ever through hole.

     

    All I want is 42 holes cut w/the copper rings around them that connect to

    traces that will run to the other 36 holes w/rings around those.

     

    It will be very similar to this board. It will only have 1 eprom connected

    instead of 2 like this board has. The board will be shaped a bit different

    as well. This is however what I need, just different chip and size. But

    that is the boards I will be connecting these to.

     

    http://s14.photobucket.com/user/icemanxp300/media/adapter_zpsrn66oleo.jpg.html

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 10 years ago in reply to autodeskguest

    Hi Greg,

     

    You could pay someone to do this for you if you're not prepared to do it yourself, or you may be

    better off with alternative software - I don't know what though, because no-one works in this manner

    any more. Adding pads individually went out with the sticky-backed-crepe-paper-on-transparency-film

    methods of the 1970's.

    Somebody (e.g. a student) would probably do it for you in EAGLE for a few hundred dollars - it is probably just an

    evenings work including the time to discuss it.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    Well after watching more videos of this program it appears what I need is

    to "define an electrical connection". Well that option is NOT available in

    my version, it is no where to be found.

     

    Yes this program sucks! Must have to buy the real version in order for it

    to be a useful program. It's kind of like this website. Their is NO edit

    available anywhere, so you have to make a new post every time.

     

    Wow I will never ever recommend this program to anyone it is completely

    useless.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to autodeskguest

    This is a waste of my time. I don't think I even did it right last night. I

    need pads around the circles. There is no option to add a pad. This is just

    unreal.

     

    I added (6) 7 pin headers and 6(6) 6 pin header and those have pads, except

    when you draw a wire from them on the schematic view the wires don't show

    in the board layout.

     

    I seriously feel like an idiot. I am way better off waiting for someone to

    respond and do this for me.

     

    You say this program is easy, well it does not seem easy to me. I can't

    even get a trace ran.

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>