Hi Guys
I'm totally new to this. I'm trying to build a 4 channel opamp (boost my signal about 100x)
I'm hoping someone has the time to quickly check my design and see if it makes sense and perhaps let me know how to improve it.
Thanks
Jacob
Hi Guys
I'm totally new to this. I'm trying to build a 4 channel opamp (boost my signal about 100x)
I'm hoping someone has the time to quickly check my design and see if it makes sense and perhaps let me know how to improve it.
Thanks
Jacob
| opamp.zip |
Am 07.10.2015 um 14:02 schrieb Jacob Thastrup:
Hi Guys
I'm totally new to this. I'm trying to build a 4 channel opamp (boost my
signal about 100x)
I'm hoping someone has the time to quickly check my design and see if it
makes sense and perhaps let me know how to improve it.
Thanks
Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162669
Attachments:
opamp.zip
No capacitors?
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
You mean to filter the input?
Hi,
At least capacitors should be added on the supply...
I don"t know the purpose of your circuit but you should add at least a small one capacitor (10 to 100 nF) placed near the power supply input pins of the LM324, and a electrolytic caacitor (few µF) rignt after the supply input connector.
En large 24V supply trace, and for the GND you can enlarge the trace or better add a GND plane (polygon).
Guillaume
Hi,
The sensor cell will produce a voltage, between the 2 signals :
- the signal you will connect to your amplifier input
- and the GND.
Only the voltage between these 2 signals (the difference) is important. The current that will flow out from your cell into the input of the amplifier is exactly the same than the current flowing from the GND of your board into the GND pin of your cell.
So, the role played by the 2 wires of the oxygen cell (signal and GND) is equivalent, and there is no reason to have a different path (except if GND is also used to supply the sensor see (*) ).
On the amplifier side : it amplifies the difference between the input signal and the GND plane, the GND plane is a REFERENCE.
If instead of connecting directly the GND of sensor to your board, you connect it to a point away from the plane (name it STAR point), with all the other sensor GND and supply GND, then you connect this start point to your board with a single wire. On the paper this will work.... but....
In this last GND segment (wire from the GND plane and star point) you will have the sum of all the currents of all sensors, plus the current drained by the amplifier it self (and this last one is far more important than the others).
Where is the problem ?
The problem is that the copper is a good conductor, but not an ideal one !
You will have a little voltage difference between your GND plane and the start point, that will be dependent of that current, and the length of the wire, and so amplifier REFERENCE will not be exactly the reference of the sensor.
In other word, each signal will be polluted with the signal of the other cell and the consumption of the amplifier...
There is also other advantages of using same path for your sensor: you can use twisted pair wire, that way you reduce noise, specially if your sensor are far away from the borad.
Just one thing (*) : I don't know your sensor: is this sensor need a supply ? How this supply is wired? is the GND of sensor is only a output reference or also used for the return path of the supply ? because in that case you have to figure how best can the GND be wired.... there is no magic solution, and we can help you unless you give us more info...
Sorry with this very quick fast ultra simplified explanation... and if you want to have more fun... you can also question yourself about the output of your amplifier : How the GND path mcan be optimised and wired, on the output side (I suppose you will connect it to an acquisition device...)
Guillaume
Guillaume barrey[1
wrote on Sat, 10 October 2015 05:53]Hi,
That last design is better, the ground plane is OK.. You remove the
big
capacitor (your 5µF) I suggested to check the value and the
package,
but not t remove it ? If it was one of my design I would put a 10µF
electrolytic capacitor between GND and +24V, just right after the
supply
connector...
Nice work ....
Ah ok hehe, I've added the 10uF capasitor now.
Quote:
I think there should be a ground connection for each channel. In other
words, you will need 3-pin instead of 2-pin connectors. Otherwise your
only ground connection is through the power supply connector. The ground
pin should be between each input and output pin.
I'm not sure I understand this bit.
The signal I'm trying to amplify is coming from small oxygen cells
(galvanic cells). If I understand what you are suggesting, is that I use
the GND from each cell to connect to their respective inverting input of
the opamp? My original idea was to tie all the GND lines from the cells
into the same GND connector (the one I also connect the power supply to).
Potentially a stupid question.. will that work? I don't need to ground
everything "together"?
Quote:
If you swap the ends of R5 and R6, then you can have a single trace for
OUT3, instead of 2 traces. You can do the same thing for the other
channels.
Once again thanks for all the help!!
-Jacob
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
| test5-3.zip |
Jacob Thastrup wrote on Fri, 09 October 2015 12:34
Once again thank you guys!!
Guillaume, thank you for the explanation it really helps!
I've added a ground plane to Joern's design... does that make sense?
I hope you can see the attached file..otherwise I'll go register at
eaglecentral as well.
-Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162904
Attachments:
test5.zip
I think there should be a ground connection for each channel. In other
words, you will need 3-pin instead of 2-pin connectors. Otherwise your only
ground connection is through the power supply connector. The ground pin
should be between each input and output pin. I agree with others that you
should have a cap across the power supply terminals. Also, on your layout,
if you switch to a finer grid (i.e. 10 mil aka(0.01")), you can move some
traces slightly and improve the ground plane near the left end of the chip
(also changing the polygon width to 12 mils helps). If you swap the ends of
R5 and R6, then you can have a single trace for OUT3, instead of 2 traces.
You can do the same thing for the other channels.
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
Am 09.10.2015 um 18:34 schrieb Jacob Thastrup:
Once again thank you guys!!
Guillaume, thank you for the explanation it really helps!
I've added a ground plane to Joern's design... does that make sense?
I hope you can see the attached file..otherwise I'll go register at
eaglecentral as well.
-Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162904
Attachments:
test5.zip
You should go there anyway. It is just the better link to the cadsoft
They don't have trouble with attachments (as you have seen).
BTW my "design" was just a suggestion.
Maybe you should add an electrolytic capacitor in general and foresee
some holes to screw this print somewhere.
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
Hi,
That last design is better, the ground plane is OK.. You remove the big capacitor (your 5µF) I suggested to check the value and the package, but not t remove it ? If it was one of my design I would put a 10µF electrolytic capacitor between GND and +24V, just right after the supply connector...
Nice work ....
Once again thank you guys!!
Guillaume, thank you for the explanation it really helps!
I've added a ground plane to Joern's design... does that make sense?
I hope you can see the attached file..otherwise I'll go register at eaglecentral as well.
-Jacob
| test5.zip |
On 09.10.2015 11:12, Joern Paschedag wrote:
Am 09.10.2015 um 10:42 schrieb Joern Paschedag:
Am 08.10.2015 um 17:38 schrieb Jacob Thastrup:
Hi Joern
Maybe I'm getting it wrong. But I don't see any files from you?
Thanks
-Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162826
I attached it but I suppose it is the glorious interconnection between
the newsgroup and element 14 that never works since years...
Next try now...
No, sorry it didn't go throu, maybe because I'm not registered at
element14 .
And I'm not interested to register there.
You can find them here
http://www.eaglecentral.ca/forums/index.php/t/51848/5abd43c14367c14cffef482390e897d4/
Am 09.10.2015 um 10:42 schrieb Joern Paschedag:
Am 08.10.2015 um 17:38 schrieb Jacob Thastrup:
Hi Joern
Maybe I'm getting it wrong. But I don't see any files from you?
Thanks
-Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162826
I attached it but I suppose it is the glorious interconnection between
the newsgroup and element 14 that never works since years...
Next try now...
No, sorry it didn't go throu, maybe because I'm not registered at
element14 .
And I'm not interested to register there.
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
Am 08.10.2015 um 17:38 schrieb Jacob Thastrup:
Hi Joern
Maybe I'm getting it wrong. But I don't see any files from you?
Thanks
-Jacob
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/162826
I attached it but I suppose it is the glorious interconnection between
the newsgroup and element 14 that never works since years...
Next try now...
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
Hmmm not sure i got the capcitors right. ;-)
Partially...
For the 5µF capacitor: it's connected correctly in schematic, but I'm not sure you will found a value of 5µF, but a value of 4,7µF, 10µF, 22µF, 47µF... are standardized values . Did you check if you use the good package ? often this king of capacitor have a cylinder shape, and it polarized (+ shoufd be connected to +24V, and - to GND)
A good advice would be to found a capacitor (buy it or at least found were you will buy it), so you be sure of the value, the dimensions, the shape, if it's polarized or not....
The physical position on the board doesn't really mater for that capacitor.
For the 2 others, It's NOT OK: you need only one capacitor, and it should be in parallel not in series with LM324 :
-> in schematic : you connect the +V pin (pad number 4) of the LM324 directly to +24V, and do the same with the GND pin (pad number 11), connect directly to GND. Then you add your 100nF capacitor and connect one pin to +24V, the other one to GND
-> in board, you place physically this capacitor near the LM324, the nearest is the best.
The role of these capacitor is :
- filter noise coming from your supply.
- provide a local reserve of energy for you amp : when the amp will need to swing is output, it will sink current, and will need fast, and if there is no capacitor around, the current will flow from your supply through your cable and the copper of your board. With ideal wire no problem. but in real life, they have a little resistance and inductance: both will slow down current flow, and the voltage of the supply near the LM324 will goes down....
That why a good practice is to add :
- 1 huge capacitor (10µ - 100µF) for the board: it's provide energy for 'slow' consumption raises, and filter low frequency noise from the power supply...
- 1 little capacitor for each integrated circuit (chip), near the chip, for fast consumption variations, and filter for higher frequency noise...
This is only a very very simplified explanation and complex design need more than this little cook book, but in you case that could be a good start !
That also why you need to have larger wire for supply than for the other signal.
Guillaume.
Hmmm not sure i got the capcitors right. ;-)
Partially...
For the 5µF capacitor: it's connected correctly in schematic, but I'm not sure you will found a value of 5µF, but a value of 4,7µF, 10µF, 22µF, 47µF... are standardized values . Did you check if you use the good package ? often this king of capacitor have a cylinder shape, and it polarized (+ shoufd be connected to +24V, and - to GND)
A good advice would be to found a capacitor (buy it or at least found were you will buy it), so you be sure of the value, the dimensions, the shape, if it's polarized or not....
The physical position on the board doesn't really mater for that capacitor.
For the 2 others, It's NOT OK: you need only one capacitor, and it should be in parallel not in series with LM324 :
-> in schematic : you connect the +V pin (pad number 4) of the LM324 directly to +24V, and do the same with the GND pin (pad number 11), connect directly to GND. Then you add your 100nF capacitor and connect one pin to +24V, the other one to GND
-> in board, you place physically this capacitor near the LM324, the nearest is the best.
The role of these capacitor is :
- filter noise coming from your supply.
- provide a local reserve of energy for you amp : when the amp will need to swing is output, it will sink current, and will need fast, and if there is no capacitor around, the current will flow from your supply through your cable and the copper of your board. With ideal wire no problem. but in real life, they have a little resistance and inductance: both will slow down current flow, and the voltage of the supply near the LM324 will goes down....
That why a good practice is to add :
- 1 huge capacitor (10µ - 100µF) for the board: it's provide energy for 'slow' consumption raises, and filter low frequency noise from the power supply...
- 1 little capacitor for each integrated circuit (chip), near the chip, for fast consumption variations, and filter for higher frequency noise...
This is only a very very simplified explanation and complex design need more than this little cook book, but in you case that could be a good start !
That also why you need to have larger wire for supply than for the other signal.
Guillaume.