EAGLE User Chat (English) Eagle v8 licensing...
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
  • Replies 415 replies
  • Subscribers 217 subscribers
  • Views 31697 views
  • Users 0 members are here
  • eagle
  • license
  • freeware
  • 8.0
Related

Eagle v8 licensing...

technolomaniac
technolomaniac over 9 years ago

Hi All --

 

Moving this to a separate thread so it doesn't get lost in the ether.  Here's my two cents on licensing and I'd love your feedback:

 

Firstly, the Autodesk licensing model is subscription and the EAGLE paid license will require that you install the SW and then generate an account to retrieve your license entitlement.  Once you have this, you are good to go and the SW will run as expected.  If you lose your network connection, the SW has a 14-day heartbeat that will enable you to work offline for 14 days.  I know that some folks would prefer to never have to connect, but this is required to support a monthly subscription model that can be selectively enabled and disabled when you use the SW (so you only pay when you use it).  The total cost of ownership for those folks using it less than a few weeks a year will thus be substantially lower and still enables you to access the full software for less money.  <Insert revolt here>  image

 

WRT to "what happens if autodesk decides to one day just shut off the license server?" ...ok, sure, that's possible, but so is a reality TV star becoming President of the..cough...nevermind, bad example.

 

Point is, that's a pretty remote possibility (think: time travel and alien invasions) and it wouldn't benefit us *at all* to upset the users we just spent real money hoping to bring into autodesk and earn their business.  As the guy with both development and P&L for the product, I can tell you that it's counterintuitive and wouldn't benefit us at all.  We know this.  We make SW used by governments, movie studios, game developers, MEs, Civil Engineers, machinists, etc. and you can bet that shutting down a license server is not to our benefit in any of these categories.  To demonstrate this behavior in one category, without a path for user SW and data, calls into question ALL of our tools' viability under this model.  Not helpful.

 

Now...a question was raised about "but what if I drop my subscription and I want my data".  Awesome, the data is yours and lives on your machine.  And for SW that stores data in the cloud (we have some of these) we always provide a path to your data.  If this again fails with one product, it puts all of the others up for discussion.  Again, not helpful.  (Read:  strategy = doomed).

 

"So what about needing an entitlement for the freeware to open the data I created in another version (a *paid* version) and reading it?  What if I want access and I dont want the 14-day time out?"

 

So here's the deal...We can do better here.  So we will.  Here's my commitment to the group here for freeware that ensures you always have a license that you can fall back on without need of internet connection *except when you first install it* (which after all, you would have had to get it in the first place):  in version 8.1 or 8.0.1 or whathaveyou (let's call it 'a future release'), if you install the SW and authenticate once, we'll remove the timer req.  So what I'm saying another way is, the freeware will require you to login the first time to get your license, but if you log out beyond that, you're good.  You got your entitlement and you can use it freely without connection.

 

Caveat:  to install an update, you will need to login.  The update server (which issues the new version...e.g. 8.1 or 8.2. or 8.0.1, etc.) requires that you login and get the update, but beyond that, logout.  Thus if you want to go off-grid in a mountain cabin somewhere, get your license at Starbucks (blagh! I understand they have 'free' wifi, but no frappucinos!  ...that stuff is bad for you) then get your license and go on your merry way up to the snow drenched peaks.  When you hear from the other mountaineers or your local yodeler that a new version of EAGLE is available...download, login, get your license, get your 'decaf double-pump vanilla non-fat latte macchiato' and head back up the slopes.

 

Point being, we can do the freeware better.  So we will.

 

Hope this is clear.  Let us know if you have questions!

 

Best regards,

 

Matt Berggren

Director - Autodesk

@technolomaniac

hackaday.io/matt

  • Sign in to reply
  • Cancel

Top Replies

  • COMPACT
    COMPACT over 8 years ago in reply to autodeskguest +4
    Not to worry, it's back to the Drawing board for me.
  • shabaz
    shabaz over 9 years ago +3
    Hi Matt, When will the EAGLE Maker version (or another solution for hobbiests) be v8-ready? I see the subscription for 'EAGLE Standard' and 'EAGLE Premium' are now available on the website, but not EAGLE…
  • albertovignati
    albertovignati over 8 years ago in reply to techsupport +3
    Il 21/02/2017 22:54, Ed Robledo ha scritto: The customers are the sole driving force to the improvements to EAGLE. Some of these 'wants' take time to be done right, that's the reason they were not done…
Parents
  • dukepro
    dukepro over 9 years ago

    On 01/18/2017 02:26 PM, Matt Berggren wrote:

    Hi All --

     

    Moving this to a separate thread so it doesn't get lost in the ether.  Here's my two cents on licensing and I'd love your feedback:

     

    Firstly, the Autodesk licensing model is subscription and the EAGLE paid license will require that you install the SW and then generate an account to retrieve your license entitlement.  Once you have this, you are good to go and the SW will run as expected.  If you lose your network connection, the SW has a 14-day heartbeat that will enable you to work offline for 14 days.  I know that some folks would prefer to never have to connect, but this is required to support a monthly subscription model that can be selectively enabled and disabled when you use the SW (so you only pay when you use it).  The total cost of ownership for those folks using it less than a few weeks a year will thus be substantially lower and still enables you to access the full software for less money.  <Insert revolt here>  image

     

    I can see that you're pretty much laughing off our concerns.

     

    The only example you could present where this subscription based license

    will save the customer money is for a part time Eagle user.  Look at it

    this way...  In the last 4-1/2 years, I spent about $1000 to upgrade a

    3-user Professional license from v5 to v6, and to v7.

     

    Based on the current pricing of $500 per user per year, the equivalent

    3-user Ultimate license will now cost $6,750 for 4-1/2 years.

     

    Matt, help me to understand how the total cost of ownership is now lower

    than what it was?

     

    WRT to "what happens if autodesk decides to one day just shut off the license server?" ...ok, sure, that's possible, but so is a reality TV star becoming President of the..cough...nevermind, bad example. 

     

    Point it, that's a pretty remote possibility (think: time travel and alien invasions) and it wouldn't benefit us at all to upset the users we just spent real money hoping to bring into autodesk and earn their business.

     

    Again, I fail to see the humor.  It's not so much about shutting down a

    license server - it's more about the ability to access it.  Several

    customers, including myself, have already expressed concerns about

    this.  A scenario that is far more likely to occur would be one that is

    out of Autodesk's control - something like a virus that renders getting

    packets to and from Autodesk impossible.

     

      As the guy with both development and P&L for the product, I can tell you that it's counterintuitive and wouldn't benefit us at all.  We know this.  We make SW used by governments, movie studios, game developers, MEs, Civil Engineers, machinists, etc. and you can bet that shutting down a license server is not to our benefit in any of these categories.

     

    Yes, and you now make software that can not be used in a secure or

    remote environment.  Yeah... I also read about Global Travel Rights.

     

    Now...a question was raised about "but what if I drop my subscription and I want my data".  Awesome, the data is yours and lives on your machine.  And for SW that stores data in the cloud (we have some of these) we always provide a path to your data.  If this again fails with one product, it puts all of the others up for discussion.  Again, not helpful.  (Read:  strategy = doomed).

     

    Is it safe to assume that when you say that the license server and data

    in the cloud will always be available, it means that your servers are

    fully secured and unhackable and will never go down.  We're more likely

    to face an alien invasion than to have such servers.

     

    "So what about needing an entitlement for the freeware to open the data I created in another version (a paid version) and reading it?  What if I want access and I dont want the 14-day time out?"

     

    So here's the deal...We can do better here.  So we will.  Here's my commitment to the group here for freeware that ensures you always have a license that you can fall back on without need of internet connection except when you first install it (which after all, you would have had to get it in the first place):  *in version 8.1 or 8.0.1 or whathaveyou (let's call it 'a future release'), if you install the SW and authenticate once, we'll remove the timer req. * So what I'm saying another way is, the freeware will require you to login the first time to get your license, but if you log out beyond that, you're good.  You got your entitlement and you can use it freely without connection. 

     

    If you can remove the timer requirement for the freeware, then you can

    also set the timer to a period longer than 14 days, per Rachel's suggestion.

     

    Hope this is clear.  Let us know if you have questions!

     

    I sincerely hope that Autodesk will lend a serious ear to and address

    the concerns expressed about subscription based licensing.

     

    However, I truly believe that this is a lost cause considering that

    Autodesk's business model is subscription based.

     

    Thanks for your help,

        - Chuck

     

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • danteo
    danteo over 9 years ago in reply to dukepro

    I can see all those new licensing modes for new product. But it's not this case.

     

    The new Eagle is forked from the old Eagle.

    The old Eagle had licensed users.

    The new Eagle wants old Eagle's user pool to pay "again"?

     

    Or am I misunderstanding the whole thing?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to danteo

    On 19.01.2017 16:32, Dan Teodorescu wrote:

     

    The new Eagle wants that old Eagle's user pool to pay "again"?

     

    No they want a constant cash flow. "Pay" would imply you own the

    software afterwards, they want to rent it to you.

     

     

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
  • technolomaniac
    technolomaniac over 9 years ago in reply to autodeskguest

    No they want a constant cash flow. "Pay" would imply you own the

    software afterwards, they want to rent it to you.

     

    The major difference being that if you dont like what we release in a subsequent point-release (8.1, 8.2, 8.3...) you have not paid for everything up front, hoping one day they add better routing or better hierarchy, or better connectivity tools or design rules, etc. and then beeb disappointed that you "bet" it would come in version x.y only to find that it didnt.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to technolomaniac

    Matt Berggren schrieb:

    No they want a constant cash flow. "Pay" would imply you own the

    software afterwards, they want to rent it to you.

     

    The major difference being that if you dont like what we release in a

    subsequent point-release (8.1, 8.2, 8.3...) you have not paid for

    everything up front, hoping one day they add better routing or better

    hierarchy, or better connectivity tools or design rules, etc. and

    then beeb disappointed that you "bet" it would come in version x.y

    only to find that it didnt.

     

     

    Now you are completely inverting the facts.

     

    With a paid license, you get exactly what you pay for. You might even

    check out the freeware before to see if any new functions or changes

    justify the expenses. If you want to further use the old version

    (without additional cost, BTW), you simply don't update.

     

    With a subscription, you continuously pay even without any update (if

    it's really possible to avoid updates without losing the activation).

    Then you are disappointed!

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • autodeskguest
    autodeskguest over 9 years ago in reply to technolomaniac

    Matt Berggren schrieb:

    No they want a constant cash flow. "Pay" would imply you own the

    software afterwards, they want to rent it to you.

     

    The major difference being that if you dont like what we release in a

    subsequent point-release (8.1, 8.2, 8.3...) you have not paid for

    everything up front, hoping one day they add better routing or better

    hierarchy, or better connectivity tools or design rules, etc. and

    then beeb disappointed that you "bet" it would come in version x.y

    only to find that it didnt.

     

     

    Now you are completely inverting the facts.

     

    With a paid license, you get exactly what you pay for. You might even

    check out the freeware before to see if any new functions or changes

    justify the expenses. If you want to further use the old version

    (without additional cost, BTW), you simply don't update.

     

    With a subscription, you continuously pay even without any update (if

    it's really possible to avoid updates without losing the activation).

    Then you are disappointed!

     

    Tilmann