EAGLE User Support (English) Eagle- How do I put a hole in my PCB?
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
  • Replies 24 replies
  • Subscribers 182 subscribers
  • Views 9022 views
  • Users 0 members are here
Related

Eagle- How do I put a hole in my PCB?

stevemann
stevemann over 6 years ago

This is likely a silly question, but I am asking anyone with more Eagle PCB experience than I, which would be just about anyone, how do I put a hole for a 4-40 screw into my PCB?

I tried placing a hole using the command HOLE 0.125 *

But the PCB manufacturer bounced the order because the holes were only 0.003mm.

 

  • Sign in to reply
  • Cancel

Top Replies

  • dukepro
    dukepro over 6 years ago +2
    On 1/10/20 01:10, Stephen Mann wrote: This is likely a silly question, but I am asking anyone with more Eagle PCB experience than I, which would be just about anyone, how do I put a hole for a 4-40 screw…
  • autodeskguest
    autodeskguest over 6 years ago in reply to autodeskguest +1
    On 10/01/2020 07:30, Joern Paschedag wrote: This is likely a silly question, but I am asking anyone with more Eagle PCB experience than I, which would be just about anyone, how do I put a hole for a 4…
  • dukepro
    dukepro over 6 years ago in reply to autodeskguest +1
    On 1/14/20 04:34, Joern Paschedag wrote: Hi Chuck, IMHO the Standard is mm nowerdays. IC manufactories using it and even NASA. I could have checked or calculate it, but was 1. too lazy and 2. wanted to…
  • dukepro
    dukepro over 6 years ago in reply to autodeskguest

    On 1/13/20 14:53, Rob Pearce wrote:

    On 13/01/2020 18:11, Chuck Huber wrote:

    A #4-40 screw requires a 0.0820" (about 2mm) drill bit.

     

    <OT>

    Is that for tapping? I thought they were roughly 3mm for clearance.

     

     

    Yes, sir.  That's for a 75% thread depth.

     

        - Chuck

     

    Attachments:
    30557.att1.html.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • stevemann
    stevemann over 6 years ago in reply to autodeskguest

    Thanks, Lorenz.  I'll try hole 0.125 in on my next board.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 6 years ago in reply to autodeskguest

    On 1/14/20 04:34, Joern Paschedag wrote:

     

    Hi Chuck,

    IMHO the Standard is mm nowerdays. IC manufactories using it and even

    NASA.

    I could have checked or calculate it, but was 1. too lazy and 2.

    wanted to kick the OP to use precise information image

     

     

    Yeah... After I posted, by client updated the thread, which is when I

    found out that Rob had answered the question hours earlier.

     

    As far as standards go, it's good to hear that metric is fairly

    pervasive in Europe.  It should be world wide.

     

    Back in the late 70's, the US mounted a government mandated conversion. 

    Actually, I don't think "mandated" is the right word - it was more of a

    strong recommendation.  This effort is where we got the 2-liter Coke

    bottles and the 0.8-liter water bottles.  The drink industry adopted it

    well, but overall the effort failed miserably.  After that, the slow

    learners running our government figured out that this conversion was

    going to have to be done on a voluntary basis.

     

    Metric IC packages remained on imperial units until surface mount took

    off... mostly.  R's and C's are still referenced as 0603 or 0805 which

    reference mils.  I am glad to see that these jelly beans are also being

    referenced with their metric equivalents.  This divergence from metric

    probably stems from the fact that resistors as small as 0402 were

    available only to the military in the '50's.  At the time they were

    classified - I don't know when they were declassified.  The textual

    descriptions of R's and C's still contain the imperial sizes.  Eagle

    libraries (as late as v7 contain) contain imperial sizes for these

    components, further slowing the adoption of metric.

     

    I truly wish we would standardize on a single system of units on a

    world-wide basis.  There have been too many mishaps because of these

    differences.  I believe in NASA's case, it was the loss of the Mars

    Orbiter in 1999 wherein the engine manufacturer provided the thrust of

    the engine in pounds of thrust, when NASA used the same number as

    Newtons of thrust, that caused NASA to force all suppliers to publish

    specifications in SI units.  NASA started using SI units since at least

    1990, and 9 years later nobody bothered to verify the units.

     

    The culinary industry hasn't even thought about it.  Every recipe my

    wife has is measured in teaspoons, tablespoons, cups, pints, quarts,

    degrees Farenheit...

     

    Aviation: Altitude is still measured in feet (pretty much world wide)

    while temperature is measured in degrees Celsius.  The thrust of a jet

    engine is still measured in pounds instead of Newtons, and weight of an

    aircraft is measured in pounds instead of kg.  U.S. Government published

    charts show runway length in feet.  Charts published by a private

    company (Jeppesen/Boeing) have both feet and meters.

     

    But I digress.

     

    While I agree with you about what /should/ be done, I disagree with the

    extent of deployment, at least in the US.  Imperial units are still very

    pervasive in the consumer markets.  Sciences are being taught in SI

    units, so that will help the young understand just how long a meter is,

    and what a kg feels like when it's picked up.

     

    (BTW, I do have a 2 kg reference mass that I use for calibrating

    scales.  And yes, it does weigh less closer to the equator (N = mg -

    mv^2/r).  One must compensate for this based on latitude when calibrating.)

     

    It will be nice when we reach such a status...  One set of tools in the

    garage.

     

    Best regards,

        - Chuck

     

     

    Attachments:
    6403.att1.html.zip
    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 6 years ago in reply to dukepro

    Am 14.01.2020 um 16:17 schrieb Chuck Huber:

    On 1/14/20 04:34, Joern Paschedag wrote:

     

    Hi Chuck,

    IMHO the Standard is mm nowerdays. IC manufactories using it and even

    NASA.

    I could have checked or calculate it, but was 1. too lazy and 2.

    wanted to kick the OP to use precise information image

     

     

    Yeah... After I posted, by client updated the thread, which is when I

    found out that Rob had answered the question hours earlier.

     

    So what. No sweat image

     

    As far as standards go, it's good to hear that metric is fairly

    pervasive in Europe.  It should be world wide.

     

     

    Beleave me, I felt nearly unconsciousness when I heard (couple of years

    ago) that the British changed to metric in TV, Documentation etc.

     

    Back in the late 70's, the US mounted a government mandated conversion. 

    Actually, I don't think "mandated" is the right word - it was more of a

    strong recommendation.  This effort is where we got the 2-liter Coke

    bottles and the 0.8-liter water bottles.  The drink industry adopted it

    well, but overall the effort failed miserably. After that, the slow

    learners running our government figured out that this conversion was

    going to have to be done on a voluntary basis.

     

    Metric IC packages remained on imperial units until surface mount took

    off... mostly.  R's and C's are still referenced as 0603 or 0805 which

    reference mils.  I am glad to see that these jelly beans are also being

    referenced with their metric equivalents.  This divergence from metric

    probably stems from the fact that resistors as small as 0402 were

    available only to the military in the '50's. At the time they were

    classified - I don't know when they were declassified.  The textual

    descriptions of R's and C's still contain the imperial sizes.  Eagle

    libraries (as late as v7 contain) contain imperial sizes for these

    components, further slowing the adoption of metric.

     

    As you know in Eagle it's no problem it will be converted automatic.

     

    I truly wish we would standardize on a single system of units on a

    world-wide basis.  There have been too many mishaps because of these

    differences.  I believe in NASA's case, it was the loss of the Mars

    Orbiter in 1999 wherein the engine manufacturer provided the thrust of

    the engine in pounds of thrust, when NASA used the same number as

    Newtons of thrust, that caused NASA to force all suppliers to publish

    specifications in SI units.  NASA started using SI units since at least

    1990, and 9 years later nobody bothered to verify the units.

     

    That would be funny if the loss wouldn't be so sad image

     

    The culinary industry hasn't even thought about it.  Every recipe my

    wife has is measured in teaspoons, tablespoons, cups, pints, quarts,

    degrees Farenheit...

     

    Aviation: Altitude is still measured in feet (pretty much world wide)

    while temperature is measured in degrees Celsius.  The thrust of a jet

    engine is still measured in pounds instead of Newtons, and weight of an

    aircraft is measured in pounds instead of kg.  U.S. Government published

    charts show runway length in feet.  Charts published by a private

    company (Jeppesen/Boeing) have both feet and meters.

     

     

    I had a pilot license and if I estimate an altitude I do it in feet

    still today...

     

    But I digress.

     

    While I agree with you about what /should/ be done, I disagree with the

    extent of deployment, at least in the US.  Imperial units are still very

    pervasive in the consumer markets.  Sciences are being taught in SI

    units, so that will help the young understand just how long a meter is,

    and what a kg feels like when it's picked up.

     

    (BTW, I do have a 2 kg reference mass that I use for calibrating

    scales.  And yes, it does weigh less closer to the equator (N = mg -

    mv^2/r).  One must compensate for this based on latitude when calibrating.)

     

     

    Well that depends on the  tolerances one allows... image

     

    It will be nice when we reach such a status...  One set of tools in the

    garage.

     

    Best regards,

        - Chuck

     

     

    Was verrrry nice to hear from you image

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • stevemann
    stevemann over 6 years ago in reply to dukepro

    OP here.

    Back in the 70's I was installing brain scanners in hospitals around the US. The company was all metric which I really learned to love. (Metric, not the company).

     

    While I would love to be all metric here, American 4-40 screws are a fraction of the price for 3mm screws.  In our common home improvement stores a package of ten 3mmx10mm machine screws cost as much as fifty #4-40 screws.  If I go to a hardware store, the differential is even larger.  I did buy some metric hardware online, but the shipping cost wiped out any savings. Worse, 3mm is the smallest they stock.

     

    So, yes, my question was quite precise, even if our Country's measurements aren't.

     

    And in reply to the anonymous poster who said: "The built-in help is quite good on most of this, as is the PDF manual."

    Remember, what is obvious to you may be someone else's mystery.

     

    The built-in help does not tell me that the unit is my grid units, or that I can put the units in my hole command.

    The only example is ambiguous: "

    HOLE 0.20 •

    If the actual unit is "inch", the hole will have a diameter of 0.20 inch. "

    Until this thread, I did not know that the "actual unit" was the grid size. I am still learning.

    The PDF manual has a single line to explain the hole command: "Define a mounting hole (not plated-through).", but no examples that I could find.

     

    But, I really do appreciate the prompt suggestions.

     

    Steve

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 6 years ago in reply to stevemann

    Am 14.01.2020 um 21:03 schrieb Stephen Mann:

    OP here.

    Back in the 70's I was installing brain scanners in hospitals around the US. The company was all metric which I really learned to love. (Metric, not the company).

     

    While I would love to be all metric here, American 4-40 screws are a fraction of the price for 3mm screws.  In our common home improvement stores a package of ten 3mmx10mm machine screws cost as much as fifty #4-40 screws.  If I go to a hardware store, the differential is even larger.  I did buy some metric hardware online, but the shipping cost wiped out any savings. Worse, 3mm is the smallest they stock.

     

    So, yes, my question was quite precise, even if our Country's measurements aren't.

     

     

    In my eyes it was not. If  there is no description it is just a number

    of nothing (even if it is well known in a special job).

     

    A similar thing (in articles and forums i.e.) is the use of

    abbreviations without explaining what is meant.

     

    In some earlier days it said:"Massachusetts Institute of Technology"

    with the abbreviation (MIT) .

     

    During the article the abbreviation was used but everybody knew what was

    meant.

     

    Nowadays some just write the abbreviation alone  but check out for what

    MIT alone may stand also.

     

    Here are your own words:

    "Remember, what is obvious to you may be someone else's mystery".

     

    And in reply to the anonymous poster who said: "The built-in help is quite good on most of this, as is the PDF manual."

     

    There are no anonymous posters. The problem is the element14 interface

    with the newsreader. Appendages and other things  are not transmitted.

     

    Remember, what is obvious to you may be someone else's mystery.

     

    The built-in help does not tell me that the unit is my grid units, or that I can put the units in my hole command.

    The only example is ambiguous: "

    HOLE 0.20 •

    If the actual unit is "inch", the hole will have a diameter of 0.20 inch. "

    Until this thread, I did not know that the "actual unit" was the grid size. I am still learning.

    The PDF manual has a single line to explain the hole command: "Define a mounting hole (not plated-through).", but no examples that I could find.

     

    But, I really do appreciate the prompt suggestions.

     

    Steve

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/287201

     

     

    Don't worry if you don't find the answer in the "Help". The eagle

    community is always willing to help.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 6 years ago in reply to stevemann

    Am 14.01.2020 um 21:03 schrieb Stephen Mann:

    If the actual unit is "inch", the hole will have a diameter of 0.20 inch. "

    Until this thread, I did not know that the "actual unit" was the grid size.

     

    That's a bit of a translation problem in the documentation (remember

    EAGLE is a German product).

     

    In the German version of the manual this sentence is

    'Falls die eingestellte Maßeinheit "Inch" ist, hat das Hole einen

    Durchmesser von 0.20 Zoll.'

    which I would translate to

    'If the unit is currently set to "inch", the hole will have a diameter

    of 0.20 inch.'

     

    In German there is a word "aktuell", which sounds similar to "actual",

    but most of the times translates to "current"/"currently" (false friend).

     

    HTH

    Markus

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • stevemann
    stevemann over 6 years ago in reply to autodeskguest

    autodeskguest  wrote:

     

    Don't worry if you don't find the answer in the "Help". The eagle

    community is always willing to help.

     

    Joern Paschedag

     

    That's the best answer of all.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • stevemann
    stevemann over 6 years ago in reply to autodeskguest

    autodeskguest  wrote:

     

    That's a bit of a translation problem in the documentation (remember

    EAGLE is a German product).

    Markus

     

    Really?  The About page says Eagle by Autodesk, and to open Eagle, I log on to an Autodesk account.  Autodesk is based in San Rafael, California.

     

    But, growing up in this moronic Imperial system of inches and pounds, a 4-40 screw is remarkably normal and generally needs no further definition. To be honest, I still don't know how to describe an American Standard 4-40 screw any other way.  (In hindsight, I should have gotten my calipers and measured the hole size I want in proper units and this hole (sic) thread would be much shorter.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • omega-5
    omega-5 over 6 years ago in reply to stevemann

    Am 15.01.2020 um 15:55 schrieb Stephen Mann:

      wrote:

     

    That's a bit of a translation problem in the documentation (remember

    EAGLE is a German product).

    Markus

     

    Really?  The About page says Eagle by Autodesk, and to open Eagle, I log on to an Autodesk account.  Autodesk is based in San Rafael, California.

     

    But, growing up in this moronic Imperial system of inches and pounds, a 4-40 screw is remarkably normal and generally needs no further definition. To be honest, I still don't know how to describe an American Standard 4-40 screw any other way.  (In hindsight, I should have gotten my calipers and measured the hole size I want in proper units and this hole (sic) thread would be much shorter.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/287184

     

     

    4-40 is not the full name for the screw thread.

    It should be UNC 4-40.

     

    The UNC thread (Unified Coarse Thread Series) is the American

    coarse thread. It has a flank angle of 60 ° and is measured in

    inches. ... The corresponding fine thread is known as a UNF

    thread (Unified National Fine Thread Series).

     

     

    Freundliche Grüße / Kind regards

    Friedrich

    -


    ... use NNTP://news.cadsoft.de and a

    functional news reader like Thunderbird!

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>