Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Testpoints for ICT testers
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 26 replies
  • Subscribers 188 subscribers
  • Views 5301 views
  • Users 0 members are here
Related

Testpoints for ICT testers

e14 Contributor
e14 Contributor over 15 years ago

Is there a way to systematically insert ICT testpoints onto a PCB layout

without putting a testpoint component on each net on my schematic?

Ideally I'd like to know the percent of nets covered by testpoints and

have someway to highlight or locate nets without a testpoint so I can

either add one or can decide that the particular net isn't worth the

trouble to test.

 

-Michael

 

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 15 years ago

     

    "Michael Sansom" <mssansom@hotmail.com> wrote in message

    news:ifb4bo$pg7$1@cheetah.cadsoft.de...

    Is there a way to systematically insert ICT testpoints onto a PCB layout

    without putting a testpoint component on each net on my schematic?

    Ideally I'd like to know the percent of nets covered by testpoints and

    have someway to highlight or locate nets without a testpoint so I can

    either add one or can decide that the particular net isn't worth the

    trouble to test.

     

    -Michael

     

    Hi Michael

     

    Your requirements to reconcile net names with test pads and have a freely

    placeable copper object in the layout editor would likely require a new

    special object.

    I imagine an object that is similar to the via, but un-drilled and only on

    the top or bottom layer, would work to some degree.

    What you are left with then is, like a via, only being able to determine if

    one of these objects has a net name the same as a wire (routing). More code

    is required to determine if they touch.

     

    For now the following idea may be acceptable to you. Doing it this way you

    will be able to get all the net name reporting you require, after a ULP is

    written.

    It does involve the schematic but visually there is only an increase in the

    number of 'junction' dots displayed. I would expect that in most instances

    you will use the junctions that are already drawn and occasionally  have to

    place one on  a net wire.

    The test points symbol is mostly on a new User layer which you only display

    when needed.

    The attached image shows what I mean.

    Packages for these test points need placing in the layout editor but there

    will be an airwire to assist.

    Using Devices with multiple packages you can conveniently "Change Package"

    in the board editor to lay down a differently sized test point that is more

    appropriate for the available space.

    If the test point needs to be away from a trace, this method lets you route

    back to the trace as there is a valid net connected (airwire)

    The 'Show' command displaying the complete net assists with choosing the

    optimum place for the test point.

     

    A ULP could now identify which nets do not attach to an element (your

    various test point styles) with a nominated prefix.

    One of the current assembly ULPs could provide the XY locations of the test

    points and maybe their related net.

     

    HTH

    Warren

     

     

     

     

     

     

     

    begin 666 ICTPoint.gif

    M1TE&.#=AO0(S`?<`````````0 ``@ ``_P`@```@0 `@@ `@_P! ``! 0 !

    M@ ! P!@``!@0 !@@ !@P" ``" 0 " @ " P"@``"@0 "@@ "@P# ``#

    M0 # @ # P#``#_0 #_@ #__R ``" `0" `@" `_R @`" @0" @@" @_R!

    M`"! 0"! @"! R!@`"!@0"!@@"!@R" `"" 0"" @"" _R"@`""@0""@@""@

    M_R# `"# 0"# @"# R#`"#_0"#_@"#__T ``$ `0$ `@$ `_T @`$ @0$ @

    M@$ @_T! `$! 0$! @$! T!@`$!@0$!@@$!@T" `$" 0$" @$" _T"@`$"@

    M0$"@@$"@_T# `$# 0$# @$# T#`$#_0$#_@$#__V ``& `0& `@& `_V @

    M`& @0& @@& @_V! `&! 0&! @&! V!@`&!@0&!@@&!@V" `&" 0&" @&"

    M_V"@`&"@0&"@@&"@_V# `&# 0&# @&# V#`&#_0&#_@&#__X ``( `0( `

    M@( `_X @`( @0( @@( @_X! `(! 0(! @(! X!@`(!@0(!@@(!@X" `("

    M0(" @(" X"@`("@0("@@("@X# `(# 0(# @(# X#`(#_0(#_@(#__Z `

    M`* `0* `@* `_Z @`* @0* @@* @_Z! `! 0! @! _Z!@`!@0!@@!@

    M_Z" `" 0" @" Z"@`"@0"@@*"@Z# `# 0# @# Z#`#_0#_

    M@*#__\ ``, `0, `@, `_\ @`, @0, @@, @_\! `,! 0,! @,! _\!@`,!@

    M0,!@@,!@_\" `," 0," @," \"@`,"@0,"@@,"@\# `,# 0,# @,# \#

    M`,#_0,#_@,#___\``/\`0/\`@/\`__\@`/\@0/\@@/\@__] `/] 0/] @/]

    M__]@`/]@0/]@@/]@__^ `/^ 0/^ @/^ __^@`/^@0/^@@/^@___ `/_ 0/_

    M@/_ ____`/__0/__@/___R'Y! ``````+ ````"]`C,!``C_`/\)'$BPH,&#

    M"!,J7,BPH<.'$"-G$BQHL6+&#-JW,BQH\>/($.'$FRI,F3*%.J7,FRI<N7

    M,&/G$FSILV;.'/JW,FSI\^?0(.>E'20$%)2)$636I4J-.G4-G4JUJLFF

    M1[-J'8CU7U>K8,.'4NVK-F27;%^]<JUZ-FW<./G4O7:=JV"M?6W<NWK]^_

    M@"G>%:@7;^##B$6N3<MT:=$D",_;*IV86')F#,G7R5AUD'/?].?FIAIHL;1P8`H/S>\K=RY^/D+U]

    MS#98]1/\WY[FUM!QV !-'WT4'DI1@00NZA)] #]'''(4NE;_X(7)-3B1

    MAB!Q('*BT(HG?:45C=B1BF>)N&]S'8(H3^?=A>A .]"..--OKW'T$>ZECC

    MCCR2-^--YH$']$%JG<>>I]UJ24,6()(:=!5%[Y8T(C?AFD

    MF&-R&:.+!W5)9I1^A3E6A$JRN9.(6&X)I)!XBJFED7L:F>:=8'HYYJ!E`IHG

    MFH2Z:=&.BHJDJ.!UG3FH82Z!\BE5-'IHXPV)EJGGX6":F:D]6T:HR;@LBB

    MG90N6ADI+YJ*@OP=DGK>1=JNM4= ::XZ=Z`DOEH3W.>NNPN":[9K"MNCH2

    MK6>5.Q,O:X)[6VZ8BI5M0N-:BVKS'JZ_VRSHM9YZ*Q^GFNL
    :VBFG9K:8

    M)"=#OOKNY42NE]<XXI;MVXC?I=]GN&M6_>A(KB#(JONK/D;.Z=WHYH

    MJZ#LNL1P@UC^2VX? IJZ[@D_UENN/!RC.ZZ!!<,R+8`#_FNO .CNS"\![9

    MZ(])HJNOM]W.C'-T!M_$[:DZ\PORJ<="K&C%&"-M<M(G6^JRMI!=FQ_$&C]4

    M,$Z:GFDJPR'GZ7#'Z;HXJ<.-+DWURD-[M^O7ZW$-MMU=-T2W34>K/?*W59\-

    M]-L0UVRJ@`#7EZV_[A<MU!:YRW0U493C#?:BO<I>-0*_TSN1&W>F[DIQF,

    M:=&2IUX2Y7S3*V&RPK"CO'G)H<?[>>P6VZYXR]J>CKKJP'MT-=;4QJQED33C

    MVV_5-NML*LV=V\QYJ4JR?!W6O;\<_/;"^_Z[6:2W%#[W`Q%/_OD8,>XX7..'

    M>#GZ"YD/__P1F?[R]V2UGY^G>33___\;-?X_ 'P ZKX ( CVM'? !-*O

    M@0Z,X.2T)\$(0K""";P@!LGP0WKX,>3)VNV /"$/:/@B:D'_]2Z*H2LK!K

    M`(# "RV(PAF2+X8VS& -<Q@\",B0A_,;(0!<"$0H^;"(_ULA$LMSQ"7"#X=.

    M5%T3HWC#'U(Q;U.\8@^MJ$5V9;&J?LB&.4DQC%JK(QF5!$:T[BH-;#L4!N

    M?*,1N2C'%,6QCABZ(QZ92,<]1DF/?O0.( ,IGT$2,CJ&/.1W$JG(X3"RD=)Y

    M)"1M(\E)$J>2ED0-)C-YFTUR4C.>_&1J0BGR)"RE$Y)2H_8B'"/(DKK_R(

    ME<IF5G2<B.MW(Z .F++6RFE[[$"' LU$J/`#.8?SDF,@53(<NL1)G+W LT

    MHPF1W#A3)=.D)C,'Y,K'T":6QNRC-ED"GVNF))OCC$@N322>=H8SG3 I9UZ>

    M4YXNF28SBDF+MI_\KJ"8^V.1G/U5BS7D&= I(<TN2V,2=/Y$G\()7D&M

    M<U"$#B5 W&R-<V0IT/=LU"L1E>@_S8D2AUJT,A_5Y4A,VI-UAA1X\J3H.3MJ

    M48Z@U#%*:8W1<)2GA 31?+Z7@J6M.0H&>G/.GI3B!:0(6R,Z,-I2E=F$J^

    ME\Y$J3JA:E Q^E3NZ),C6,U),7//:O)*PXT2K];LI.E?)4JG-QZ?G,&A.T

    MWD2M\V.KDY *2[YR%#(_=2<M[6H3O%;UJ'1E"6%K8MC!PE4NC9VK4Q9+D\BB

    MDK5[6IBG;59EV!6)I8MY6=G@IZA;E4HHXWG1P6[RM0652>NO>=J.^O'V"^

    M]B:V)>=L0RB(LS[VMLG\[7(TZ\'>]A8FN07N586[''"R_[: Q_U'=%N27.76

    ME;G6Y4AO(8##Z084N]F52W6UN5WN^A "WCW)><<;7GJV-R7E->\1TTN2]9[W

    MO9!A+S*/>]X8WI>;[5O689'X (;, (3K""%\Q@`]-'OUVTKX0G3.'^]K=1

    M/O1OA3?,X0[?=RP-#K&(1TSB$BN8.9%H2UZ.$66WB]&LZPBV=,8[*8^,8X

    MSK&.AS<6&8=5P/@M27PU+-WOKM?&1,16DI/J8_!B9,)!%K(@?"P(`-?WR$C>

    MH=R6O),7Q76=ZQF,=,9@=/I;Q65J3%:/3G'Y-00L"8UGW+8YV]G#82ZS

    MGO=,9JI,^7TK73-(R%J=E\99.J"'#O2=6QSC13L:S&+ALZ0GG>.J0/$EHYT0

    M4+WVYM0D>K)-5JR$LSR?3_MDL:[5*T1,31Q6!\7'GL4RB#N-&E=W6= :2756

    M_!I +6/'UJ_&=49TO5<W^_IZM%[N=>]ZE/ P!-A*/O944"WLCA#:JZM.MFB@

    MC1-J,WNDG)8VT;3=[6I?)-/BV2RW8;-NFWB[L)TQ-DUTVXFQO>W=';O#-3

    M_V:O)NQ\<ZVN%E#F28=M:](_6I0@U;<UN$V)[AM4(8ONU]Q_K>`&_VM9\-

    MPL%X'#FY8<Q4%YNC&<6EOD^",GI;7'J.KPBS:V0SZN%9K77.126;F[7TX1

    MB=;X5NN:A-'NF.@]RTJ_F*432M::CHO";_/OF)Y#WPY#S=Y40/"ZM#SAB#

    M0X?IS_W)U96MXF]/'>@-X3I9#][-A]6&,_R*/G3O>ZV]W#)"SSS)_J39OC

    M9>G/H6U,XIYU]^(;X3)/^]%KOOC6X#PJA"_(W2=/^<K?.>]]5CQ#D][XOT=\

    MTPL7NF\+;Y6M=S[PIP_\XYTN>J)>?,!&9[SL/;_X"?\)'B:1QS3/)Q)SM#/$

    M[Z4!_-&=FO/6SY3T57$U=8 O?(T6>N3&USWRJ6+ZK?"5[>X$//$A'WTU3[\E

    M7=_XQ%UX?8.7MNV$7C[TJPX2R[O__?"'\1#UKOG9]#WUPK?]^JL2== NE./L

    M-QRYIQ#Q5X &:'>8-V9[MWFH-WNTIW_%%X"W]GT$]7,4,8" @8%#5W:PQW[,

    MAR-]X -R'T2V' 4N!)JX5P)H8%P8*NAW4=.!G.1WLT'PV2(\MWL2X7.J

    M-GXE&&UET7@M5?BMXD=VWG!UF]R3J%X$Y>((5B'0`&'0_!-"&$__UVM4

    M(0<F'%O9X15R&[=!X/2EUD>/>@0+L@7:1@25ZA:X(:&8_@7:A]72AU2EB$

    M8+B%_U31AB]Q4U95?8ZW4]B'?7>(AW 7AX97AEYH@7 8AG"&B($&A0E%A(GW

    M>Z+Y'4JSXBR!(<,D7AHXD 198>RX8[(6OZ8?9OH

    MA"B&CPWQC(V8D L9CPNY?WL(D0PAD:)(D?_83IC(BJ6'C>>QF(M@D8HB^9%*

    M]Y$8.6T:N1 <V8WUYVP5V4RS9HXYP8?4MXO?&'[4>(D!B9.RV'XON1*V5G[A

    M"([I1VJB5I!.69 'J6,>66P@Z8OH1XZX1Y*XJ(U%)Y0LYY4[^)1BJ8Y166G>

    MJ) J68TWR85<J8M@B1G+:(HF.9(>")15R9!AAX,9.92OJ)7Z)>1.)=!8.:

    MV(\LB94T$9>Y5I0)$9.U:#5OZ6^,B1".Z8/5A(1*67!,R)0NR9=B!YAPH9A$

    MZ9D(9IF89KG-IERIYHG@9J<18ZV9`YJ29H]X9IK9"VR1.XV97_;/EZ

    MKYDKM#F:@KF3D1D9OBB@$(H3'<J?4O&A

    M*(%29VB@&QH8-:J<,WH3/ZJA'I\:75VT/B>/7J=3JB2EJDPRA62#J13XJA

    M"GI/(6J(;JD<JBB81FD-O6&'5FE,IJA_O2B+ON8GPDZG: HIC9G?IYI;J%

    MIDE*HE&!HY,8<'5J4!7B5_-X%D-:C"9J6R$(HV3_>J.#:J(,M:-;>I:MR(AY

    M&8-6RJ8GQZ@&$:C7R57IGL?%A.#(\.I4KB9=T@:GW":XY*:/":=K:F2=

    MZJ26N(K'6*I>F2):G:0J9JVIDN!V0(.I/YAIA$.JE-ZH:J:IFQVJ<;]Z?0

    MJ:F!V91CF6'SEWG NHG"A2FZJ&W:H=3.J;\AL=:VW6:O.V)S1G]Z5DVY

    M.JMSD:T1N9Z^BH7@6(G\&)VNA?NRIRQ%J\JJZJ=J]UD:\P::ZC9J%2&)*N

    M)?.*I?0JK]JJXF$JYJ2*[JN:^R!JO)RHT)&Q<"RYX#ZK 8ZZAWJ%/B.JX+

    M&Z6]>JYEB6.$B6VT.+$GOTN<<NJB5YFF%UJF#3N6*WMC_GJ,)1MZ,?M79CH4

    MYV&S6Q:T<D:P_%J?,OBO5AFP%*NMJ'H13<>NEQJU-AH6: 5I(9NL8FJIDLJK

    M,PM^XNL=@H6A 6R#]NR&J=TH JH6N1V[J(&ZM <3NL.$NIGMJV6FJW2*NP

    M4)J-W-J0H7JH6CNWI%6T>[JKB#JU1581"F>VK)JWQ2I;)6*TOW:W!(BX&V%<

    MD M5WOI[]_=U2+F4-R>.I:FYY>JX5%NV(SJY_XT[M X176G&IW7KM^Y8M9\W

    M@X69A>:INJ<JNV=JC9++N'?*N1=19516N[LE$:E8D[SXJ'>9J7&JM\9JM5?[

    MMQPOLYHT/V7RS!;1<IJX:)O33O>_NA81N:]KO%"!IPS!7Z'VN"EQE8

    MDC]IE[=K$QW;F,B[M\1;O'DQNB!7NGJU=(28NEQZK@S,8?Y59TTF83MK8A/1

    MA&JIOX0[G@KMK[N0'<OJ&HNVSAAS8)D-@JD V<PA/6:"R\81-<8A6\:Q3E

    M&FY%O<1ZGXOI7_FXO^7#D] KO=+KNQJLO1L!O_%[HJ'&O"#QO#(,;C3<5GA;

    MHF#J92XAOBQ)ON,;J?\1NL$$8<3Q^V+TJQ),W(N\RXBC:L.4B\.V*E_-:;\D

    MK'''D<4_.Q]B\1@NEW=5<4E%$MNBYE^*GYS!WJ,$+,$8UF$O3&(Q7)C1

    M6[X\G)A<[&H2KO61J_NZ[7J6<B:#&-T-JT**!&5H;A/3,9H'MC2Q&>:U-_

    M&,F\241]NYVGALK,=U.5(2UAR',7'Z[A*W.8BVP2,X];^9K,.TG+M0

    M7,9O;Y"RLIVPHF,&X:[@B.\Q3FV(OH7Q^2K3V&:@J\"!6Y)+)<T$4<=#

    M#,JG1LQ'LN(EF2!#30G=:7,[.?,[JE,X=K,J6?+,S]\Y?&LS2,X]3,0S

    M;P%M_FRK:P1P@S"1O+4?._H>ZJQJ@=C'XT8C1I[U;B\I7NSODOQUHU(9DKTSU/-U'#]=H6JIR[[

    MR*T;TQ
    S1#TRHVV.G:M#X[PU\X.5I-@US=:Y -:#(;V@:NK8KD@`[U!.7

    MVA:XV@)LUV9-BL&\KK6-U;?=UDZLUME;O94[F&=IU<]EVRN(V^LCJ-L,#6KT

    M`6Q<?<N93;A%';%7W-6MJL9KF['!:MK&O=UN;7^53=TQFI!MQ\W_Q*SF;94<

    M_==606VB37_5VMSDW54\%M+G_;2BV-HH2\T-/1ET#=MJ=M_4JG@[*LJGW3C0

    MW7S2S:,"KBP>\D4/8'K;8E.BY?.C8RXK:/&[=FF?8%#MAE3>"S#:DN_<'Q

    MC:0R/=)>;77U/-8&_K:P;.(K/K*4^-XX_N)]?> R_MW\C.$;==(]IZ@EO>&6

    M(>1?S>0G?L\:KN+ _-D?#>69&X9(#L]4WLYH;8)8?A:()=]O=M(M62K>-5

    MWL\X_]ZB40Y9%^S(LLVG:)[F%U[DMEOG_EO=-1[5F0BP<S[ K]S;I=/GS:SE

    MH-WE97'&$C[B]/S4^\3GD&ZP*.[F6>Y1$=OA@3[CK6;H:<=V0=[FC\ZV>AXM

    M86X68]YLCAW@8Q;9@BKIF.Z 64S?IE7JIHY3?>S;L2[4Z/W8K>[:0JOHV1'G

    M@.[=.,6_OF;4\]REDXX6F$W;Z4WD;SY<-LF-(57'_C/*30VSL:Z)LV[FTG[I

    M=7'=FF[L?>GHS-R"GI[4NOL;93[=F0+LO"'6-_Y*>2W0>^;J1HCNV_Y02/G3

    MXOXF$"/1HIZ!ZVY.O [@`%CA)B$_PE'P0='BT>[EL ?49:H,EP>?YYS=V74-

    M??S>[SY%OE2JYAX/NI==<<U.$A,EY;F1\/\@\%\_1^Z!7/\9H-M2D_$AO=

    M'/,-[C4!00XOY8L><8/>\7<^DA]OZXKQ[RNM'#4*]%JF[3#?4B@GTC./[#F?

    M/COT\$4?\=:WOU?_\U@+]18/4C?O$]B]Z6L:RO]*PD\FI/\4/,."FZ&7S<

    M]>#!W1//M_#XJ4GIY*6LBR^_[$_!W"U/X_]9[]1T?[68<=U-G\P9%>/=>>[[

    M;O-GC_9$C].G#LGC)QE^K_E6CI:D7-#H2_8FW]UA47!@G_$R\?32QOJM[\K6

    M"%"A6?JOGQ]>ODA?ZSP+O>'ON!B6((N79%Z/8-K[JLP_C!<??&/VAZ/_)-

    M?GZIKM=7V?PAD9R2AEJ=/-I1O1O7![A N_AVV_C<9C=7_93#[1C#?SI[&)

    M/&)"3\Z2G[64;Z">GX1.;MVS#_FDG_@`\4_@0((%`15$F%#A0H8-'3X<" $"

    M1(H5!P":%%2P8T).P[\*#"D19(E32[$>/#D2I8",Z)4V5F3)HU_Z74R%'A

    M2(0\;?Y<B1/H4(;_,8D>A2@1Z4.A%$?Z_/=4YU*J3%]6;9E2ZU:N7;U>Q1H6

    M:5.(3R6=10OR[$ZQ;0F2=1M7+DNE<V^"?6@6[5J1>WO:#0L7<-&OA0US'6Q1

    MXF+&C1<#`'!8\M><!*%:Y@LR,57!FSTGKJLQK=K1$#M_1DWR=.J[DUUK9=W0

    M\6S&D%_?-IIWJD.IL6VN]NW2</"2H9U:UEP2.''FK9LK?W[2>-SE?Y%[W"TR

    M.LOJJ'%O9SA==_+#KN#_WP>?6[T#L6W5:_]NO7D]=M7C&\7-^7[&BO

    M\A*KS^Y"C0PP8^"PPOWC@2\",!Z5.P(03AZ\J@W+SJC\&RY /1*O8J??3L

    M0A(-]' AOTC3,0363,1JPP1<K UV-IL2&H!M1PQ!<!B]&[X5[,D4()30KR

    M1Z"2/(H_A6J\Z$;PBF2K2M.@5/) +*/[KD(JYXLJ1(N8S)(F,I>4$B;SS@SK

    MRS"M&]-'U7T:$4Q`YRP3.?NVVK!-W$+BH[KYQ33['8__QIR[<*?0O'B4CB
    MZ4C\%-6IM_I:#/#-%Q&5<<8H>_3S/D"M"XG'11DUM"I.J4-55,9$LW-0%X\K

    M-="-)(VTS%67\G11`IV<\E&3=IRTU53'HK2Y9-&;;:[X;@7S+UPIW'39S8"E

    ML=!0@SWI,E.C-/98HG;%D*%(6U0QPF]E:E;<"6%L\I,XXWS1'1K([2-)\;

    M]<YH;16SY*HQ?." V]M\%T=^-QW9]H@[BVR/J4[#@02QUMWGG_)3'A1(U=

    M-MS/^LU58(!%AC9:"6LMV&'P/%;5QY3]-7>NB".VC>#RCJX8/F.WC>C@/>

    MCNCH&H.U-%GE!)!>GS*=5M.A1?]>B>#?1@RZ-ZUM=LS99;<F5;.@3:X09E:S

    M;)=5E)VN.6J.RS8:QD)9)F\JEQ]^U>M6GZ;9Z;'OYC)N9>?N"=V=U,4J;;?4

    M@[<\C04&?'"J8]N2[I_M[EFL?J_>.U!!"=8Z3UT%9PY+=.&E,ZZ;<9Y8Y\(L

    MCA=COA[W.?224^/\#C_)EMS85G*?%9QU1Z=<M]ECKQU6?+V77*\NJ9[]@-

    MIM9>W$O4G6:P[=I<QV*'=U<NJVNJ,6N[SY=+<0R-W?XZH"$???)A;;>JYMVU

    M'ZS[U"DR&_QLY1<_?#G/N[E7P/"MM\,-8W)?4/60)LV0`!.7.=!_X"K>

    M_BX0<2-M45_,^F.]#Z'<PMK5H`%!($IQ>BV>7O=SYFP4ON<&9H^#Z)L@

    M#$4GO!G&#(6Y4^'G(+26L:GNA2V)X?5Z."8E4LZ&[:,>8#YH)1XN$5D_Q)ZA

    MII@\PF#1BOQKXOR:]$0<7DZ*1T0B$[WXQ2KR:8V^V:+0F.:4087.A/237 :I

    M",4BNB6.;X/)&]G8_T6X:1&-W5.M2Q%P@VJ)54R[)0&X>9WK7ID(A4XR"O

    M6$BT&3"-JOF:K598LC#A\7:"3$&!S;$E)F279<<%BA1J<G_<?)'ZCM4.GD

    MMOLA(RI^25K_EC))P63ECVR)9&Z=D $RLN,*GND,;.HIV$"[EEU.'XD'?"

    M"D%&2<NC3?.<URL(KHAVI"2F@B 9,T/6Q)J*9!C+-67:,Y2M[\)C@;(\YQ

    M;LM["2PE_ `Y-3W>TI/ 2R3[1,G+BVW3>O8T8B>1QLQ_XK"5U')E<-;)&8BZ

    M<+$&X_QZO:FC/IFHS89YL@.NC[8-=21C93C0PMZ(EPV2&IHQTT?=E1#_O"

    M4D'=TTL%`[9#.VJSI$[D*6#PJ4Q]2JR?' KI",U8Q'EFZ:0U22EJ-L?(=)[J

    MF$.YZE&6RM2F0H"?3]6E1:.H4SV%=29956E)9L8V,"95DVX="EP]NE*;?@B@

    M%R5I/;WDTS\15H/'.]E7\54FO>[5L&-\%\,H"=.N&@BO+6DL:![KN8$)U:Z#

    MO"S>VAE+S!@NL70$739->U2Y?;8JF74A)EGX/<5RCK&;=908[>.PT%I5FA&E

    M)FZS@UA"UI9\O]7L:'-B.=XB]YB]E8YPN47:V=;5N,=U+7!OUNZ$NJZ9GN

    M[Y03 U%V78=-\.I=K6\.9PN]3M;":__\3Z)H$MF?D[GJMZ]=R5.R,55G

    M>[DVWLI4U[OSS8J 7RM=?O&UKU&M&T/7ZM `9]>/##X:AKM+X5HBF#L*ILI]

    MC?C1Q:45.Q(680TMW%,"-VVWM/7P2>I;' T'IZ:=NJDS)VPRUN9NQ>(-+G>)

    M&T@`H9<\ZC6A3']:X]B4U:EH]6<Y,S;5ZO78Q^_%,GE+Z]F6QLZ_"AQH@F9,

    M$A%?V,EG12M_":@=JG*1H)V\[6+T8^((CW3-E6W/F!7#Y"8O$Z3-O#-@RWLL

    M/=.%S\+T<XES?&(["\W*UP+Q4LILYDD7,[)@?ND\'RVD'UM2H@[VH9H3V.;J

    M*;FP8:>X9)XWM35IK>.ZN4FG WJ9.V#LHF-B>5-;7IQ!2:(I6^L)99N.H8

    M!R72,:U$_4]"]9&^G\WIH.$J7;G,]<$3FF6:)IJE$';VCC<<O\&B

    MVL4`MK2VD71L("<;V!V&,.I:.&A"LYLH[VXW?#G\*VG[S]?1-;>.QD=LU'+U

    M9T2%M:E11.T5ZW4IU6W?/,9\,-.%L81W^I@ZQO/&,0XQ=7)L7W*#99?ASD

    MKAYM'-;Y-GW* IKVC'A=-O\/W[(?CVM+ ?7ER>M?K(LDKRFR>^\?P2O.5S

    M_]2X1"&%Y)+>F5W=JG,BV9OY<%<Y48_.L\7_FF<>QS0=7YFHWD-)HOV.J:2;WNLO:[N!.

    M.S(?CP\`5V;"N\0PSU#:XF@^:EJSG44T9GX/)<]Q)7ZJB"MV^UQ_WI<Y=W

    MX9-.UJ9:OI_-7NNSZ4YNP[,>]$W_N50;& 5E]OO;S/]-Y7.][_R.8T=OOM

    M3Y[W2LT=>6.?,\U1JGS-_AWPDMPM[XH?ZZ'/&M0<7?2H!4IXVJ^^^]<WEY$/

    M[GC30K[;O]>GZ\>)2EKOM30UYOO#Y]+Z8OK&2FOHDS4K9;VQ>5BSUQ2S'C

    M\[SI.[MQ64#_>\"C>#L)]#;@[V-D;T)PS_T8Y8`3*[HVSNM"SFN`T&GR[Z

    M&3*XZ3^:F$!)\T"]"T'%.[\95+0B\[GULYJ@4\$8Y,$>C"NBX\ 8_#\?)$(/

    M:T&D:,$A7(\(,(F7LCI$"R6T'!<L(JM$*@@,)[>\$VZ@Q!);S"+P3#,'3"

    $@ ``.P``

    `

    end

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 12/28/2010 4:02 PM, Warren Brayshaw wrote:

    "Michael Sansom"<mssansom@hotmail.com>  wrote in message

    news:ifb4bo$pg7$1@cheetah.cadsoft.de...

    >> Is there a way to systematically insert ICT testpoints onto a PCB layout

    >> without putting a testpoint component on each net on my schematic?

    >> Ideally I'd like to know the percent of nets covered by testpoints and

    >> have someway to highlight or locate nets without a testpoint so I can

    >> either add one or can decide that the particular net isn't worth the

    >> trouble to test.

    >>

    >> -Michael

     

    Hi Michael

     

    Your requirements to reconcile net names with test pads and have a freely

    placeable copper object in the layout editor would likely require a new

    special object.

    I imagine an object that is similar to the via, but un-drilled and only on

    the top or bottom layer, would work to some degree.

    What you are left with then is, like a via, only being able to determine if

    one of these objects has a net name the same as a wire (routing). More code

    is required to determine if they touch.

     

    For now the following idea may be acceptable to you. Doing it this way you

    will be able to get all the net name reporting you require, after a ULP is

    written.

    It does involve the schematic but visually there is only an increase in the

    number of 'junction' dots displayed. I would expect that in most instances

    you will use the junctions that are already drawn and occasionally  have to

    place one on  a net wire.

    The test points symbol is mostly on a new User layer which you only display

    when needed.

    The attached image shows what I mean.

    Packages for these test points need placing in the layout editor but there

    will be an airwire to assist.

    Using Devices with multiple packages you can conveniently "Change Package"

    in the board editor to lay down a differently sized test point that is more

    appropriate for the available space.

    If the test point needs to be away from a trace, this method lets you route

    back to the trace as there is a valid net connected (airwire)

    The 'Show' command displaying the complete net assists with choosing the

    optimum place for the test point.

     

    A ULP could now identify which nets do not attach to an element (your

    various test point styles) with a nominated prefix.

    One of the current assembly ULPs could provide the XY locations of the test

    points and maybe their related net.

     

    HTH

    Warren

     

     

    Thanks for your suggestion Warren.  That is certainly an improvement in

    my opinion to the cluttered schematic that would result from attaching

    visible test point components to the schematic on the majority of the nets.

     

    Yes, I agree that a special component like a via would be required.  In

    fact, if I could just specify a via with no drill that would work as a

    kludge.

     

    Once again, thanks for the suggestion.

     

    -Michael

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 12/28/2010 4:02 PM, Warren Brayshaw wrote:

    "Michael Sansom"<mssansom@hotmail.com>  wrote in message

    news:ifb4bo$pg7$1@cheetah.cadsoft.de...

    >> Is there a way to systematically insert ICT testpoints onto a PCB layout

    >> without putting a testpoint component on each net on my schematic?

    >> Ideally I'd like to know the percent of nets covered by testpoints and

    >> have someway to highlight or locate nets without a testpoint so I can

    >> either add one or can decide that the particular net isn't worth the

    >> trouble to test.

    >>

    >> -Michael

     

    Hi Michael

     

    Your requirements to reconcile net names with test pads and have a freely

    placeable copper object in the layout editor would likely require a new

    special object.

    I imagine an object that is similar to the via, but un-drilled and only on

    the top or bottom layer, would work to some degree.

    What you are left with then is, like a via, only being able to determine if

    one of these objects has a net name the same as a wire (routing). More code

    is required to determine if they touch.

     

    For now the following idea may be acceptable to you. Doing it this way you

    will be able to get all the net name reporting you require, after a ULP is

    written.

    It does involve the schematic but visually there is only an increase in the

    number of 'junction' dots displayed. I would expect that in most instances

    you will use the junctions that are already drawn and occasionally  have to

    place one on  a net wire.

    The test points symbol is mostly on a new User layer which you only display

    when needed.

    The attached image shows what I mean.

    Packages for these test points need placing in the layout editor but there

    will be an airwire to assist.

    Using Devices with multiple packages you can conveniently "Change Package"

    in the board editor to lay down a differently sized test point that is more

    appropriate for the available space.

    If the test point needs to be away from a trace, this method lets you route

    back to the trace as there is a valid net connected (airwire)

    The 'Show' command displaying the complete net assists with choosing the

    optimum place for the test point.

     

    A ULP could now identify which nets do not attach to an element (your

    various test point styles) with a nominated prefix.

    One of the current assembly ULPs could provide the XY locations of the test

    points and maybe their related net.

     

    HTH

    Warren

     

     

    Thanks for your suggestion Warren.  That is certainly an improvement in

    my opinion to the cluttered schematic that would result from attaching

    visible test point components to the schematic on the majority of the nets.

     

    Yes, I agree that a special component like a via would be required.  In

    fact, if I could just specify a via with no drill that would work as a

    kludge.

     

    Once again, thanks for the suggestion.

     

    -Michael