EAGLE User Support (English) Devices on Schematic, but not on PCB
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
  • Replies 15 replies
  • Subscribers 181 subscribers
  • Views 2507 views
  • Users 0 members are here
Related

Devices on Schematic, but not on PCB

Former Member
Former Member over 15 years ago

How can I have devices on the schematic diagram, but not on the PCB ?

 

On my schematic I want to draw some devices who are external to the PCB,

essentially to have the complete thing on the same diagram. Some of the

devices are external to the PCB. What do I have to do for Eagle to know

about that and not to insist the I place an route them ?

 

Markus

 

  • Sign in to reply
  • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    This is why I used the name "symbols not on board" image

    r

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    Ing. J.M. Rafetseder wrote:

    >This is why I used the name "symbols not on board" image

    >r

     

    yes I know, but the OP wrote "But when I want to add this device to my

    board I get the error 'Device has no Package'"

     

    So I pointed that out again

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 15 years ago in reply to Former Member

    On Wed, 16 Mar 2011 06:23:49 +0000, Lorenz wrote:

    Ing. J.M. Rafetseder wrote:

    yes I know, but the OP wrote "But when I want to add this device to my

    board I get the error 'Device has no Package'"

     

    Yes, I found that you can not have pins, that means I can not just copy a

    symbol to a library, remove the package and use it. You have to remove

    the pins too.

     

    For now I have placed the drawing into layer 97 (info). From scratch with

    no library involved.

     

    Markus

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wheelthru
    wheelthru over 9 years ago

    I know this is an old post, but I'm facing exactly the same situation:  I'd like to include parts in my schematic that are external to the board.  Here's one more vote for adding a less arcane facility than having to replicate and modify lib parts with no pins or package.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 9 years ago in reply to wheelthru

    Jim Williams wrote:

     

    I know this is an old post, but I'm facing exactly the same

    situation:  I'd like to include parts in my schematic that are

    external to the board.  Here's one more vote for adding a less arcane

    facility than having to replicate and modify lib parts with no pins or

    package.

     

    search for "Devices without packages" or "external" in the online help

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<