Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Missing components in the library...
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 37 replies
  • Subscribers 188 subscribers
  • Views 4170 views
  • Users 0 members are here
Related

Missing components in the library...

e14 Contributor
e14 Contributor over 15 years ago

Hello,

Still using the free version and still at newby silly question level.

I am creating (at least trying to) my first PCB board which is going to be a PMW. I started by ordering all the coponents from digikey (got an head acke with their web tool..)

 

My coponents are in my ordering list:

* SN74ACC14N: Found it sounds good

* EVU-F3lFL3B14 (potentiometer): even with the datacheet I do not find it

* 1N5817 (diode): can not find it... 9there is of course some close enough)

* BUL704 (NPN) was not able to find it directly but using the number of the datasheet TO-220 whihc was not in the database either I end up finding it using TO220...

* 1N914BTR (diode) was not able to find it... (same thing found stuff close enough after some time but my electronic level is limited)

 

And the list is going a like that on every conponent.

My frustration level in rising, I spent more time looking ofr the components that I will spend on creating the board (step that I have note reached yet...)

 

 

So simple questions:

1) I am doing something wrong?

2) If I am not doing anything wrong where can I find an extended library of components?

3) If netheir one or two are possible, how do you proceed on your side to order components? you try to see if they exist in Eagle then in DIgikey (for example) and then only order them?

 

Thank you for your help

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to Richard_H

    Thank you Richard.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Richard_H
    Richard_H over 15 years ago in reply to e14 Contributor

    Am 21.03.2011 02:33, schrieb badbad2142:

    as an example:

    http://i203.photobucket.com/albums/aa14/badbad214/Eagle/legnumber.jpg

     

    on this component from the library how do you know if the pin and gates are numbered as in the datasheet of the component?

     

    AB

     

     

     

    SET PAD ON or OFF

    or go to Options/Set/Misc menu and look for "Display pad names".

     

     

    --

    Mit freundlichen Gruessen / Best regards

    Richard Hammerl

      CadSoft Support -- hotline@cadsoft.de

      FAQ: http://www.cadsoft.de/faq.htm

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    as an example:

    http://i203.photobucket.com/albums/aa14/badbad214/Eagle/legnumber.jpg

     

    on this component from the library how do you know if the pin and gates are numbered as in the datasheet of the component?

     

    AB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Back on business Thank you Warren.

     

    Another question (tell em if I need a new post by the way):

    when I run the check I get warning on wires close but unconnected:

    http://i203.photobucket.com/albums/aa14/badbad214/Eagle/WiresNotConnected.jpg

     

    The fact that I put a junction should not have fixed the issue?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    badbad2142 wrote:

    I keep struggling but sure for no reason I must be doing something

    wrond becasue a component as simple as a resistor gives me issues:

     

    http://i203.photobucket.com/albums/aa14/badbad214/Eagle/R1_Position2.jp

    g[/IMG]

    >

    http://i203.photobucket.com/albums/aa14/badbad214/Eagle/R1_Position1.jp

    g[/IMG]

    As you can see my resistor (that I picked from the library) is

    oscillating between two posiitons AROUND the grid... I think that I

    have the snap on the grid function activated (I did Grid On command

    but not sure if it is the right one). I tried to move the component

    using the Alt but it does not stop right on the grid and the

    connection does not create itself. I did not chage the size of the

    grid... ?

     

    Hold the CTL  key down when you select the resistor. It will snap the

    resistor to your 0.1 grid

     

    HTH

    Warren

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    I keep struggling but sure for no reason I must be doing something wrond becasue a component as simple as a resistor gives me issues:

    [IMG]http://i203.photobucket.com/albums/aa14/badbad214/Eagle/R1_Position2.jpg[/IMG]

     

    [IMG]http://i203.photobucket.com/albums/aa14/badbad214/Eagle/R1_Position1.jpg[/IMG]

    As you can see my resistor (that I picked from the library) is oscillating between two posiitons AROUND the grid... I think that I have the snap on the grid function activated (I did Grid On command but not sure if it is the right one). I tried to move the component using the Alt but it does not stop right on the grid and the connection does not create itself. I did not chage the size of the grid...

    ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Thank you all for your help.

     

    Marius: I will try it right away.

     

    Gary: For the grid being french I went for mm which is may be not wise with some of the existing components of the library.

    My circuits are going to be home made (at least the first few to see if I can do something by myself) so coarse is ok for now. I will remember it for next time.

     

    Jorge: I have not tried yet and I will.

     

    Joerg: I am sad (but also veyr happy) to say that I am currently living in the US and undertsand perfectly what you mean concerning the cheese!!! Trust me...

     

    :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    Gary Gofstein wrote:

    On 3/18/2011 1:05 PM, Joerg wrote:

    >> badbad2142 wrote:

     

     

    >>> Now that I here one more question: Why do I struggle so much to have

    >>> a connection between my wire and my components? one time out of two

    >>> it does not requognize each other... is there a parameter to make

    >>> that more automatique?

    >>>

    >>

    >> As Marius hinted you might have veered slightly off the grid. When doing

    >> normal schematic drafting I suggest to keep "stay on grid" turned on and

    >> not set too fine a grid. It should be left at default or at least make

    >> it coarse enough so you can easily see the grid steps when moving a

    >> part, seeing a "ratchet" motion and not a smooth motion. Otherwise it

    >> can become impossible to see when a wire stopped a fraction of a

    >> millimeter from a component pin. That becomes worse the older you get image

    >>

    Our standard is to make sure all library pins are on the 0.100 inch

    grid, which is also what your grid should be set to in schematic editor.

    The board editor grid and the routing grid are totally seperate and can

    be set to whatever you want. Note that the default routing grid of 0.050

    is very coarse for modern circuits.

     

     

    Same here, schematics are all 0.1", with very few exceptions. I don't do

    layouts myself but guide them a lot. There the grid is nowadays more

    like 0.01, sometimes even smaller.

     

    Turning the grid off is only needed when you do fancy artwork with

    Eagle. Like birthday banners image

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    On 3/18/2011 1:05 PM, Joerg wrote:

    badbad2142 wrote:

    >> Thank you Joerg. Quoi comme frommage, un chevre par exemple? le

    >> boursin ne me dit rien pour l electronique...

    >>

    >

    I like both goat cheese and Boursin, even when doing electronic design image

     

    You guys live in paradise when it comes to cheese. The Camembert we can

    get in America is a far cry from the cheese I enjoyed in France (where

    you take a bite and your breath stops for a couple of seconds). Luckily

    we can buy Boursin.

     

    >

    >> I have been able to create my two first items in my library (thanks

    >> to kd7vnn

    >> http://www.instructables.com/id/How-to-make-a-custom-library-part-in-Eagle-CAD-too/).

    >>

    >>

    >> I undertsand what you say about 50% of the job but when you are just

    >> doing it once in a while it is a bruden... but it is ok.

    >>

    >

    That's the same with all software. I just finished my tax preparation

    (to give to the CPA). A law had changed which required me to do a minor

    database modification here. I struggled for almost an hour to do

    something rather simple.

     

    >

    >> Now that I here one more question: Why do I struggle so much to have

    >> a connection between my wire and my components? one time out of two

    >> it does not requognize each other... is there a parameter to make

    >> that more automatique?

    >>

    >

    As Marius hinted you might have veered slightly off the grid. When doing

    normal schematic drafting I suggest to keep "stay on grid" turned on and

    not set too fine a grid. It should be left at default or at least make

    it coarse enough so you can easily see the grid steps when moving a

    part, seeing a "ratchet" motion and not a smooth motion. Otherwise it

    can become impossible to see when a wire stopped a fraction of a

    millimeter from a component pin. That becomes worse the older you get image

     

    Our standard is to make sure all library pins are on the 0.100 inch

    grid, which is also what your grid should be set to in schematic editor.

    The board editor grid and the routing grid are totally seperate and can

    be set to whatever you want. Note that the default routing grid of 0.050

    is very coarse for modern circuits.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 15 years ago in reply to e14 Contributor

    badbad2142 wrote:

    Thank you Joerg. Quoi comme frommage, un chevre par exemple? le

    boursin ne me dit rien pour l electronique...

     

     

    I like both goat cheese and Boursin, even when doing electronic design image

     

    You guys live in paradise when it comes to cheese. The Camembert we can

    get in America is a far cry from the cheese I enjoyed in France (where

    you take a bite and your breath stops for a couple of seconds). Luckily

    we can buy Boursin.

     

     

    I have been able to create my two first items in my library (thanks

    to kd7vnn

    http://www.instructables.com/id/How-to-make-a-custom-library-part-in-Eagle-CAD-too/).

     

     

    I undertsand what you say about 50% of the job but when you are just

    doing it once in a while it is a bruden... but it is ok.

     

     

    That's the same with all software. I just finished my tax preparation

    (to give to the CPA). A law had changed which required me to do a minor

    database modification here. I struggled for almost an hour to do

    something rather simple.

     

     

    Now that I here one more question: Why do I struggle so much to have

    a connection between my wire and my components? one time out of two

    it does not requognize each other... is there a parameter to make

    that more automatique?

     

     

    As Marius hinted you might have veered slightly off the grid. When doing

    normal schematic drafting I suggest to keep "stay on grid" turned on and

    not set too fine a grid. It should be left at default or at least make

    it coarse enough so you can easily see the grid steps when moving a

    part, seeing a "ratchet" motion and not a smooth motion. Otherwise it

    can become impossible to see when a wire stopped a fraction of a

    millimeter from a component pin. That becomes worse the older you get image

     

    --

    Regards, Joerg

     

    http://www.analogconsultants.com/

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>