When I start my Eagle 5.11.0 I have to define the PROJECT directory every
time - it says it's not there, and when I click Yes to create, I get a
message that it can't be created.
When I go to Options/Directories then I CAN in fact see the right path, but
I HAVE to Browse and then click OK to get it to work right. When I do it
this way it works till the next time the machine has been shot down and
start again.
The project directory is on a NAS-drive and the other directories is on the
C-drive
What is wrong here ?
--
Best regards
KSor, Denmark
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.