If I install eagle on a linux or Mac SMP system, will it take advantage
of the multiple processors?
Thanks,
- Chuck
If I install eagle on a linux or Mac SMP system, will it take advantage
of the multiple processors?
Thanks,
- Chuck
Op Mon, 19 Sep 2011 15:00:14 +0200 schreef Chuck Huber
If I install eagle on a linux or Mac SMP system, will it take advantage
of the multiple processors?
To quote Cadsoft's Jorge Garcia from a thread a few days back: "... EAGLE
is exactly the same across all three major Os's. All of the muscle your
machines have is futile because EAGLE can't make use of multiple
cores(this is true of most commercial software today, parallization isn't
the easiest thing to manage)"
So I think the answer should be no.
HTH
Richard
Am 19.09.2011 19:40, schrieb Richard Herman:
Op Mon, 19 Sep 2011 15:00:14 +0200 schreef Chuck Huber
>> If I install eagle on a linux or Mac SMP system, will it take advantage
>> of the multiple processors?
To quote Cadsoft's Jorge Garcia from a thread a few days back: "...
EAGLE is exactly the same across all three major Os's. All of the muscle
your machines have is futile because EAGLE can't make use of multiple
cores(this is true of most commercial software today, parallization
isn't the easiest thing to manage)"
So I think the answer should be no.
HTH
Richard
Your answer is correct, EAGLE currently does not support more than
one core.
--
Mit freundlichen Gruessen / Best regards
Richard Hammerl
CadSoft Support -- hotline@cadsoft.de
FAQ: http://www.cadsoft.de/training/faq/
Am 19.09.2011 19:40, schrieb Richard Herman:
Op Mon, 19 Sep 2011 15:00:14 +0200 schreef Chuck Huber
>> If I install eagle on a linux or Mac SMP system, will it take advantage
>> of the multiple processors?
To quote Cadsoft's Jorge Garcia from a thread a few days back: "...
EAGLE is exactly the same across all three major Os's. All of the muscle
your machines have is futile because EAGLE can't make use of multiple
cores(this is true of most commercial software today, parallization
isn't the easiest thing to manage)"
So I think the answer should be no.
HTH
Richard
Your answer is correct, EAGLE currently does not support more than
one core.
--
Mit freundlichen Gruessen / Best regards
Richard Hammerl
CadSoft Support -- hotline@cadsoft.de
FAQ: http://www.cadsoft.de/training/faq/
Chuck Huber <chuck.huber@dukepro.com> wrote:
On 09/20/2011 07:10 AM, Richard Hammerl wrote:
Am 19.09.2011 19:40, schrieb Richard Herman:
>> Op Mon, 19 Sep 2011 15:00:14 +0200 schreef Chuck Huber
>> <chuck.huber@dukepro.com>:
>>
>>> If I install eagle on a linux or Mac SMP system, will it take advantage
>>> of the multiple processors?
>>
>> To quote Cadsoft's Jorge Garcia from a thread a few days back: "...
>> EAGLE is exactly the same across all three major Os's.
...
>> So I think the answer should be no.
...
Your answer is correct, EAGLE currently does not support more than
one core.
Hmmm... Interesting... Come to think of it, there aren't many places
where multiple threads are needed. I could see multiple threads when
rendering layers then alpha blend the multiple results into one
display. I can also see multi thread use when running CAM jobs - one
per section. But for the most part, eagle runs at the user's speed.
Wise use of an AGP would probably be the best area in which to focus
speed-up efforts.
Online DRC check in the vincinity of the thing you move/draw would be
of great help...
--
Uwe Bonnes bon@elektron.ikp.physik.tu-darmstadt.de
Institut fuer Kernphysik Schlossgartenstrasse 9 64289 Darmstadt
-
Tel. 06151 162516 -
Fax. 06151 164321 -
On 09/20/2011 07:10 AM, Richard Hammerl wrote:
Am 19.09.2011 19:40, schrieb Richard Herman:
>> Op Mon, 19 Sep 2011 15:00:14 +0200 schreef Chuck Huber
>> <chuck.huber@dukepro.com>:
>>
>>> If I install eagle on a linux or Mac SMP system, will it take advantage
>>> of the multiple processors?
>>
>> To quote Cadsoft's Jorge Garcia from a thread a few days back: "...
>> EAGLE is exactly the same across all three major Os's.
...
>> So I think the answer should be no.
...
Your answer is correct, EAGLE currently does not support more than
one core.
Hmmm... Interesting... Come to think of it, there aren't many places
where multiple threads are needed. I could see multiple threads when
rendering layers then alpha blend the multiple results into one
display. I can also see multi thread use when running CAM jobs - one
per section. But for the most part, eagle runs at the user's speed.
Wise use of an AGP would probably be the best area in which to focus
speed-up efforts.
POSIX threads and POSIX mutexes are supported on all three platforms,
but as was mentioned earlier, handling multiple threads is a non-trivial
matter.
Enjoy,
- Chuck