Hi,
How to you JOIN the two ground VSS & GND signals? without having one net
name?
Thanks Dave M
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
Hi,
How to you JOIN the two ground VSS & GND signals? without having one net
name?
Thanks Dave M
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
On 12/04/2011 10:22 PM, davem wrote:
Hi,
How to you JOIN the two ground VSS & GND signals? without having one net
name?
Thanks Dave M
Dave,
The easiest way it to create a library part called "connector" or
"short". Such a device has two SMD pads that overlap, and a symbol with
two pins that just connect to each other.
You'll get a DRC error with the pads, and maybe even with traces that
approach it, but they're easy enough to approve.
I've attached a shorts library. I believe Olin originally made this,
but I wouldn't swear to it. If you use the SMD package, be sure to edit
the library to get rid of the solder paste layer and optionally the
solder mask layer. You can do this by editing each SMD pad and turn the
Cream and Mask flags off.
Enjoy,
- Chuck
| shorts-old.lbr.zip |
On 12/05/2011 08:38 AM, Chuck Huber wrote:
On 12/04/2011 10:22 PM, davem wrote:
>> Hi,
>>
>>
>> How to you JOIN the two ground VSS & GND signals? without having one net
>> name?
The shorts devices have come in handy when you need to keep an analog
ground separate from a digital ground. Since they're treated as
separate nets in Eagle, one can place the short close to your star
ground point.
- Chuck
Hi Chuck,
Thanks for the reply,
I forgot to mention I need to "JOIN" these two polygon "grounds" with
VIA's. Many of them, which also act as a heat sink.
My grounds Connect at a voltage regulators ground plan ( as suggested by
the manufacturers specifications.
I have done ALL my design/layout work, except for the "Joins"
One ground is the top layer, the other is the bottom,
I checked out the Shorting links, I have seen those before, but that wont
work for my design.
The only thing I can think off is the RENAME my "analog ground" to "VSS",
and then my vias will work, but that make my schematics incorrect, and is
this was done before layout started I would of had a great big mess.!
I believe this is a short coming of eaglecad, and a fix for this problem
needs to be addressed, has this been discussed before?
We need a "JOINING VIA" or even someway of joining to different nets.
Thanks
Dave M
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
Hi Chuck,
Thanks for the reply,
I forgot to mention I need to "JOIN" these two polygon "grounds" with
VIA's. Many of them, which also act as a heat sink.
My grounds Connect at a voltage regulators ground plan ( as suggested by
the manufacturers specifications.
I have done ALL my design/layout work, except for the "Joins"
One ground is the top layer, the other is the bottom,
I checked out the Shorting links, I have seen those before, but that wont
work for my design.
The only thing I can think off is the RENAME my "analog ground" to "VSS",
and then my vias will work, but that make my schematics incorrect, and is
this was done before layout started I would of had a great big mess.!
I believe this is a short coming of eaglecad, and a fix for this problem
needs to be addressed, has this been discussed before?
We need a "JOINING VIA" or even someway of joining to different nets.
Thanks
Dave M
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
On 12/5/2011 5:10 PM, davem wrote:
Hi Chuck,
Thanks for the reply,
I forgot to mention I need to "JOIN" these two polygon "grounds" with
VIA's. Many of them, which also act as a heat sink.
My grounds Connect at a voltage regulators ground plan ( as suggested by
the manufacturers specifications.
I have done ALL my design/layout work, except for the "Joins"
One ground is the top layer, the other is the bottom,
I checked out the Shorting links, I have seen those before, but that wont
work for my design.
>
The only thing I can think off is the RENAME my "analog ground" to "VSS",
and then my vias will work, but that make my schematics incorrect, and is
this was done before layout started I would of had a great big mess.!
I believe this is a short coming of eaglecad, and a fix for this problem
needs to be addressed, has this been discussed before?
We need a "JOINING VIA" or even someway of joining to different nets.
Thanks
Dave M
>
Hi Dave,
Another solution is to just overlap the polygons at a single point, it
will generate a single DRC overlap error but will get you the result you
want. This will work as long as both polygons have the same rank, if
they have different ranks then one will subtract from the other which is
not what you intend in this case. This is probably the best solution for
you particular scenario, sometimes you have to violate DRC to get what
you want done.
Best Regards,
Jorge Garcia
Cadsoft Support
davem wrote:
Hi Chuck,
Thanks for the reply,
I forgot to mention I need to "JOIN" these two polygon "grounds" with
VIA's. Many of them, which also act as a heat sink.
My grounds Connect at a voltage regulators ground plan ( as suggested
by the manufacturers specifications.
I have done ALL my design/layout work, except for the "Joins"
One ground is the top layer, the other is the bottom,
I checked out the Shorting links, I have seen those before, but that
wont work for my design.
There is another way that my be of interest.
Consider the following:
Instead of a VIA place a HOLE.
The next consideration is that a polygon will keep away from the edge of
that hole by the mount set in the DRC (Keeps away from all in the dimension
layer)
Now define a user layer and using that place a patch (rect circle etc) over
the hole. That layer needs to be included when making the top and bottom
gerbers.
This would result in a plated through hole at most board houses.
You could create the above as a 'fake via' package that you add to the board
in place of a via. As there is no device, you can do this while working with
a consistant schem/brd pair.
This keeps the hole and patch locked together so that they move together.
The above technique is probably best limited to 2 layer boards and you do
have to remember the extra layer to include in the gerber.
HTH
Warren
--
Viewed / responded via the newsgroup at
news.cadsoft.de
HI Warren,
I SOLVED IT!
You can't do this with some kind of via or custom part, I tried, but the
hole wants to create its own mask, no matter how you set it.
How I fixed it,
I think it was suggested somewhere before, but I split the ground plane in
two, then , for where my vias go, I name that ground plane to match "VSS",
its was "GND" before, Now I have a small polygon overlap, for both the GND
& VSS ground planes, they will join as far as copper is concerned, and it
does show up an error in the DRC, but who cares!
thanks for everyone's help.
I still think cadsoft need to make this easier for us.
dave M
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
HI George,
Your idea worked, and would you believe I have done this before! but I
could not remember!
thanks mate!
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.