EAGLE User Support (English) How to you JOIN  two grounds, i.e VSS   & GND signals?
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
  • Replies 16 replies
  • Subscribers 183 subscribers
  • Views 4997 views
  • Users 0 members are here
Related

How to you JOIN  two grounds, i.e VSS   & GND signals?

Former Member
Former Member over 14 years ago

Hi,

 

 

How to you JOIN the two ground VSS & GND signals? without having one net

name?

 

Thanks Dave M

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • dukepro
    dukepro over 14 years ago

    On 12/04/2011 10:22 PM, davem wrote:

    Hi,

     

     

    How to you JOIN the two ground VSS & GND signals? without having one net

    name?

     

    Thanks Dave M

     

    Dave,

     

    The easiest way it to create a library part called "connector" or

    "short".  Such a device has two SMD pads that overlap, and a symbol with

    two pins that just connect to each other.

     

    You'll get a DRC error with the pads, and maybe even with traces that

    approach it, but they're easy enough to approve.

     

    I've attached a shorts library.  I believe Olin originally made this,

    but I wouldn't swear to it.  If you use the SMD package, be sure to edit

    the library to get rid of the solder paste layer and optionally the

    solder mask layer.  You can do this by editing each SMD pad and turn the

    Cream and Mask flags off.

     

    Enjoy,

        - Chuck

     

    Attachments:
    shorts-old.lbr.zip
    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 14 years ago in reply to dukepro

    On 12/05/2011 08:38 AM, Chuck Huber wrote:

    On 12/04/2011 10:22 PM, davem wrote:

    >> Hi,

    >>

    >>

    >> How to you JOIN the two ground VSS & GND signals? without having one net

    >> name?

     

    The shorts devices have come in handy when you need to keep an analog

    ground separate from a digital ground.  Since they're treated as

    separate nets in Eagle, one can place the short close to your star

    ground point.

     

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to dukepro

    Hi Chuck,

     

    Thanks for the reply,

     

    I forgot to mention I need to "JOIN" these two polygon "grounds" with

    VIA's. Many of them, which also act as a heat sink.

     

    My grounds Connect at a voltage regulators ground plan ( as suggested by

    the manufacturers specifications.

     

    I have done ALL my design/layout work, except for the "Joins"

     

    One ground is the top layer, the other is the bottom,

     

    I checked out the Shorting links, I have seen those before, but that wont

    work for my design.

     

     

    The only thing I can think off is the RENAME my "analog ground" to "VSS",

    and then my vias will work, but that make my schematics incorrect, and is

    this was done before layout started I would of had a great big mess.!

     

    I believe this is a short coming of eaglecad, and a fix for this problem

    needs to be addressed, has this been discussed before?

     

    We need a "JOINING VIA" or even someway of joining to different nets.

     

    Thanks

     

    Dave M

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    On 12/5/2011 5:10 PM, davem wrote:

    Hi Chuck,

     

    Thanks for the reply,

     

    I forgot to mention I need to "JOIN" these two polygon "grounds" with

    VIA's. Many of them, which also act as a heat sink.

     

    My grounds Connect at a voltage regulators ground plan ( as suggested by

    the manufacturers specifications.

     

    I have done ALL my design/layout work, except for the "Joins"

     

    One ground is the top layer, the other is the bottom,

     

    I checked out the Shorting links, I have seen those before, but that wont

    work for my design.

     

    >

    The only thing I can think off is the RENAME my "analog ground" to "VSS",

    and then my vias will work, but that make my schematics incorrect, and is

    this was done before layout started I would of had a great big mess.!

     

    I believe this is a short coming of eaglecad, and a fix for this problem

    needs to be addressed, has this been discussed before?

     

    We need a "JOINING VIA" or even someway of joining to different nets.

     

    Thanks

     

    Dave M

     

    >

     

    Hi Dave,

     

    Another solution is to just overlap the polygons at a single point, it

    will generate a single DRC overlap error but will get you the result you

    want. This will work as long as both polygons have the same rank, if

    they have different ranks then one will subtract from the other which is

    not what you intend in this case. This is probably the best solution for

    you particular scenario, sometimes you have to violate DRC to get what

    you want done.

     

    Best Regards,

     

    Jorge Garcia

    Cadsoft Support

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    On 12/5/2011 5:10 PM, davem wrote:

    Hi Chuck,

     

    Thanks for the reply,

     

    I forgot to mention I need to "JOIN" these two polygon "grounds" with

    VIA's. Many of them, which also act as a heat sink.

     

    My grounds Connect at a voltage regulators ground plan ( as suggested by

    the manufacturers specifications.

     

    I have done ALL my design/layout work, except for the "Joins"

     

    One ground is the top layer, the other is the bottom,

     

    I checked out the Shorting links, I have seen those before, but that wont

    work for my design.

     

    >

    The only thing I can think off is the RENAME my "analog ground" to "VSS",

    and then my vias will work, but that make my schematics incorrect, and is

    this was done before layout started I would of had a great big mess.!

     

    I believe this is a short coming of eaglecad, and a fix for this problem

    needs to be addressed, has this been discussed before?

     

    We need a "JOINING VIA" or even someway of joining to different nets.

     

    Thanks

     

    Dave M

     

    >

     

    Hi Dave,

     

    Another solution is to just overlap the polygons at a single point, it

    will generate a single DRC overlap error but will get you the result you

    want. This will work as long as both polygons have the same rank, if

    they have different ranks then one will subtract from the other which is

    not what you intend in this case. This is probably the best solution for

    you particular scenario, sometimes you have to violate DRC to get what

    you want done.

     

    Best Regards,

     

    Jorge Garcia

    Cadsoft Support

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • Former Member
    Former Member over 14 years ago in reply to Former Member

    HI George, 

     

    Your idea worked, and would you believe I have done this before! but I

    could not remember!

     

    thanks mate!

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.