Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) via's, polygons and cutouts
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 188 subscribers
  • Views 428 views
  • Users 0 members are here
Related

via's, polygons and cutouts

e14 Contributor
e14 Contributor over 14 years ago

New to eagle along with the fact that the last time I ever laid out a board

we were still using tape and pads. :d   So far things are going well but I

have a few questions.

 

1. Via's with SMD parts. when connecting two SMD parts on direct opposite

sides of a board and who's pads line up, in this case two 5050 LED's, can

you place a via, or the plate through hold, on the pad? I hate to loose the

lanes just to place a full via pad.

 

2. Polygons for power and ground on a two sided board. Can I use the

polygon to interconnect the power and grounds to components? I'd like to

know keep putting in traces and just let the polygon connect them.

 

3. Cutouts. I have a large hole that need to be cut in the middle of the

board so part of a component can go though it. What's the best way to do

this?

 

4. Can eagle panelize or is that best left to the vendor?

 

Thanks

 

John

 

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    John Warren schrieb:

     

    New to eagle along with the fact that the last time I ever laid out a board

    we were still using tape and pads. :d   So far things are going well but I

    have a few questions.

     

    First of all: welcome. image

     

    1. Via's with SMD parts. when connecting two SMD parts on direct opposite

    sides of a board and who's pads line up, in this case two 5050 LED's, can

    you place a via, or the plate through hold, on the pad? I hate to loose the

    lanes just to place a full via pad.

     

    If you put vias inside of SMD pads, they will drain the solder paste

    during reflow process unless you let the boardhouse "plug" (fill) them,

    which is more expensive. It's good practice to keep vias separate from

    pads (so that some solder stop mask is inbetween).

     

    If you're soldering manually, you might accept vias in pads, however.

     

    2. Polygons for power and ground on a two sided board. Can I use the

    polygon to interconnect the power and grounds to components? I'd like to

    know keep putting in traces and just let the polygon connect them.

     

    Yes, you can use polygons to also provide connections - however take

    care that a) you reach all desired pads, and b) you always know where

    the current paths are (think of EMV). It's always good to keep the

    complete design in mind during the whole routing process...

     

    3. Cutouts. I have a large hole that need to be cut in the middle of the

    board so part of a component can go though it. What's the best way to do

    this?

     

    Simply draw the desired outline information in the dimension layer. I

    always recommend to draw it also in the milling layer, using really thin

    wires - that's for providing the contour data to the board house without

    the implicit circles of illegal width that are generated in the

    dimension layer for holes.

     

    4. Can eagle panelize or is that best left to the vendor?

     

    Yes, it can, and I always do it myself and provide exact and complete

    data to the board house. Of course they can also panelize the boards for

    you. Talk to them for their preference and pricing...

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Tilmann Reh wrote on Thu, 08 December 2011 12:53

    John Warren schrieb:

     

    First of all: welcome. image

     

    Thanks

     

    If you put vias inside of SMD pads, they will drain the solder paste

    during reflow process unless you let the boardhouse "plug" (fill)

    them,

    which is more expensive. It's good practice to keep vias separate from

    pads (so that some solder stop mask is in-between).

     

    If you're soldering manually, you might accept vias in pads, however.

     

    For now I'll just push the via up tight to the pad and accept the

    clearance error. I must say that working with SMDs is really different.

     

    I'm used to running traces between pads but that's not an option with

    TSSOP and the like as the pads aren't much wider than the traces and the

    spacing is about the same as a trace.

     

    It's going to be fun hand building my prototypes. :d  I may even have

    to purchase a new solder station.

     

    Do you happen to have a link to a good tutorial on building boards with

    SMD so I can brush up?

     

    Yes, you can use polygons to also provide connections - however take

    care that a) you reach all desired pads, and b) you always know

    where

    the current paths are (think of EMV). It's always good to keep the

    complete design in mind during the whole routing process...

     

    Likely best to just connect then up then add the poly afterwards.

     

    Simply draw the desired outline information in the dimension layer. I

    always recommend to draw it also in the milling layer, using really

    thin

    wires - that's for providing the contour data to the board house

    without

    the implicit circles of illegal width that are generated in the

    dimension layer for holes.

     

    I'll give that a try.

     

    When you have a polygon on both sides of the board tied to the same

    signal name, i.e., GND, is it more acceptable to just drop a hole to

    connect them rather than a VIA?

     

    Yes, it can, and I always do it myself and provide exact and complete

    data to the board house. Of course they can also panelize the boards

    for

    you. Talk to them for their preference and pricing...

     

    Likely best if the board how does it for now as it wouldn't take many

    repeats to go a larger board than my version allows. I'll just have make

    sure the repeat information get back to me for the pick and place machine

    to use.

     

    Tilmann

     

     

    Again thanks

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hello John,

     

    please take care of correct quoting - your answers can't be

    distinguished from my previous post, which makes it rather hard to read

    and understand. (I'm fixing the quote levels below.)

     

    >> If you put vias inside of SMD pads, they will drain the solder

    >> paste during reflow process unless you let the boardhouse "plug"

    >> (fill) them, which is more expensive. It's good practice to keep

    >> vias separate from pads (so that some solder stop mask is

    >> in-between).

    >>

    >> If you're soldering manually, you might accept vias in pads, however.

     

    For now I'll just push the via up tight to the pad and accept the

    clearance error. I must say that working with SMDs is really different.

     

    Yes, if you didn't use SMD before, you will have to get used to it...

    It's a little bit more like routing a single sided board, making good

    placement really essential. Take the time needed to properly place the

    parts.

     

    If you know you're going to use ground polygons, disable the display of

    ground airwires ("ratsnest ! gnd") at first. However, take care to leave

    enough room for the gnd vias that are needed later...

     

    I'm used to running traces between pads but that's not an option with

    TSSOP and the like as the pads aren't much wider than the traces and the

    spacing is about the same as a trace.

     

    With SMD, normally no traces are run between pads at a pitch less than

    1.27 mm (50 mil - standard SO). This makes placement even more essential.

     

    It's going to be fun hand building my prototypes. :d  I may even have

    to purchase a new solder station.

     

    Do you happen to have a link to a good tutorial on building boards with

    SMD so I can brush up?

     

    I don't know which soldering station you currently have, but provided

    it's a good one with decent temperature regulation, you might at first

    simply try a suitable tip.

     

    For soldering SMD ICs, even fine pitch, here is a very good tutorial

    video: <http://www.youtube.com/watch?v=wQXhny3R7lk>

    You simply don't need to solder all the pads separately, in case you had

    feared that. image

     

    >> Yes, you can use polygons to also provide connections - however

    >> take care that a) you reach all desired pads, and b) you always

    >> know where the current paths are (think of EMV). It's always good

    >> to keep the complete design in mind during the whole routing

    >> process...

     

    Likely best to just connect then up then add the poly afterwards.

     

    That heavily depends on the circuit and placement... If you know that

    there will be a gnd polygon covering about the whole solder side (except

    for say a few short slots), you can simply hide the gnd airwires and

    route the signals. Afterwards, enable the gnd airwires, draw your

    polygon, and connect the gnd (with vias to the polygon wherever needed

    and/or possible).

     

    For using polygons and signals on both copper layers, strategy is

    different. Take care to finally get a good gnd "mesh" covering the whole

    board, by connecting the two polygons more or less regularly with vias.

     

    (Hint: if you just drop vias in there, they will get their own signal

    names and thus not be connected to the polygons. They need to have the

    same signal name as the polygon, you can "rename" them with NAME. Or,

    much easier: simply enter "via gnd" and then drop them where needed...)

     

    When you have a polygon on both sides of the board tied to the same

    signal name, i.e., GND, is it more acceptable to just drop a hole to

    connect them rather than a VIA?

     

    No, you need to use VIAs. HOLEs are electrically insulated and just for

    mechanical purposes (mounting of larger parts, or the board itself).

    Observe the difference after doing a ratsnest (polygon recalculation).

     

    >> Yes, it can, and I always do it myself and provide exact and complete

    >> data to the board house. Of course they can also panelize the boards

    >> for

    >> you. Talk to them for their preference and pricing...

     

    Likely best if the board how does it for now as it wouldn't take many

    repeats to go a larger board than my version allows. I'll just have make

    sure the repeat information get back to me for the pick and place machine

    to use.

     

    P&P machines normally support panelizing by themselves. You just need

    the P&P data for a single board, then add information about board count

    and offsets in the panel.

     

    Tilmann

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hello John,

     

    please take care of correct quoting - your answers can't be

    distinguished from my previous post, which makes it rather hard to read

    and understand. (I'm fixing the quote levels below.)

     

    >> If you put vias inside of SMD pads, they will drain the solder

    >> paste during reflow process unless you let the boardhouse "plug"

    >> (fill) them, which is more expensive. It's good practice to keep

    >> vias separate from pads (so that some solder stop mask is

    >> in-between).

    >>

    >> If you're soldering manually, you might accept vias in pads, however.

     

    For now I'll just push the via up tight to the pad and accept the

    clearance error. I must say that working with SMDs is really different.

     

    Yes, if you didn't use SMD before, you will have to get used to it...

    It's a little bit more like routing a single sided board, making good

    placement really essential. Take the time needed to properly place the

    parts.

     

    If you know you're going to use ground polygons, disable the display of

    ground airwires ("ratsnest ! gnd") at first. However, take care to leave

    enough room for the gnd vias that are needed later...

     

    I'm used to running traces between pads but that's not an option with

    TSSOP and the like as the pads aren't much wider than the traces and the

    spacing is about the same as a trace.

     

    With SMD, normally no traces are run between pads at a pitch less than

    1.27 mm (50 mil - standard SO). This makes placement even more essential.

     

    It's going to be fun hand building my prototypes. :d  I may even have

    to purchase a new solder station.

     

    Do you happen to have a link to a good tutorial on building boards with

    SMD so I can brush up?

     

    I don't know which soldering station you currently have, but provided

    it's a good one with decent temperature regulation, you might at first

    simply try a suitable tip.

     

    For soldering SMD ICs, even fine pitch, here is a very good tutorial

    video: <http://www.youtube.com/watch?v=wQXhny3R7lk>

    You simply don't need to solder all the pads separately, in case you had

    feared that. image

     

    >> Yes, you can use polygons to also provide connections - however

    >> take care that a) you reach all desired pads, and b) you always

    >> know where the current paths are (think of EMV). It's always good

    >> to keep the complete design in mind during the whole routing

    >> process...

     

    Likely best to just connect then up then add the poly afterwards.

     

    That heavily depends on the circuit and placement... If you know that

    there will be a gnd polygon covering about the whole solder side (except

    for say a few short slots), you can simply hide the gnd airwires and

    route the signals. Afterwards, enable the gnd airwires, draw your

    polygon, and connect the gnd (with vias to the polygon wherever needed

    and/or possible).

     

    For using polygons and signals on both copper layers, strategy is

    different. Take care to finally get a good gnd "mesh" covering the whole

    board, by connecting the two polygons more or less regularly with vias.

     

    (Hint: if you just drop vias in there, they will get their own signal

    names and thus not be connected to the polygons. They need to have the

    same signal name as the polygon, you can "rename" them with NAME. Or,

    much easier: simply enter "via gnd" and then drop them where needed...)

     

    When you have a polygon on both sides of the board tied to the same

    signal name, i.e., GND, is it more acceptable to just drop a hole to

    connect them rather than a VIA?

     

    No, you need to use VIAs. HOLEs are electrically insulated and just for

    mechanical purposes (mounting of larger parts, or the board itself).

    Observe the difference after doing a ratsnest (polygon recalculation).

     

    >> Yes, it can, and I always do it myself and provide exact and complete

    >> data to the board house. Of course they can also panelize the boards

    >> for

    >> you. Talk to them for their preference and pricing...

     

    Likely best if the board how does it for now as it wouldn't take many

    repeats to go a larger board than my version allows. I'll just have make

    sure the repeat information get back to me for the pick and place machine

    to use.

     

    P&P machines normally support panelizing by themselves. You just need

    the P&P data for a single board, then add information about board count

    and offsets in the panel.

     

    Tilmann