Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) in V6.0.0 manual routing got really hard
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 190 subscribers
  • Views 4691 views
  • Users 0 members are here
Related

in V6.0.0 manual routing got really hard

e14 Contributor
e14 Contributor over 14 years ago

somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires

5.11 didnt do this... i have messed with alot of settings, nothing seems to help

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 12/16/2011 12:55 PM, Mitch Solomon wrote:

    somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires

    5.11 didnt do this... i have messed with alot of settings, nothing seems to help

     

     

    Check your catch factor and select factor settings, by default they

    should be 5% and 2% respectively. Perhaps on a MAC this is different or

    the OS interprets the values differently it may be worth playing with

    them to get everything working nicely. Try 7% and 3% or maybe 8% and 4%.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Guest wrote:

     

    On 12/16/2011 12:55 PM, Mitch Solomon wrote:

    somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires

    5.11 didnt do this... i have messed with alot of settings, nothing seems to help

     

     

    Check your catch factor and select factor settings, by default they

    should be 5% and 2% respectively. Perhaps on a MAC this is different or

    the OS interprets the values differently it may be worth playing with

    them to get everything working nicely. Try 7% and 3% or maybe 8% and 4%.

     

    hth,

    Jorge Garcia

     

     

    It's not that - you can zoom in all you want, and virtually hover over the exact centre of the pad, and it won't "ping" to let you know it's connected.

     

    It even happens if you route a wire into another wire - if the other wire is on the grid, it doesn't think you've finished, so you have to double-click to stop it carrying on.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Just tried it in 6.0.2 (beta version) - still broken.

     

    Steps to reproduce:

     

    1. Move component with air wires connected to pads
    2. Manually route to one of the component's pad from another one

     

    It's easier to reproduce if the component's pads aren't on the grid.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    No problem!

     

    http://www.tribbeck.com/misc/Test5_11_0.zip is the URL for this.

     

    It's not an exact match in terms of the original layout, but it behaves exactly the same when loaded into 6.0.0 (can't manually route after rotating Q1), and works correctly on 5.11.0.

     

    btw, I used to run the support team for my company (which is also a software developer), so I know how useful it is to have these kind of files for developers. I'm now one of the developers (I was beforehand - just my project got cancelled, and they needed someone to run support...)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 12/28/2011 1:37 PM, Jason Tribbeck wrote:

    No problem, Jorge.

     

    Do you still want a V5 version? (Now I'm at home, I've got time to prepare one as well).

     

    The only other issue I've got is a MacOS X one, which I posted in the "Is there a list of open issues?" thread. That one shouldn't be too hard to see and fix image But I'll leave that for you to comment on that thread instead of this one (I know you're reading this one, so it's really just a bit of a prompt!)

     

     

    Hi Jason,

     

    If you don't mind prepare a V5 variant and put everything together in

    the test.zip file that way the developers have access to everything and

    we can make they're jobs as easy as possible.

     

    I'll go look at the other thread.

     

    Thanks again.

     

    Jorge

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    No problem, Jorge.

     

    Do you still want a V5 version? (Now I'm at home, I've got time to prepare one as well).

     

    The only other issue I've got is a MacOS X one, which I posted in the "Is there a list of open issues?" thread. That one shouldn't be too hard to see and fix image But I'll leave that for you to comment on that thread instead of this one (I know you're reading this one, so it's really just a bit of a prompt!)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 12/28/2011 3:49 AM, Jason Tribbeck wrote:

    Hi,

     

    Okay - it also happens in the Windows version as well. Unfortunately, I don't have a v5 format file (I'll need to switch the directories back over, and I really should be working at work image ), but I've made it available (since I'm not NNTP, I don't have your email address, so it's on my web site).

     

    http://www.tribbeck.com/misc/test.zip

     

    This is a zip of my Eagle project directory, and contains the schematic and board files. It's a simple LED driver circuit that I've thrown together.

     

    This is reproducable using the following command:

     

    ROTATE =MR45 Q1

     

    Then, try and manually route the signal from SV1 pin 1 to pin 1 of Q1.

     

    I'm pretty sure it's never happened on 5.x.

     

     

    Awesome Jason,

     

    Thanks for preparing this, I'll forward this to our developers and

    hopefully they can get on it for the next beta.

     

    Thanks again for helping, and I apologize for the delay in getting to

    you with the release of V6 it's been very crazy around here.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi,

     

    Okay - it also happens in the Windows version as well. Unfortunately, I don't have a v5 format file (I'll need to switch the directories back over, and I really should be working at work image ), but I've made it available (since I'm not NNTP, I don't have your email address, so it's on my web site).

     

    http://www.tribbeck.com/misc/test.zip

     

    This is a zip of my Eagle project directory, and contains the schematic and board files. It's a simple LED driver circuit that I've thrown together.

     

    This is reproducable using the following command:

     

    ROTATE =MR45 Q1

     

    Then, try and manually route the signal from SV1 pin 1 to pin 1 of Q1.

     

    I'm pretty sure it's never happened on 5.x.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi,

     

    Many thanks for the response.

     

    Since I'm back at work today, I'll need to get these this evening.

     

    However, I have downloaded the Windows version, so I'll see if I can reproduce it here.

     

    The reproduction was a little annoying in that some times I was able to reproduce it easily, started to record and found it worked fine. Or, if I loaded in my example from a fresh start, it wouldn't do it for a while.

     

    But it doesn't take longer than 2 minutes of doing and undoing (which might be part of the problem) stuff before it shows its head - so I don't think it's hard to reproduce.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi,

     

    Many thanks for the response.

     

    Since I'm back at work today, I'll need to get these this evening.

     

    However, I have downloaded the Windows version, so I'll see if I can reproduce it here.

     

    The reproduction was a little annoying in that some times I was able to reproduce it easily, started to record and found it worked fine. Or, if I loaded in my example from a fresh start, it wouldn't do it for a while.

     

    But it doesn't take longer than 2 minutes of doing and undoing (which might be part of the problem) stuff before it shows its head - so I don't think it's hard to reproduce.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    No problem!

     

    http://www.tribbeck.com/misc/Test5_11_0.zip is the URL for this.

     

    It's not an exact match in terms of the original layout, but it behaves exactly the same when loaded into 6.0.0 (can't manually route after rotating Q1), and works correctly on 5.11.0.

     

    btw, I used to run the support team for my company (which is also a software developer), so I know how useful it is to have these kind of files for developers. I'm now one of the developers (I was beforehand - just my project got cancelled, and they needed someone to run support...)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 12/28/2011 1:37 PM, Jason Tribbeck wrote:

    No problem, Jorge.

     

    Do you still want a V5 version? (Now I'm at home, I've got time to prepare one as well).

     

    The only other issue I've got is a MacOS X one, which I posted in the "Is there a list of open issues?" thread. That one shouldn't be too hard to see and fix image But I'll leave that for you to comment on that thread instead of this one (I know you're reading this one, so it's really just a bit of a prompt!)

     

     

    Hi Jason,

     

    If you don't mind prepare a V5 variant and put everything together in

    the test.zip file that way the developers have access to everything and

    we can make they're jobs as easy as possible.

     

    I'll go look at the other thread.

     

    Thanks again.

     

    Jorge

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    No problem, Jorge.

     

    Do you still want a V5 version? (Now I'm at home, I've got time to prepare one as well).

     

    The only other issue I've got is a MacOS X one, which I posted in the "Is there a list of open issues?" thread. That one shouldn't be too hard to see and fix image But I'll leave that for you to comment on that thread instead of this one (I know you're reading this one, so it's really just a bit of a prompt!)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 12/28/2011 3:49 AM, Jason Tribbeck wrote:

    Hi,

     

    Okay - it also happens in the Windows version as well. Unfortunately, I don't have a v5 format file (I'll need to switch the directories back over, and I really should be working at work image ), but I've made it available (since I'm not NNTP, I don't have your email address, so it's on my web site).

     

    http://www.tribbeck.com/misc/test.zip

     

    This is a zip of my Eagle project directory, and contains the schematic and board files. It's a simple LED driver circuit that I've thrown together.

     

    This is reproducable using the following command:

     

    ROTATE =MR45 Q1

     

    Then, try and manually route the signal from SV1 pin 1 to pin 1 of Q1.

     

    I'm pretty sure it's never happened on 5.x.

     

     

    Awesome Jason,

     

    Thanks for preparing this, I'll forward this to our developers and

    hopefully they can get on it for the next beta.

     

    Thanks again for helping, and I apologize for the delay in getting to

    you with the release of V6 it's been very crazy around here.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi,

     

    Okay - it also happens in the Windows version as well. Unfortunately, I don't have a v5 format file (I'll need to switch the directories back over, and I really should be working at work image ), but I've made it available (since I'm not NNTP, I don't have your email address, so it's on my web site).

     

    http://www.tribbeck.com/misc/test.zip

     

    This is a zip of my Eagle project directory, and contains the schematic and board files. It's a simple LED driver circuit that I've thrown together.

     

    This is reproducable using the following command:

     

    ROTATE =MR45 Q1

     

    Then, try and manually route the signal from SV1 pin 1 to pin 1 of Q1.

     

    I'm pretty sure it's never happened on 5.x.