somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires
5.11 didnt do this... i have messed with alot of settings, nothing seems to help
somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires
5.11 didnt do this... i have messed with alot of settings, nothing seems to help
Am 16.12.2011 18:55, schrieb Mitch Solomon:
somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires
5.11 didnt do this... i have messed with alot of settings, nothing seems to help
Gentlemen, so far I have followed all this postings and noticed that
there is is very little information about what machine and operating
system you are using.
I think to mention this would be a great help for cadsoft in eliminating
these errors.
I don't have this error on my windows xp sp3.
--
Mit freundlichen Grüßen / With best regards
Joern Paschedag
On 12/01/2012 13:36, Joern Paschedag wrote:
Am 16.12.2011 18:55, schrieb Mitch Solomon:
>> somethings changed, when i manually route and click on the destination
>> pad, if i dont click dead center now... im left with tiny tiny airwires
>> 5.11 didnt do this... i have messed with alot of settings, nothing
>> seems to help
>>
>
Gentlemen, so far I have followed all this postings and noticed that
there is is very little information about what machine and operating
system you are using.
I think to mention this would be a great help for cadsoft in eliminating
these errors.
I don't have this error on my windows xp sp3.
Using the files linked-to in this thread I can reproduce the fault under
Eagle 6.0.0 and Eagle 6.0.2 in Windows 7 x64.
I was also seeing this leftover airwires problem on Linux x64 (but with
a different (production!) board) using 6.0.0.
The exchange of messages in this thread, between Jorge Garcia and Jason
Tribbeck, suggests that the developers have all they need to be able to
reproduce this.
Hopefully 6.1 will nail it. Hopefully soon!
Andrew
0xADF
I've replicated this on 6.0.0 Mac OS, and Windows XP SP3, and 6.0.2 on Mac OS.
Because this is a fairly UI independant operation, I would imagine it's across all operating systems (so I'm not surprised to see it in Linux).
The video should show that it's Mac OS that I had originally found it on, but I'm sure if Jorge wanted to know what platforms it was failing on, he would've asked 
It doesn't happen all the time, and it did take a while to come up with an example that is guaranteed to fail. It normally occurs when you're being complacent and not expecting it to happen.
Hi Chuck,
By default, you should receive email notifications for any discussion thread that you have posted in. On this page, there is a Actions widget near the top on the right hand side where you can disable email notifications for this thread. Additionally, you can view all your email notifications and disable as desired by clicking 'Manage email notifications' in the Actions widget on your profile page.
There had been an issue with delivery of email from element14 that impacted some users. This issue was resolved recently, and, thus, you may now be receiving notifications that you had not previously.
Cheers,
Drew
Why am I suddenly receiving email copies of posts?
On 01/12/2012 01:49 PM, Jason Tribbeck wrote:
Just downloaded 6.1.0, and my test example isn't failing as before.
So, 6.1.0 looks like it may have fixed it (I'll need to do some more tests though).
Yay!
Why am I suddenly receiving email copies of posts?
On 01/12/2012 01:49 PM, Jason Tribbeck wrote:
Just downloaded 6.1.0, and my test example isn't failing as before.
So, 6.1.0 looks like it may have fixed it (I'll need to do some more tests though).
Yay!
Hi Chuck,
By default, you should receive email notifications for any discussion thread that you have posted in. On this page, there is a Actions widget near the top on the right hand side where you can disable email notifications for this thread. Additionally, you can view all your email notifications and disable as desired by clicking 'Manage email notifications' in the Actions widget on your profile page.
There had been an issue with delivery of email from element14 that impacted some users. This issue was resolved recently, and, thus, you may now be receiving notifications that you had not previously.
Cheers,
Drew