Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) in V6.0.0 manual routing got really hard
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 36 replies
  • Subscribers 190 subscribers
  • Views 4687 views
  • Users 0 members are here
Related

in V6.0.0 manual routing got really hard

e14 Contributor
e14 Contributor over 14 years ago

somethings changed, when i manually route and click on the destination pad, if i dont click dead center now... im left with tiny tiny airwires

5.11 didnt do this... i have messed with alot of settings, nothing seems to help

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    No problem, Jorge.

     

    Do you still want a V5 version? (Now I'm at home, I've got time to prepare one as well).

     

    The only other issue I've got is a MacOS X one, which I posted in the "Is there a list of open issues?" thread. That one shouldn't be too hard to see and fix image But I'll leave that for you to comment on that thread instead of this one (I know you're reading this one, so it's really just a bit of a prompt!)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 12/28/2011 3:49 AM, Jason Tribbeck wrote:

    Hi,

     

    Okay - it also happens in the Windows version as well. Unfortunately, I don't have a v5 format file (I'll need to switch the directories back over, and I really should be working at work image ), but I've made it available (since I'm not NNTP, I don't have your email address, so it's on my web site).

     

    http://www.tribbeck.com/misc/test.zip

     

    This is a zip of my Eagle project directory, and contains the schematic and board files. It's a simple LED driver circuit that I've thrown together.

     

    This is reproducable using the following command:

     

    ROTATE =MR45 Q1

     

    Then, try and manually route the signal from SV1 pin 1 to pin 1 of Q1.

     

    I'm pretty sure it's never happened on 5.x.

     

     

    Awesome Jason,

     

    Thanks for preparing this, I'll forward this to our developers and

    hopefully they can get on it for the next beta.

     

    Thanks again for helping, and I apologize for the delay in getting to

    you with the release of V6 it's been very crazy around here.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi,

     

    Okay - it also happens in the Windows version as well. Unfortunately, I don't have a v5 format file (I'll need to switch the directories back over, and I really should be working at work image ), but I've made it available (since I'm not NNTP, I don't have your email address, so it's on my web site).

     

    http://www.tribbeck.com/misc/test.zip

     

    This is a zip of my Eagle project directory, and contains the schematic and board files. It's a simple LED driver circuit that I've thrown together.

     

    This is reproducable using the following command:

     

    ROTATE =MR45 Q1

     

    Then, try and manually route the signal from SV1 pin 1 to pin 1 of Q1.

     

    I'm pretty sure it's never happened on 5.x.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi,

     

    Many thanks for the response.

     

    Since I'm back at work today, I'll need to get these this evening.

     

    However, I have downloaded the Windows version, so I'll see if I can reproduce it here.

     

    The reproduction was a little annoying in that some times I was able to reproduce it easily, started to record and found it worked fine. Or, if I loaded in my example from a fresh start, it wouldn't do it for a while.

     

    But it doesn't take longer than 2 minutes of doing and undoing (which might be part of the problem) stuff before it shows its head - so I don't think it's hard to reproduce.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 12/26/2011 9:12 AM, Jason Tribbeck wrote:

    I'm guessing you're reading this from the newsgroups - in which case, it looks like if you post a video on the e14 forum, the link doesn't come through.

     

    For those of you using NNTP, then here's the link:

     

    https://www.youtube.com/watch?v=rZvQ3c9uDWk

     

     

    Hi Jason,

     

    Our developers are requesting the following, they would like some

    "patients" they could use to test and analyze the issue. My gut tells me

    that perhaps having the same design in version 5 and in version 6 with

    some clear instructions on how to reproduce the issue exactly. It's not

    easy to recreate something like this.

     

    In any event, I will forward you're video to the developers and see if

    that helps clear things up, but what will get this issue resolved the

    quickest is a couple of test files.

     

    You can e-mail them to me directly and I will pass it on to the developers.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Fix this it's so frustrating.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to dukepro

    I'm guessing you're reading this from the newsgroups - in which case, it looks like if you post a video on the e14 forum, the link doesn't come through.

     

    For those of you using NNTP, then here's the link:

     

    https://www.youtube.com/watch?v=rZvQ3c9uDWk

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • dukepro
    dukepro over 14 years ago in reply to e14 Contributor

    On 12/26/2011 04:52 AM, Jason Tribbeck wrote:

    I did a video of it to help explain what is happening - although reproducing it seems difficult when you're recording!

     

     

     

     

    ... and where might this video be?

     

        - Chuck

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    I did a video of it to help explain what is happening - although reproducing it seems difficult when you're recording!

     

    You don't have permission to edit metadata of this video.
    Edit media
    x
    image
    Upload Preview
    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Just tried it in 6.0.2 (beta version) - still broken.

     

    Steps to reproduce:

     

    1. Move component with air wires connected to pads
    2. Manually route to one of the component's pad from another one

     

    It's easier to reproduce if the component's pads aren't on the grid.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>