Hello?
Any thoughts on this? Can anyone reproduce this artifact?
David
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
Hello?
Any thoughts on this? Can anyone reproduce this artifact?
David
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
Unfortunately, I've not seen the original discussion about it, so I don't know if I can reproduce it or not (or at least have a go).
What, roughly, were you doing?
Hi Jason,
I attached the schematic and layout files to the original message. This bug
does not exist in version 5. the first time I saw it was in a PCB on which
I had a via/mounting hole near the origin. To make sure I don't have any
silkscreen too close to the pad, I turn on solder mask and do a DRC because
it will tell me if a part of the silkscreen is too close.
On this and all my other PCBs done in version 5 and earlier, I never had an
error. In Version 6, for some reason the component name/value are placed
invisibly near the origin. when I turn on the stop mask and run a DRC, this
invisible text shows up in the stop mask of the pad/via and generates
dozens of errors. These errors mask and make it very hard to find real
errors.
The steps to replicate it:
1. Create a simple schematic with a connector near the origin. Other
components may work. I just choose a random connector from the supplied
libraries. I originally found it with a 2 pin MTA connector I had modified.
However, it seems to happen with any random connector and I suspect it will
happen with any component.
2. Create PCB
3. Create a large Via, like 0.5 inch drill
4. Put the Via at 0, 0
5. Turn on the top stop mask layer
6. Do a DRC check
7. The name of the component shows up in the Via Stop Mask and causes all
sorts of stop mask errors.
The attached project shows this.
Thanks
David
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
Bug fixed in version 6.1.
Thanks CadSoft!
David
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
Well, I was going to have a go at recording it tonight (last night got a bit hectic), and I saw that 6.1.0 had been released.
I've not been able to reproduce it in this version - although it might be because I'm on a Mac here, or my reproduction procedure isn't working.
Anyway, worth a shot upgrading...
Hi,
It took a while (and I had to go to the eaglecentral.ca web site to see your screenshot), but I have reproduced it.
It doesn't happen if you don't have vector fonts enabled (i.e. if it's proportional, it doesn't happen). Most of the default components use proportional fonts, which is probably why other people haven't reproduced it (if they've tried).
The DRC rules do appear valid - but only if the text had actually been placed there!
I'll try to make a video of it tonight on my Mac (I've got the full Eagle license there - but not at work).
Hi,
It took a while (and I had to go to the eaglecentral.ca web site to see your screenshot), but I have reproduced it.
It doesn't happen if you don't have vector fonts enabled (i.e. if it's proportional, it doesn't happen). Most of the default components use proportional fonts, which is probably why other people haven't reproduced it (if they've tried).
The DRC rules do appear valid - but only if the text had actually been placed there!
I'll try to make a video of it tonight on my Mac (I've got the full Eagle license there - but not at work).
Bug fixed in version 6.1.
Thanks CadSoft!
David
--
Web access to CadSoft support forums at www.eaglecentral.ca. Where the CadSoft EAGLE community meets.
Well, I was going to have a go at recording it tonight (last night got a bit hectic), and I saw that 6.1.0 had been released.
I've not been able to reproduce it in this version - although it might be because I'm on a Mac here, or my reproduction procedure isn't working.
Anyway, worth a shot upgrading...