Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Overlapping Pads
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 188 subscribers
  • Views 631 views
  • Users 0 members are here
Related

Overlapping Pads

e14 Contributor
e14 Contributor over 14 years ago

I have two problems that I need to solve, both involving high-current

circuits:

 

First, I'm going to be laying down some FETs in SO-8 packages, and I want

a good solid connection from the four drain pins to a surrounding

polygon, both for current flow and to provide a thermal path for heat

sinking.  For the same part I want the same solid connection to the

source pins, although I don't need a polygon.  Connections that allow

good wide traces (up to 200 mils would be nice) without stomping on the

gate connection would be nice.

 

Second, I'll be putting in some current sense resistors.  While I'm going

cheap and using 2-terminal resistors, I'd like to make a pseudo 4-

terminal device by laying the part out with four pads, but then

connecting pairs of pads with a polygon or some such so that it looks and

solders like a regular resistor, but so that I can have my nice high-

current connections going to it with honkin' big traces, and still have

some thin traces coming off of the pads -- independent of the big traces

-- in a "pseudo Kelvin" connection.

 

Has anyone solved this problem before?  Got any suggestions on how to

proceed?

 

--

My liberal friends think I'm a conservative kook.

My conservative friends think I'm a liberal kook.

Why am I not happy that they have found common ground?

 

Tim Wescott, Communications, Control, Circuits & Software

http://www.wescottdesign.com

 

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    Tim Wescott wrote:

    I have two problems that I need to solve, both involving high-current

    circuits:

     

    First, I'm going to be laying down some FETs in SO-8 packages, and I

    want a good solid connection from the four drain pins to a surrounding

    polygon, both for current flow and to provide a thermal path for heat

    sinking.  For the same part I want the same solid connection to the

    source pins, although I don't need a polygon.  Connections that allow

    good wide traces (up to 200 mils would be nice) without stomping on

    the gate connection would be nice.

     

    Second, I'll be putting in some current sense resistors.  While I'm

    going cheap and using 2-terminal resistors, I'd like to make a pseudo

    4- terminal device by laying the part out with four pads, but then

    connecting pairs of pads with a polygon or some such so that it looks

    and solders like a regular resistor, but so that I can have my nice

    high- current connections going to it with honkin' big traces, and

    still have some thin traces coming off of the pads -- independent of

    the big traces -- in a "pseudo Kelvin" connection.

     

    Has anyone solved this problem before?  Got any suggestions on how to

    proceed?

     

    Hi Tim

     

    Mock up an image of what you are attempting. That would make a potentially

    long reply more targetted.

     

    Warren

     

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Tim

    See this document

    http://www.irf.com/technical-info/appnotes/an-1154.pdf

     

    Do you want to achieve the land pattens they have for their SO8

    Fig 4

     

    Warren

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Tim

    See this document

    http://www.irf.com/technical-info/appnotes/an-1154.pdf

     

    Do you want to achieve the land pattens they have for their SO8

    Fig 4

     

    Warren

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Tim Wescott wrote:

    On Tue, 07 Feb 2012 07:56:59 +1300, Warren Brayshaw wrote:

     

    >> Tim Wescott wrote:

    >>> I have two problems that I need to solve, both involving

    >>> high-current circuits:

    >>>

    >>> First, I'm going to be laying down some FETs in SO-8 packages, and I

    >>> want a good solid connection from the four drain pins to a

    >>> surrounding polygon, both for current flow and to provide a thermal

    >>> path for heat sinking.  For the same part I want the same solid

    >>> connection to the source pins, although I don't need a polygon.

    >>> Connections that allow good wide traces (up to 200 mils would be

    >>> nice) without stomping on the gate connection would be nice.

    >>>

     

    As you know that 4 pins on one side are common and three on the other are

    common I would make a library device that a single pad covering those

    regions, including the heat sink.

    That gives only 3 pins of the symbol to match with three pads of the

    package. When placed on the board, connect up with modest traces initially .

    Then plonk a polygon over the drain and source pins as required to get the

    copper coverage.

    Name these polygons to match the signal name at the drain and source as

    appropriate.

    Increase the sizes of the feeder traces as best you can.

     

    HTH

    Warren

    --

    Viewed / responded via the newsgroup at

    news.cadsoft.de