Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) High Current Traces
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 24 replies
  • Subscribers 190 subscribers
  • Views 4413 views
  • Users 0 members are here
  • current
  • trace
  • width
  • high
Related

High Current Traces

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I'm a new Eagle user, but I suspect this is actually a more complicated question.

 

I have traces that will carry up to 2 amps.  Those traces also control various FETs and other signals.  If I set that net node to the trace width for the high current, all of the net gets set to that width and I don't have room to route my board.  I've already re-arranged all my components so that the wide traces are short and the pins near each other.  I've even gone from 4 layers to 6 layers.  (The board routes just fine with 4 layers by 7 mil traces.)

 

I don't see a way to set the width of signals before routing, and after routing is too late.  One idea is to isolate the low current part of the net from the high current with a 0 ohm resistor, then after routing fill in will a trace.  But even that seems a little clumsy.

 

I'm considering going to thicker copper layers so that I can reduce the trace width, but I haven't tried that yet.

 

Does anyone have any ideas on how I might solve this problem?

 

Thanks,

 

Dave

  • Sign in to reply
  • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hmmm...  Maybe I'm being too obsessed with eliminating the errors/warnings.  Why couldn't I just rip those couple of traces, get rid of the polygons (which have line width) and draw a rectangle on that layer of the board overlapping the pins (to replace the polygon).  That would give me overlap errors, but so what?  As long as the rectangle (or overlapping rectangles) connects the pins, it should be OK.

     

    Is this a simple solution?  (I don't want to go for fab then find out I missed something.  image )

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Dave,

     

    Ok, I see now. :-)

     

    There are two possible solutions. The first would be to "partially" decrease traces width just between pins 15 & 16 (and 11 & 12). You can do this trick by routing three traces instead of one between those pins and editing each trace section - middle section is 0.5mm, remaining two are thinner and are present just to avoid errors.

    The second approach is to place a polygon (and name it with net's name, additionally uncheck Thermals option).

     

    Please find attached example screenshot of the description above.

    At the picture top you can see just traces/polygon, at the bottom these traces/polygon are presented with chip pins.

    From left to right, first is your approach, then 3-traces solution (the two error-avoiding traces are highlighted in orange, just to point out that they are present) and the most right is a polygon.

     

    image

     

     

    Probably there are also some other solutions, but I'm not aware of any which would not require some manual intervention.

     

     

    Best wishes,  Ivan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Ivan Zilic wrote:

     

    Hi Dave,

     

    For easier visualisation, a screenshot of this problematic PCB part would be useful... ;-)

     

    Anyway, I can read your fear about high currents and traces width. That's ok, but current is not the only parameter to be considered during traces width selection. Actually, it is the temperature which you should have in mind. When you have good air flow or larger enclosure, you can decrease traces width.

    To avoid guessing, you can use one of online calculators which return min trace width based on your temperatures (environment and max allowed trace temperature) and few laminate properties. Hopefully, you will find out that 0.25mm is enough.

     

     

    Best wishes,  Ivan.

    Hi Ivan,

     

    Yes, I've considered trace temperature and I think I'm being conservative regarding trace width.  I'd rather err on the safe side and I think I'm pretty close to routing with 0.50 mm traces on the high current lines, including the low current traces on the same net as the high current traces.

     

    But I still have this one clearance issue when the 0.25 mm pad is routed with a 0.50 mm trace.  A picture of this is below.  Two pins on the top right (pins 16 & 15) and four pins coming down the right side from the top (pins 14 through 11) are on the same net.  You can see the bulge on pin 16 which is too close to pin 17, and a similar bulge between pins 11 and 10.  These bulges are the 0.50 mm traces added by the router.  I can rip those traces, but even if I route manually they are the same 0.50 mm width and I have the same problem.  There is also a polygon with the same net sitting on top of these pads and extending to the right.  (Some caps sit on the other end of the polygon.)

     

    I tried eliminating 5 of the pins in the symbol, then putting a polygon in the package to cover the 1 remaining pin and where the other 5 pins would be.  But that gives me an overlap error.

     

    I'll keep trying things but if anyone has a good idea, let me know.

     

    Thanks,

     

    Dave

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Dave,

     

    For easier visualisation, a screenshot of this problematic PCB part would be useful... ;-)

     

    Anyway, I can read your fear about high currents and traces width. That's ok, but current is not the only parameter to be considered during traces width selection. Actually, it is the temperature which you should have in mind. When you have good air flow or larger enclosure, you can decrease traces width.

    To avoid guessing, you can use one of online calculators which return min trace width based on your temperatures (environment and max allowed trace temperature) and few laminate properties. Hopefully, you will find out that 0.25mm is enough.

     

     

    Best wishes,  Ivan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago

    OK, final post on this.  After a bunch of tweaks, I've gotten everything to route with this last problem.

     

    I have a QFN24 package that has 6 output pins which together provide up to 5 amps.  Each pin has a width of 0.25 mm.  The 6 pins are overlaid with a polygon which is connected to one of my high current traces.  My high current trace is 0.5 mm.  The router creates traces which are the width of the wide netclass trace, 0.5 mm, and even though there is a polygon connecting the pins, the router runs traces between all the pins.

     

    Here's the problem.  At the end points of the polygon connecting the 6 pins, the 0.5 mm traces extend past the 0.25 mm pads, violating the spacing to the next pins.  I can't change the width of the pins or the width of the traces.  Do I rip just those traces then route manually?

     

    Thanks,

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Ivan,

     

    Thanks for the suggestions.  Yes, that's pretty much what I thought

    needed to be done.  But as my initial report said, I'm a new user so

    I'm still learning a lot.  One thing that stops me from manually

    routing is I ran into a roadblock adding vias.  I couldn't figure out

    how to make the corresponding hole in the ground plane to run the via through.

     

    In the meantime, I figure I can go to 2 oz copper and thinner

    traces.  I'm pretty close in routing everything (3 wires out of 350),

    so figure I can get there with some care.

     

    Not sure about some manual routing.  I don't know enough about Eagle yet.

     

    Thanks again!!!

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Hi Dave,

     

    If you insist in 0-ohm "bridges", you might (most likely, according to your description how this is becoming complicated) want to add more than one split-resistor per net.

     

    To get a good estimation about number of 0-ohm resistors needed, perform the following steps: (1) run autorouter, (2) highlight trace of interest, (3) count number of trace branches mixing high and low current flows. These joints are initial candidates for your 0-ohm resistors location.

     

     

    BTW: I prefer (at least) partial manual routing.

     

     

    Best wishes,  Ivan.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to Morosh

    Hi Morosh,

     

    Yes, that is where I started in my original post.  I tried doing it and it got complicated.  Maybe I'll try again.

     

    Thanks,

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Morosh
    Morosh over 14 years ago in reply to e14 Contributor

    On 10/06/2012 09:10, Dave Wills wrote:

    My apologies if I'm being dense.

     

    I don't appear to be able to change the width on any unrouted traces.  Am I missing something?

     

    Manually routing some nodes doesn't seem like a good option.  If I tweak anything and need to start over, it takes a lot of time.

     

    I could route the wide traces first, but I can't rip some of the traces on a node and leave others alone, then auto routed the ripped wide traces with a smaller width.  At least, not without a lot of manual work.  Seems I'd need to route wide traces, rip the ones that don't need to be wide, then change the width of the signals on that net, and finally continue routing with the new widths.  Again, this is a lot of manual work.

     

    To give an idea, here are my high current nodes:

     

    N$61  C21      1        P$1        3 *** up to 1 amp

              C22      1        P$1        3 *** up to 1 amp

              L3        2        2          3 *** up to 2 amps

              R24      1        P$1        3 signal level

              R25      2        P$2        3 signal level

              R26      C        P$2        3 *** up to 2 amps

              R27      2        P$2        3 signal level

              U4       9        VON        3 signal level

     

    N$60   C19      2        P$2        3 signal level

              L3        1        1            3 *** up to 2 amps

              U4       11       SW         3 *** up to 1 amp

              U4       12       SW         3 *** up to 1 amp

              U4       13       SW         3 *** up to 1 amp

              U4       14       SW         3 *** up to 1 amp

              U4       15       SW         3 *** up to 1 amp

              U4       16       SW         3 *** up to 1 amp

     

    N$62   Q8       4        S          3 *** up to 2 amps

              R26      A        P$1        3 *** up to 2 amps

              U5       6        -IN        3 signal level

              U7       6        -IN        3 signal level

     

    N$63   Q10      4        S          3 *** up to 2 amps

              Q11      4        S          3 *** up to 2 amps

              Q8       1        D          3 *** up to 2 amps

              Q8       2        D          3 *** up to 2 amps

              Q8       5        D          3 *** up to 2 amps

              Q8       6        D          3 *** up to 2 amps

     

    You can see that there are low current (skinny traces) mixed in with high current (wide) traces.  Even though the traces that need to be wide are near each other, the signal level traces get routed as wide traces.  When these need to go through vias and inner layers, it doesn't leave enough room for the rest of the signal level traces.  (Note that I have created some polygons around some of the signals, for example U4 11 - 16.  That does help routing somewhat.)

     

    And then, consider the same problem when you look at GND.  I have a similar number of high current traces.  Though I have a ground plane, I need to specify some vias as larger than others into the ground plane in order to carry the current.

     

    I'm starting to think that maybe Eagle isn't useful for boards with mixed trace widths and high density.  I might be better off having a professional layout firm do the last step.

     

    Thanks for reading.

     

    Dave

     

    In your schematic, connect the non_high current nets to the high current

    nets with a 0 ohm resistor, they'll have a different name.

    Specify the adequate width to the high-current nets using class, route

    as usual, then remove the resistor and connect directly.

    there is some work in the schematic.

    HTH

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    My apologies if I'm being dense.

     

    I don't appear to be able to change the width on any unrouted traces.  Am I missing something?

     

    Manually routing some nodes doesn't seem like a good option.  If I tweak anything and need to start over, it takes a lot of time.

     

    I could route the wide traces first, but I can't rip some of the traces on a node and leave others alone, then auto routed the ripped wide traces with a smaller width.  At least, not without a lot of manual work.  Seems I'd need to route wide traces, rip the ones that don't need to be wide, then change the width of the signals on that net, and finally continue routing with the new widths.  Again, this is a lot of manual work.

     

    To give an idea, here are my high current nodes:

     

    N$61  C21      1        P$1        3 *** up to 1 amp
             C22      1        P$1        3 *** up to 1 amp
             L3        2        2          3 *** up to 2 amps
             R24      1        P$1        3 signal level
             R25      2        P$2        3 signal level
             R26      C        P$2        3 *** up to 2 amps
             R27      2        P$2        3 signal level
             U4       9        VON        3 signal level

     

    N$60   C19      2        P$2        3 signal level
             L3        1        1            3 *** up to 2 amps
             U4       11       SW         3 *** up to 1 amp
             U4       12       SW         3 *** up to 1 amp
             U4       13       SW         3 *** up to 1 amp
             U4       14       SW         3 *** up to 1 amp
             U4       15       SW         3 *** up to 1 amp
             U4       16       SW         3 *** up to 1 amp

     

    N$62   Q8       4        S          3 *** up to 2 amps
             R26      A        P$1        3 *** up to 2 amps
             U5       6        -IN        3 signal level
             U7       6        -IN        3 signal level

     

    N$63   Q10      4        S          3 *** up to 2 amps
             Q11      4        S          3 *** up to 2 amps
             Q8       1        D          3 *** up to 2 amps
             Q8       2        D          3 *** up to 2 amps
             Q8       5        D          3 *** up to 2 amps
             Q8       6        D          3 *** up to 2 amps

     

    You can see that there are low current (skinny traces) mixed in with high current (wide) traces.  Even though the traces that need to be wide are near each other, the signal level traces get routed as wide traces.  When these need to go through vias and inner layers, it doesn't leave enough room for the rest of the signal level traces.  (Note that I have created some polygons around some of the signals, for example U4 11 - 16.  That does help routing somewhat.)

     

    And then, consider the same problem when you look at GND.  I have a similar number of high current traces.  Though I have a ground plane, I need to specify some vias as larger than others into the ground plane in order to carry the current.

     

    I'm starting to think that maybe Eagle isn't useful for boards with mixed trace widths and high density.  I might be better off having a professional layout firm do the last step.

     

    Thanks for reading.

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>