Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Use Improvements?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 8 replies
  • Subscribers 189 subscribers
  • Views 570 views
  • Users 0 members are here
Related

Use Improvements?

e14 Contributor
e14 Contributor over 14 years ago

New user, so maybe I'm missing something.  But I would like to have these:

 

On most tools, once you select the tool and use it, a left click on a new item repeats the tool.  Would be nice if Properties worked this way.

 

For library maintenance, you can't remove a device, package or symbol unless you have that item open.  Would be nice to be able to delete anything without opening it first.

 

Would be nice to have a "Repeat" button so some operation on one item can be repeated on another.  A simple example is VALUE.

 

Dave

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    On 6/14/2012 12:15 PM, Dave Wills wrote:

    New user, so maybe I'm missing something.  But I would like to have these:

     

    On most tools, once you select the tool and use it, a left click on a new item repeats the tool.  Would be nice if Properties worked this way.

     

    For library maintenance, you can't remove a device, package or symbol unless you have that item open.  Would be nice to be able to delete anything without opening it first.

     

    Would be nice to have a "Repeat" button so some operation on one item can be repeated on another.  A simple example is VALUE.

     

    Dave

     

     

    Hi Dave,

     

    A couple of points need to be corrected.

     

    In the libraries as long as you have the library open, going Library->

    Remove allows you to remove anything as long as you know it's name; the

    specific package,device, or symbol need not be open. So lets say you

    have device called test you want to delete but you're working on a

    package, you don't have to open the device. Just go Library-> Remove,

    then in the little dialog that pops up type:

     

    test.dev and press enter

     

    A repeat button is unnecessary since most of EAGLE's commands work this

    way. If you click on the VALUE icon it will stay active until you press

    escape or select another command. While the command is active you can

    just left click on each component and alter it's value one by one.

     

    Thank you for your suggestions and we hope that you continue to enjoy

    working with EAGLE.

     

    Best Regards,

     

    Jorge Garcia

    Cadsoft Support

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Jorge Garcia wrote:

    >On 6/14/2012 12:15 PM, Dave Wills wrote:

    >>[...]

    >> Would be nice to have a "Repeat" button so some operation on one item can be repeated on another.  A simple example is VALUE.

    >[...]

    >A repeat button is unnecessary since most of EAGLE's commands work this

    >way. If you click on the VALUE icon it will stay active until you press

    >escape or select another command. While the command is active you can

    >just left click on each component and alter it's value one by one.

     

    elaborating on that: invoking a for instance a change or value command

    via the command line lets you modifiy part attributs by clicking in

    them until you abort the command or enter/select a new one.

    --

     

    Lorenz

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks Jorge and Lorenz,

     

    On the first item: Here's an example. I have nothing selected in the schematic page. I right click on any part, then select NAME. The NAME popup appears and I can modify it. I can left click on any other part and the NAME popup appears for that part. Now I want to change something in Properties, lets say Net Class. So I right click on a wire, select Properties, select the Net Class I want and then click OK. To modify the Net Class of the next wire, I need to right click and Properties again. Since the previous operation was Properties, why can't it just open the Properties window with a single click?  Rather, if I left click the NAME window from before pops up.  This isn't the only example of this, and if you do Properties a lot, it's a lot of clicking and mouse moves.  (Repeat does work on many commands, just not Properties.)

     

    On the second item: I just tried this again and was able to remove a part that was not open (package).  I know there are conditions where this isn't true.  When I find them, I'll post again.

     

    On the third item: Consider the first item.  If I want to do the same operation under Properties a bunch of times, I have to do all the clicks and mouse moves just to get to Properties as above first, then the same operation I did for the previous item.  So for Net Class, if I could left click on what I want then have a "Repeat <previous operation such as Net Class>" button, it would save a ton of time.

     

    Lorenz, sorry, I don't understand.  I'm an old time UNIX guy, but I'm perfectly happy using IDEs rather than command line.  Can you give me a specific example I can try?

     

    Thanks,

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Thanks Jorge and Lorenz,

     

    On the first item: Here's an example. I have nothing selected in the schematic page. I right click on any part, then select NAME. The NAME popup appears and I can modify it. I can left click on any other part and the NAME popup appears for that part. Now I want to change something in Properties, lets say Net Class. So I right click on a wire, select Properties, select the Net Class I want and then click OK. To modify the Net Class of the next wire, I need to right click and Properties again. Since the previous operation was Properties, why can't it just open the Properties window with a single click?  Rather, if I left click the NAME window from before pops up.  This isn't the only example of this, and if you do Properties a lot, it's a lot of clicking and mouse moves.  (Repeat does work on many commands, just not Properties.)

     

    On the second item: I just tried this again and was able to remove a part that was not open (package).  I know there are conditions where this isn't true.  When I find them, I'll post again.

     

    On the third item: Consider the first item.  If I want to do the same operation under Properties a bunch of times, I have to do all the clicks and mouse moves just to get to Properties as above first, then the same operation I did for the previous item.  So for Net Class, if I could left click on what I want then have a "Repeat <previous operation such as Net Class>" button, it would save a ton of time.

     

    Lorenz, sorry, I don't understand.  I'm an old time UNIX guy, but I'm perfectly happy using IDEs rather than command line.  Can you give me a specific example I can try?

     

    Thanks,

     

    Dave

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • CSWalt
    CSWalt over 14 years ago in reply to e14 Contributor

    On 06/18/2012 02:35 PM, Christian Bohrer wrote:

    "Dave Wills"<noreply-108456@element14.com>  a écrit dans le message de news:

    433705745.23551339799637003.JavaMail.jive@flcspu-csapp-01.premierfarnell.com...

    >> Thanks Jorge and Lorenz,

    >>

    >> On the first item: Here's an example. I have nothing selected in the schematic page. I right

    >> click on any part, then select NAME. The NAME popup appears and I can modify it. I can left click

    >> on any other part and the NAME popup appears for that part. Now I want to change something in

    >> Properties, lets say Net Class. So I right click on a wire, select Properties, select the Net

    >> Class I want and then click OK. To modify the Net Class of the next wire, I need to right click

    >> and Properties again. Since the previous operation was Properties, why can't it just open the

    >> Properties window with a single click? Rather, if I left click the NAME window from before pops

    >> up. This isn't the only example of this, and if you do Properties a lot, it's a lot of clicking

    >> and mouse moves. (Repeat does work on many commands, just not Properties.)

     

    Select the command first. The command selected will stay active until you STOP it.

    Example: if you select first the button info (Properties), you can open successively  the

    "Properties Box" of each element by a simple click.

     

    >

    OK, and another thing:

    To modify the netclass many times you simply use CHANGE CLASS (see change submenu).

    Then click all the nets you want to have and that's it !

     

    Regards,

    Walter Spermann

     

     

    --

    -


    Walter Spermann

    Softwareentwicklung

    CadSoft Computer GmbH

    Pleidolfweg 15

    84568 Pleiskirchen

    Tel.: 08635/6989-10

    www.cadsoft.de

    -


    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Thomas Liratsch

    -


     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Christian Bohrer wrote on Mon, 18 June 2012 05:35

    Select the command first. The command selected will stay active until you

    STOP it.

    Example: if you select first the button [i

    info (Properties), you can open successively  the

    "Properties Box" of each element by a simple click.

     

     

    Ah yes.  I hadn't thought of that simple solution.  OTOH, if you click the

    icon, you can left click as many other items you want and still get

    properties.  If you right click then select NAME, you can still get the

    NAME of all the other items.  (It switches from Properties to Name.)  If

    you then right click and select Properties, it only does it once.

    Unexpected behavior.

     

    Thanks,

     

    Dave

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

     

    "Dave Wills" <noreply-108456@element14.com> a écrit dans le message de news:

    433705745.23551339799637003.JavaMail.jive@flcspu-csapp-01.premierfarnell.com...

    Thanks Jorge and Lorenz,

     

    On the first item: Here's an example. I have nothing selected in the schematic page. I right

    click on any part, then select NAME. The NAME popup appears and I can modify it. I can left click

    on any other part and the NAME popup appears for that part. Now I want to change something in

    Properties, lets say Net Class. So I right click on a wire, select Properties, select the Net

    Class I want and then click OK. To modify the Net Class of the next wire, I need to right click

    and Properties again. Since the previous operation was Properties, why can't it just open the

    Properties window with a single click? Rather, if I left click the NAME window from before pops

    up. This isn't the only example of this, and if you do Properties a lot, it's a lot of clicking

    and mouse moves. (Repeat does work on many commands, just not Properties.)

     

    Select the command first. The command selected will stay active until you STOP it.

    Example: if you select first the button info (Properties), you can open successively  the

    "Properties Box" of each element by a simple click.