Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Arbitrary Pad Shapes
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 7 replies
  • Subscribers 188 subscribers
  • Views 1223 views
  • Users 0 members are here
Related

Arbitrary Pad Shapes

e14 Contributor
e14 Contributor over 14 years ago

Hi,

 

I have a FET with the pad layout shown in the attached drawing.  I've tried

a few things but can't get past the "Package ... contains an invalid

polygon."

 

First I tried having 4 pads all connected with a polygon in the shape of an

"H".  That didn't work.

 

Next I tried a single pad with the "H" creating the other 3 pads with the

polygon.  That did't work.  In addition, if I make the polygon width too

large, it doesn't fit, too small, Eagle complains, and anything in the

middle leaves the corners of the other 3 pads rounded.

 

Next I tried a single pad but creating the pad with wires.  This doesn't

work either and I have the same problem with the rounded corners.

 

Finally I tried a single pad and making the "H" with overlapping rectangles

on the top side.  And guess what?  That didn't work either.

 

What is even more confusing is for the last 2 attempts there aren't even

any polygons in the package (and I have only this one library turned on so

there aren't any other conflicting packages).

 

I'm baffled as to how to do this.  Any ideas?

 

Thanks,

 

Dave

--

Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

 

Attachments:
image
  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 14 years ago

    OK, I think I fixed this on my 6th attempt.

     

    What I did was to make the 4 outer rectangles 4 different pads, then make

    an inner pad which abuts the 4 outer pads.  Then for that device, I connect

    all 5 pads to the same pin of the symbol.

     

    This seems to work OK but I'm confused by some things.  First, is there any

    way to connect those 5 pads within the library part so that the autorouter

    doesn't connect them?  The reason is all 5 pads carry high current

    (discussion in another post I made) and so traces on that net class are

    wider than a single pin.  Letting the autorouter connect the pins external

    to the library means the wider traces have clearance errors unless I

    manually make the ones that have clearance errors smaller.  (This is why I

    tried the first 5 attempts at creating the part which didn't work.)

     

    The other question is unrelated.  I have a QFN24 SMD device with an exposed

    pad underneath.  The exposed pad pin is connected to GND on the schematic.

    To make sure I get sufficient thermal and current transfer with the exposed

    pad, I add some vias to my GND layer on the pad.  But DRC gives me overlap

    errors.  The exposed pad is connected to GND and the NAME on the vias is

    GND.  Why would I get overlap errors?

     

    Thanks a ton.

     

    Dave

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    On 6/27/2012 2:07 PM, Dave Wills wrote:

    OK, I think I fixed this on my 6th attempt.

     

    What I did was to make the 4 outer rectangles 4 different pads, then make

    an inner pad which abuts the 4 outer pads.  Then for that device, I connect

    all 5 pads to the same pin of the symbol.

     

    This seems to work OK but I'm confused by some things.  First, is there any

    way to connect those 5 pads within the library part so that the autorouter

    doesn't connect them?  The reason is all 5 pads carry high current

    (discussion in another post I made) and so traces on that net class are

    wider than a single pin.  Letting the autorouter connect the pins external

    to the library means the wider traces have clearance errors unless I

    manually make the ones that have clearance errors smaller.  (This is why I

    tried the first 5 attempts at creating the part which didn't work.)

     

    Hi Dave,

     

    The key to making the Arbitrary pad shapes is that the pad must be

    completely enclosed by the polygon and any wires used to define the

    arbitrary pad shape must run through the center of said pad in order to

    be recognized.

     

    A better way is to create a single small pad in the center of the giant

    pad and then form the giant pad using a single polygon in the library.

    All you have to do is figure out where the corners of the PAD are

    located and making the polygon will be easy since you can input specific

    points in the command line.

     

    hth,

    Jorge Garcia

    Cadsoft Support

     

    The other question is unrelated.  I have a QFN24 SMD device with an exposed

    pad underneath.  The exposed pad pin is connected to GND on the schematic.

    To make sure I get sufficient thermal and current transfer with the exposed

    pad, I add some vias to my GND layer on the pad.  But DRC gives me overlap

    errors.  The exposed pad is connected to GND and the NAME on the vias is

    GND.  Why would I get overlap errors?

     

    I'm going to answer for you here, but in the future if you wish to

    present a different problem it's preferable to start a new thread. It

    makes it easier when users search the forum for answers to questions.

     

    The manual states that Overlap errors occur when copper objects of

    disimilar classes come into contact with each other. Can you confirm

    that all of the items belong to the GND net by typing show GND in the

    command line?

     

    hth,

    Jorge Garcia

     

    Thanks a ton.

     

    Dave

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Jorge Garcia wrote on Wed, 27 June 2012 14:19

    On 6/27/2012 2:07 PM, Dave Wills wrote:

    <snip>

    Hi Dave,

     

    The key to making the Arbitrary pad shapes is that the pad must be

    completely enclosed by the polygon and any wires used to define the

    arbitrary pad shape must run through the center of said pad in order to

     

    be recognized.

     

    A better way is to create a single small pad in the center of the giant

     

    pad and then form the giant pad using a single polygon in the library.

     

    All you have to do is figure out where the corners of the PAD are

    located and making the polygon will be easy since you can input

    specific

    points in the command line.

     

    hth,

    Jorge Garcia

    Cadsoft Support

    <snip>

    I'm going to answer for you here, but in the future if you wish to

    present a different problem it's preferable to start a new thread. It

    makes it easier when users search the forum for answers to questions.

     

    The manual states that Overlap errors occur when copper objects of

    disimilar classes come into contact with each other. Can you confirm

    that all of the items belong to the GND net by typing show GND in the

    command line?

     

    hth,

    Jorge Garcia

     

     

     

    Hi Jorge,

     

    WRT polygons, I think this gets me back to the problems I reported to

    start.  Polygons have width and the width will have to be less than the pad

    size in order to include the fingers of the "H" (or overlap).  So unless

    the polygon has near zero width, the fingers will have rounded corners.

    I'll try again to see what I come up with.  Regardless, I think I end up

    with errors/warnings that can't be resolved, just approved.

     

    WRT the GND net, yes, if I show GND, the vias, the exposed pad and the GND

    layer all show up.  The name of the pin on the package is EXP and it is

    connected to GND with a wire.  The net list shows that pin of the IC

    connected to GND.

     

    Thanks,

     

    Dave

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 14 years ago in reply to e14 Contributor

    Jorge Garcia wrote on Wed, 27 June 2012 14:19

    On 6/27/2012 2:07 PM, Dave Wills wrote:

    <snip>

    Hi Dave,

     

    The key to making the Arbitrary pad shapes is that the pad must be

    completely enclosed by the polygon and any wires used to define the

    arbitrary pad shape must run through the center of said pad in order to

     

    be recognized.

     

    A better way is to create a single small pad in the center of the giant

     

    pad and then form the giant pad using a single polygon in the library.

     

    All you have to do is figure out where the corners of the PAD are

    located and making the polygon will be easy since you can input

    specific

    points in the command line.

     

    hth,

    Jorge Garcia

    Cadsoft Support

    <snip>

    I'm going to answer for you here, but in the future if you wish to

    present a different problem it's preferable to start a new thread. It

    makes it easier when users search the forum for answers to questions.

     

    The manual states that Overlap errors occur when copper objects of

    disimilar classes come into contact with each other. Can you confirm

    that all of the items belong to the GND net by typing show GND in the

    command line?

     

    hth,

    Jorge Garcia

     

     

     

    Hi Jorge,

     

    WRT polygons, I think this gets me back to the problems I reported to

    start.  Polygons have width and the width will have to be less than the pad

    size in order to include the fingers of the "H" (or overlap).  So unless

    the polygon has near zero width, the fingers will have rounded corners.

    I'll try again to see what I come up with.  Regardless, I think I end up

    with errors/warnings that can't be resolved, just approved.

     

    WRT the GND net, yes, if I show GND, the vias, the exposed pad and the GND

    layer all show up.  The name of the pin on the package is EXP and it is

    connected to GND with a wire.  The net list shows that pin of the IC

    connected to GND.

     

    Thanks,

     

    Dave

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.