Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Formatting Xref net labels
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 42 replies
  • Subscribers 192 subscribers
  • Views 7938 views
  • Users 0 members are here
Related

Formatting Xref net labels

zainka
zainka over 13 years ago

Hi

 

Normally I have used only the text-based net labels on line that goes

from one sheet to another. My wish is to use the XREF option but I am

not comfortable with the format options.

 

My "big" problem is that the signal name for a given net label comes

inside the flag. I would prefer all symbols to be of equal size and to

have the text align on beside of the net flag instead.

 

not like this            but like this

   ______________________          _____

/NETLABEL_SIGNAL_NAME |       /     | NETLABEL_SIGNAL_NAME

  \______________________|        \_____|

 

If not existing as an option already I would recommend to make the order

of the label xref formatting tags relevant (as set in misc menu) to the

result. Se my examples below:

 

                  ________________

%F%N (%S)      / NETLABEL (1)  |

                 \________________|

 

                  _____

%N %F(%S)      / (1) | NETLABEL

                 \_____|

                  _____

%N (%S)%F      /     | NETLABEL (1)

                 \_____|

 

Here everything coming in front of the %F tag ends up outside the flag

and everything after %F ends up inside. The flag symbol would thus have

a minimum size like say 3 letters.

 

Second. Is it possible to have flags indicating direction of a net? I.e.

if signal is in, out or bidirectional. This should be possible to change

with a change command like for example CHANGE DIRECTION or CHANGE FLAG

if not existing as an option already somewhere.

 

input             bi              output

   _______          ______         ______

_/       |       /      \       |      \

  \_______|        \______/       |______/

 

 

NOTE: I asked this as an question in the support forum, but as mentioned

there I would put it here as a suggestion if it was not possible in some

other way already. As far as I can see, it is not, though I am using

glasses....!*

 

Breg

Vidar (Z)

 

  • Sign in to reply
  • Cancel
  • zainka
    zainka over 13 years ago in reply to e14 Contributor

    On 11/23/2012 02:36 PM, Olin Lathrop wrote:

    Vidar (Z) wrote on Fri, 23 November 2012 04:46

    >>> If a pin direction was fixed and you knew you wanted to show it in

    >>> the

    >>> schematic every time, you could even add this to the symbol in the

    >>> library.

    >>

    >> You do not know what the direction of a MCU port pin will be, as

    >> already

    >> stated by your self, so thus adding directions symbols in the library

    >> is

    >> in my opinion lack of consistency when it comes to drawing symbols.

     

    Right, that's why I said "if".  I have only added direction symbols a few

    times in libraries.  Most of the confusion is around microcontroller pins

    that can be used different ways.  For those I add the little arrows in the

    schematic as I showed.  This is really easy.

     

     

    Well, I did not comment on that before, but I did not like your

    "solution" at all, but we live in a free world and you may do as you like.

     

    However, a flag as outlined in my suggestion will be attached to the net

    and by dragging the flag one will bring the net with you making it easy

    to rearrange the schematic, if needed, without having to move around

    self drawn arrows as-well.

     

    And as mentioned. The flag option is partly implemented already and thus

    part of eagle today, and one is free to use the feature, if implemented,

    or to use whatever self-invented options one like.

     

     

    /quote

    and there are many peoples that finds this suggestion to be important

    as-well.

    I seriously doubt that.  You have latched onto this issue for some reason,

    but it's really a minor nit in the overall scheme of things.  We don't want

    CadSoft getting distracted by all the little minor nits to the point that

    the truly useful major features get less attention.  The great thing about

    Eagle is you can already do many things you wish it had on your own well

    enough.  This particular feature is a great example of that.

     

     

    I won't (almost) even comment that more than to saying there is

    different opinions on this than yours and mine.

     

    In fact, I also wish for hierarchical schematic blocks (HSB) to be

    implemented, but they are longer down on my list than directional flags.

    HSB is also useless, imho, if they do not show the signal directions.

    Thus implementing directional flags is a step towards getting HSB and

    should therefore be on the wish list for all of us. image

     

    Have a nice weekend

     

    Breg

    Vidar (Z)

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to zainka

    Vidar (Z) wrote on Fri, 23 November 2012 04:46

    If a pin direction was fixed and you knew you wanted to show it in

    the

    schematic every time, you could even add this to the symbol in the

    library.

     

    You do not know what the direction of a MCU port pin will be, as

    already

    stated by your self, so thus adding directions symbols in the library

    is

    in my opinion lack of consistency when it comes to drawing symbols.

     

    Right, that's why I said "if".  I have only added direction symbols a few

    times in libraries.  Most of the confusion is around microcontroller pins

    that can be used different ways.  For those I add the little arrows in the

    schematic as I showed.  This is really easy.

     

    /quote

    and there are many peoples that finds this suggestion to be important

    as-well.

    I seriously doubt that.  You have latched onto this issue for some reason,

    but it's really a minor nit in the overall scheme of things.  We don't want

    CadSoft getting distracted by all the little minor nits to the point that

    the truly useful major features get less attention.  The great thing about

    Eagle is you can already do many things you wish it had on your own well

    enough.  This particular feature is a great example of that.

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • zainka
    zainka over 13 years ago in reply to e14 Contributor

    On 11/22/2012 03:43 PM, Olin Lathrop wrote:

    Joern Paschedag wrote on Thu, 22 November 2012 03:11

    >> In nowadays circuits with microcontrollers etc. most of the pins can be

    >>

    >> of plural directions,  just depending on programming.

     

    Exactly.  The pin direction in Eagle is only a very rough clue about

    whether information actually flows in, out, or both ways of a pin.  We

    already have enough problems from Eagle trying to infer too much from such

    things. For example, you end up with nuisance ERC errors when a supply pin

    named VDD is connected to +3.3V, or far worse, the supply pin VDD is

    automatically connected to the net VDD without any indication of this on

    the schematic.

     

    It is no big deal to add your own direction symbols.  I have done this

    routinely for years.  The important point is that I can chose where I want

    to show a direction and what that direction is.  I have little arrows for

    this purpose in my symbols library.  Here is a snippet of a schematic

    showing their use:

     

     

     

     

    If a pin direction was fixed and you knew you wanted to show it in the

    schematic every time, you could even add this to the symbol in the library.

     

     

    You do not know what the direction of a MCU port pin will be, as already

    stated by your self, so thus adding directions symbols in the library is

    in my opinion lack of consistency when it comes to drawing symbols.

     

      There are already plenty of easy ways to solve this problem.  Let's not

    invent yet another automatic thing for Each to get right 90% of the time,

    and more pointless busywork for the CadSoft developers.  There are plenty

    of important features to implement, like hierarchical schematic blocks for

    example.

     

    >

     

     

    But..!  the suggestion is not a suggestion to have directional flags

    that changes their sign by their own will. Nor was the original

    suggestion to have the direction flag to inherit the value by the pin it

    is connected to. The only wish I had was to be able to change the

    direction of the already existing flag by a change command. Its

    already half way implemented in the form of a flag that has the ability

    to show only one direction. Adding the option to change direction will

    in my opinion complete an existing feature

     

    The "inherit direction from nearest pin" option was only rised during

    the discussion that came after Walter at Cadsoft had some questions. but

    it is not a part of my original request and never was the intention.

     

    Finally, The correct rating of what is an "important feature" to be

    implemented is highly individual, and there are many peoples that finds

    this suggestion to be important as-well.

     

     

     

    To clear things up, These are my suggestion...:

     

     

    1) To have the option to change the flag direction by a change command

    (but the flag shall not sniff on the pins on the net, I at-least have no

    needs for that)

     

    2) To be able to choose which data to be inside and which to be outside

    the flag by using the formatting options position relative to %F ..

     

     

     

    I am sorry if I was unclear in the beginning

     

     

     

     

    Breg

    Vidar

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    Joern Paschedag wrote on Thu, 22 November 2012 03:11

    In nowadays circuits with microcontrollers etc. most of the pins can be

     

    of plural directions,  just depending on programming.

     

    Exactly.  The pin direction in Eagle is only a very rough clue about

    whether information actually flows in, out, or both ways of a pin.  We

    already have enough problems from Eagle trying to infer too much from such

    things. For example, you end up with nuisance ERC errors when a supply pin

    named VDD is connected to +3.3V, or far worse, the supply pin VDD is

    automatically connected to the net VDD without any indication of this on

    the schematic.

     

    It is no big deal to add your own direction symbols.  I have done this

    routinely for years.  The important point is that I can chose where I want

    to show a direction and what that direction is.  I have little arrows for

    this purpose in my symbols library.  Here is a snippet of a schematic

    showing their use:

     

     

     

    If a pin direction was fixed and you knew you wanted to show it in the

    schematic every time, you could even add this to the symbol in the library.

    There are already plenty of easy ways to solve this problem.  Let's not

    invent yet another automatic thing for Each to get right 90% of the time,

    and more pointless busywork for the CadSoft developers.  There are plenty

    of important features to implement, like hierarchical schematic blocks for

    example.

     

     

    --

    Web access to CadSoft support forums at www.eaglecentral.ca.  Where the CadSoft EAGLE community meets.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to zainka

    Hi,

     

    I agree with Vidar. It's the designer that should choose the right

    label. See attached... Some pins are only outputs, some are only

    inputs and some are bidirectional. If I could choose the label shape

    I could emphasize this and the design will be more readable. Label text

    inside or outside? I think it would be more beautiful if the text were

    outside and shapes had the same length...

    Best thing would be if I could choose two more shapes to the only two

    available today (arrow shape or nothing), and also if I could decide if

    the text is inside or outside.

     

    Best regards

     

    Alberto Vignati

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • zainka
    zainka over 13 years ago in reply to e14 Contributor

    > On 11/22/2012 09:11 AM, Joern Paschedag wrote:

    >

    >

    > In nowadays circuits with microcontrollers etc. most of the pins can be

    > of plural directions,  just depending on programming.

    > In plenty of revisions I made those directions pointers were mostly

    > confusing since they did not reflect the truth.

    > So imho showing a direction of labels is for the birds.

     

    I do not agree with you. A schematic that does not reflect reality is a

    poorly designed schematic. The schematic is an important documentation

    for the product and if it is not put up to date after a software change

    its value is at best reduced.

     

    Birds are free, by the way, and I prefer that...

     

    >

    > If  such a direction is "a must" for some people then it should be

    > realized just  as "show business" like A. Weidner pointed out.

    > Just keep it simple.

    >

    > The Text of a connector should be inside the frame which is

    > a:Standard in electrical drawings and otherwise

     

    Not so standard as you might think it is. I have been working both with

    Mentorgraphics and Orcad for different companies and they both have

    direction labels with net names put outside the flag as suggested above.

     

    I have also been working with many big international companies, NVIDIA

    to mention only one, and the schematics I have seen from them (which

    uses for me an unknown eCAD software) has their net names written

    outside the flag.

     

    I have also seen flags which has the shape as I outlined in my ASCII

    drawings with the words IN, OUT and BI written inside the flag and the

    net name written outside. Yet, I have seen specialized direction flags

    for buses with the shape of a bi flag with double walls. Something like

    this:

        _______

       /_______\

    _//      

     
    _______//

       \_______/

     

     

    So the standard you referee to is not so standard after all.

     

     

    > b: might be confused with normal text nearby.

    >

     

    Its the designer that has the power and responsible to avoid putting

    text so close together that the viewer might get confused. If so has

    been done then the design and documentation of the product is of poor

    quality in my point of view.

     

    Breg

    Vidar (Z)

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to CSWalt

    Am 21.11.2012 23:32, schrieb Walter.Spermann@cadsoft.de:

    Hi,

     

    On 11/21/2012 10:25 AM, Andreas Weidner wrote:

    >> I do not care about text OUTSIDE the label frame (it will always stay

    >> INSIDE for me), but I also would very much like to

    >> see in/out/bi labels as outlined.

    >>

    >> Am 20.11.2012 18:22, schrieb Walter Spermann:

    >>>> input bi output

    >>>> _______ ______ ______

    >>>> _/ | / \ | \

    >>>> \_______| \______/ |______/

    >>>>

    >>> Thanks, but some questions on this:

    >>> - What flags would you set if the net has many (>2) pin connections ?

    >>

    >> The form of the label MUST NOT be set automatically! Please leave it

    >> in the responsibility of the user to select the

    >> appropriate form and make the following choices available: INPUT and

    >> OUTPUT and BIDIRECTIONAL as shown above, and

    >> perhaps even RECTANGLE, which is a simple surrounding rectangle with

    >> no directional information.

    >>

    >>> - How should it behave is a user has a net with unlogical

    >>> connections, say input - input ?

    >>

    >> As stated above, the label form is NOT changed automatically, and

    >> therefore, no 'behaviour' is necessary at all. Also,

    >> please no ERC checks or anything else. Just graphics. Easy to program,

    >> no hassles, no automatisms.

    I forgot to mention change package, replace and library update: If the

    adjacent pins change, the labels

    would have to be adapted. I think choosing a simple solution as you

    suggest is better here. Thanks.

     

    Walter Spermann

     

    >>

    >>> This can cause confusion.

    >>

    >> Without automatisms, confusion won't be possible (other than the user

    >> labelling nets with the WRONG graphics, but that's

    >> the user's fault, then, and not CadSoft's).

    >>

    >> Andreas Weidner

     

    In nowadays circuits with microcontrollers etc. most of the pins can be

    of plural directions,  just depending on programming.

    In plenty of revisions I made those directions pointers were mostly

    confusing since they did not reflect the truth.

    So imho showing a direction of labels is for the birds.

     

    If  such a direction is "a must" for some people then it should be

    realized just  as "show business" like A. Weidner pointed out.

    Just keep it simple.

     

    The Text of a connector should be inside the frame which is

    a:Standard in electrical drawings and otherwise

    b: might be confused with normal text nearby.

     

    By for more important I consider a separate size of labels, independent

    of the text size.

    It is a horror if placing text and labels of different sizes and to

    adjust the sizes each time.

     

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • CSWalt
    CSWalt over 13 years ago in reply to e14 Contributor

    Hi,

     

    On 11/21/2012 10:25 AM, Andreas Weidner wrote:

    I do not care about text OUTSIDE the label frame (it will always stay INSIDE for me), but I also would very much like to

    see in/out/bi labels as outlined.

     

    Am 20.11.2012 18:22, schrieb Walter Spermann:

    >>> input bi output

    >>> _______ ______ ______

    >>> _/ | / \ | \

    >>> \_______| \______/ |______/

    >>>

    >> Thanks, but some questions on this:

    >> - What flags would you set if the net has many (>2) pin connections ?

     

    The form of the label MUST NOT be set automatically! Please leave it in the responsibility of the user to select the

    appropriate form and make the following choices available: INPUT and OUTPUT and BIDIRECTIONAL as shown above, and

    perhaps even RECTANGLE, which is a simple surrounding rectangle with no directional information.

     

    >> - How should it behave is a user has a net with unlogical connections, say input - input ?

     

    As stated above, the label form is NOT changed automatically, and therefore, no 'behaviour' is necessary at all. Also,

    please no ERC checks or anything else. Just graphics. Easy to program, no hassles, no automatisms.

    I forgot to mention change package, replace and library update: If the adjacent pins change, the labels

    would have to be adapted. I think choosing a simple solution as you suggest is better here. Thanks.

     

    Walter Spermann

     

    >> This can cause confusion.

     

    Without automatisms, confusion won't be possible (other than the user labelling nets with the WRONG graphics, but that's

    the user's fault, then, and not CadSoft's).

     

    Andreas Weidner

     

    --

    -


    Walter Spermann

    Softwareentwicklung

    CadSoft Computer GmbH

    Pleidolfweg 15

    84568 Pleiskirchen

    Tel.: 08635/6989-10

    www.cadsoft.de

    -


    Registergericht: Amtsgericht Traunstein HRB 5573

    Geschäftsführer: Thomas Liratsch

    -


     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • zainka
    zainka over 13 years ago in reply to e14 Contributor

    On 11/21/2012 10:25 AM, Andreas Weidner wrote:

    I do not care about text OUTSIDE the label frame (it will always stay

    INSIDE for me), but I also would very much like to see in/out/bi labels

    as outlined.

     

    By implementing the proposed 'position dependent xref tag setup' Eagle

    will become flexible enough to meet most peoples wishes in a simple

    manner. A program that puts the user in the front seat is a good

    program. (well almost always). Eagle should default to already existing

    xref formatting of-course and leaving it up to the user to change it to

    whatever they need.

     

     

    As stated above, the label form is NOT changed automatically, and

    therefore, no 'behaviour' is necessary at all. Also, please no ERC

    checks or anything else. Just graphics. Easy to program, no hassles, no

    automatisms.

     

    This can be made as an option to choose automated direction setting

    based on the nearest pin, or if it must be set manually. I guess

    defaulting to 'input' is the most logical choice when set to manual

    since the existing flag label has the form of an input flag.

     

    But, I my self agree that only manual setting of the direction is

    necessary as it also force the user to think throughly through the

    design. That has never hurt anyone and as also stated, the flag is only

    a way of visualizing the actual signal flow and making a schematic more

    readable

     

    ERC should off course not reflect if the chosen label flag direction

    shows the direction of the pin connected to or not. A flag showing a

    direction is, once again, only a visualization of the signal flow as

    seen from the user perspective view, and it must be possible to set to

    whatever direction one wants regardless of the direction of the pin one

    connects to.

     

    This is called KIS design (Keep It Simple)

     

    >> This can cause confusion.

     

    Without automatisms, confusion won't be possible (other than the user

    labelling nets with the WRONG graphics, but that's the user's fault,

    then, and not CadSoft's).

     

     

    In the end, what brings confusion is highly individual. So in stead of

    arguing for or against I repeat the humble words of Aristotle:

     

    "To say of what is that it is not, or of what is not that it is, is

    false, while to say of what is that it is, and of what is not that it is

    not, is true."

     

     

     

    Breg

    Vidar (Z)

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to CSWalt

    I do not care about text OUTSIDE the label frame (it will always stay

    INSIDE for me), but I also would very much like to see in/out/bi labels

    as outlined.

     

    Am 20.11.2012 18:22, schrieb Walter Spermann:

    >> input             bi              output

    >>    _______          ______         ______

    >> _/       |       /      \       |      \

    >>   \_______|        \______/       |______/

    >>

    Thanks, but some questions on this:

      - What flags would you set if the net has many (>2) pin connections ?

     

    The form of the label MUST NOT be set automatically! Please leave it in

    the responsibility of the user to select the appropriate form and make

    the following choices available: INPUT and OUTPUT and BIDIRECTIONAL as

    shown above, and perhaps even RECTANGLE, which is a simple surrounding

    rectangle with no directional information.

     

      - How should it behave is a user has a net with unlogical connections, say input - input ?

     

    As stated above, the label form is NOT changed automatically, and

    therefore, no 'behaviour' is necessary at all. Also, please no ERC

    checks or anything else. Just graphics. Easy to program, no hassles, no

    automatisms.

     

    This can cause confusion.

     

    Without automatisms, confusion won't be possible (other than the user

    labelling nets with the WRONG graphics, but that's the user's fault,

    then, and not CadSoft's).

     

    Andreas Weidner

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
<>