Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Import DXF file in Eagle Pro 6.2.0
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 188 subscribers
  • Views 4685 views
  • Users 0 members are here
Related

Import DXF file in Eagle Pro 6.2.0

e14 Contributor
e14 Contributor over 13 years ago

Hello,

 

Do you know how i can import a dxf file in eagle pro 6.2.0?

  • Sign in to reply
  • Cancel
  • skyflyrr
    skyflyrr over 12 years ago in reply to e14 Contributor

    Jorge,

     

    Can you send me the dxfimport.ulp please. I've tried various ulp's without success.

     

    Best bet is to send it to bmoreno@fireflyrfid.com

     

    Thank you,

     

    Bob Moreno

    firefly RFID

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to e14 Contributor

    On 4/12/2013 4:48 PM, Richard Karlquist wrote:

    Both the successful and unsuccessful .dxf files use splines.  They are

    not binary files.  The only unique type in the unsuccessful one is

    "CEPSN TYPE".  However, shouldn't the ULP at least import the types it

    knows about, or produce some sort of error message?  It just happily

    reports zero lines, zero circles, etc.  The .dxf files are being

    produced by my mechanical engineer with his CAD program, so I am not in

    a position to waste his time with endless experimentation with .dxf

    files.  He already tried several different CAD programs that output

    dxf.   I guess there is no documentation as to what is or is not

    supported.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/74032#74032

     

     

    Hi Richard,

     

    There's more to it than that. The SPLINES are never imported because the

    ULP doesn't support that yet. As of now the ULP supports the following:

     

    LINES,

    ARCS

    CIRCLES,

    POLYLINES,

    and

    LWPOLYLINES

     

    That's it, the file that imports properly has one or more of these

    elements. The one that doesn't lacks these completely.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to autodeskguest

    Both the successful and unsuccessful .dxf files use splines.  They are not binary files.  The only unique type in the unsuccessful one is "CEPSN TYPE".  However, shouldn't the ULP at least import the types it knows about, or produce some sort of error message?  It just happily reports zero lines, zero circles, etc.  The .dxf files are being produced by my mechanical engineer with his CAD program, so I am not in a position to waste his time with endless experimentation with .dxf files.  He already tried several different CAD programs that output .dxf.   I guess there is no documentation as to what is or is not supported.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to e14 Contributor

    On 4/11/2013 10:44 PM, Richard Karlquist wrote:

    I tried using the ULP "dxfimport".  It worked on a .dxf file that I

    exported from Visio, but it did not work on a file I exported from a

    mechanical engineering program.  In the latter case, it said there were

    zero wires, etc; zero of everything.  The file that worked had Imperial

    units and the one that didn't was metric.  I did remember to select the

    correct units in the dialog box.  What other reason would explain a file

    being DOA?  BTW, the file imports into Visio OK.

     

    Rick Karlquist

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/73966#73966

     

    Hi Rick,

     

    I hope you're doing well. The DXF standard supports many types of

    objects, texts, lines, arcs, polylines, etc. The dxfimport.ulp currently

    implements the most common objects. However there are still programs

    that export designs as SPLINES or other less frequent object types and

    the ULP currently can't handle them. Also Binary DXFs exist versus the

    text based ones the ULP is setup to handle so you have to make sure

    you're using a text based DXF file.

     

    If you're program can export various types of DXF files try the

    different forms out and see what you get.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago

    I tried using the ULP "dxfimport".  It worked on a .dxf file that I exported from Visio, but it did not work on a file I exported from a mechanical engineering program.  In the latter case, it said there were zero wires, etc; zero of everything.  The file that worked had Imperial units and the one that didn't was metric.  I did remember to select the correct units in the dialog box.  What other reason would explain a file being DOA?  BTW, the file imports into Visio OK.

     

    Rick Karlquist

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    On 12/18/2012 6:42 PM, shabaz wrote:

    Hi Jorge,

     

    No problem at all, you're welcome to port or to make use of it however you wish. Unfortunately I was only familiar with the script commands, not ULP.

    HPGL is a nice format because it is quite simplistic!

     

     

    Thanks Shabaz,

     

    I will get on it, and thanks for your contribution to the community.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • shabaz
    shabaz over 13 years ago in reply to e14 Contributor

    Hi Jorge,

     

    No problem at all, you're welcome to port or to make use of it however you wish. Unfortunately I was only familiar with the script commands, not ULP.

    HPGL is a nice format because it is quite simplistic!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    On 12/18/2012 3:01 AM, grigson prendergast wrote:

    Thankyou i read your link etc.but i still dont understand what all this process of getting a dxf into eagle is all about.

     

    I mean, the only thing that can be brought into an eagle layotu is a part, so do i have to convert the dxf file into a part?

    No you don't convert the DXF file into a part, although you can if you

    want to.

     

    ...is there a youtube video that i can see that shows the dxf import process?

     

    Am i just being a bit weak and pathetic here, because this whole concept of dxf import into Eagle via these ULP's sounds liek rocket science to me.

     

    ...should i just get on with it, and when i start clcking the conversion ULP, everything will just happen before my eyes , so to speak?

     

    I've attached the dxfimport.ulp, hopefully it makes it to you. All you

    have to do to use it is type RUN followed by enter in one of the

    editors. Browse to the ULP and hit open. The ULP will now run and

    present you with an easy to follow dialog.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    On 12/17/2012 5:27 PM, shabaz wrote:

    Personally I didn't have much luck with some user language programs for DXF (maybe they have improved, I checked over a year ago so my

    information could be old).

     

    But, I found a nice method which works well, and can work for some other popular file formats too.

    Basically the trick is to use an in-between format. I found that inkscape (freeware) is good at reading DXF and can convert to HPGL format.

    I picked HPGL format because it is a trivial exercise to convert that to EAGLE script format. More info on it is here (http://badcafe.co.uk/2011/03/20/dxf-hpgl-to-eagle-script-conversion/).

     

     

    Hi Shabaz,

     

    This looks very cool, I would encourage you to upload this script to

    www.cadsoftusa.com for the benefit of other EAGLE users. Additionally I

    would like your permission to port the code over to EAGLE's ULP language

    to make a more integrated utility in EAGLE.

     

    The importdxf utility I mentioned is newer than a year old and I

    basically combined the best parts of the existing DXF import tools along

    with some new functionality to make a ULP that could import 75% of the

    DXF files you'll run into. I would like to do something similar with

    your utility especially for the possibility to import various image

    formats into EAGLE. I will give proper attribution as would be expected

    in the open source community.

     

    Best Regards,

    Jorge Garcia

    Cadsoft Support

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to shabaz

    Thankyou i read your link etc.but i still dont understand what all this process of getting a dxf into eagle is all about.

     

    I mean, the only thing that can be brought into an eagle layout is a part, so do i have to convert the dxf file into a part?

     

    ....is there a youtube video that i can see that shows the dxf import process?

     

    Am i just being a bit weak and pathetic here, because this whole concept of dxf import into Eagle via these ULP's sounds liek rocket science to me.

     

    ....should i just get on with it, and when i start clcking the conversion ULP, everything will just happen before my eyes , so to speak?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>