Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Import DXF file in Eagle Pro 6.2.0
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 12 replies
  • Subscribers 188 subscribers
  • Views 4686 views
  • Users 0 members are here
Related

Import DXF file in Eagle Pro 6.2.0

e14 Contributor
e14 Contributor over 13 years ago

Hello,

 

Do you know how i can import a dxf file in eagle pro 6.2.0?

  • Sign in to reply
  • Cancel
Parents
  • e14 Contributor
    e14 Contributor over 13 years ago

    I tried using the ULP "dxfimport".  It worked on a .dxf file that I exported from Visio, but it did not work on a file I exported from a mechanical engineering program.  In the latter case, it said there were zero wires, etc; zero of everything.  The file that worked had Imperial units and the one that didn't was metric.  I did remember to select the correct units in the dialog box.  What other reason would explain a file being DOA?  BTW, the file imports into Visio OK.

     

    Rick Karlquist

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to e14 Contributor

    On 4/11/2013 10:44 PM, Richard Karlquist wrote:

    I tried using the ULP "dxfimport".  It worked on a .dxf file that I

    exported from Visio, but it did not work on a file I exported from a

    mechanical engineering program.  In the latter case, it said there were

    zero wires, etc; zero of everything.  The file that worked had Imperial

    units and the one that didn't was metric.  I did remember to select the

    correct units in the dialog box.  What other reason would explain a file

    being DOA?  BTW, the file imports into Visio OK.

     

    Rick Karlquist

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/73966#73966

     

    Hi Rick,

     

    I hope you're doing well. The DXF standard supports many types of

    objects, texts, lines, arcs, polylines, etc. The dxfimport.ulp currently

    implements the most common objects. However there are still programs

    that export designs as SPLINES or other less frequent object types and

    the ULP currently can't handle them. Also Binary DXFs exist versus the

    text based ones the ULP is setup to handle so you have to make sure

    you're using a text based DXF file.

     

    If you're program can export various types of DXF files try the

    different forms out and see what you get.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to autodeskguest

    Both the successful and unsuccessful .dxf files use splines.  They are not binary files.  The only unique type in the unsuccessful one is "CEPSN TYPE".  However, shouldn't the ULP at least import the types it knows about, or produce some sort of error message?  It just happily reports zero lines, zero circles, etc.  The .dxf files are being produced by my mechanical engineer with his CAD program, so I am not in a position to waste his time with endless experimentation with .dxf files.  He already tried several different CAD programs that output .dxf.   I guess there is no documentation as to what is or is not supported.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to autodeskguest

    Both the successful and unsuccessful .dxf files use splines.  They are not binary files.  The only unique type in the unsuccessful one is "CEPSN TYPE".  However, shouldn't the ULP at least import the types it knows about, or produce some sort of error message?  It just happily reports zero lines, zero circles, etc.  The .dxf files are being produced by my mechanical engineer with his CAD program, so I am not in a position to waste his time with endless experimentation with .dxf files.  He already tried several different CAD programs that output .dxf.   I guess there is no documentation as to what is or is not supported.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • autodeskguest
    autodeskguest over 13 years ago in reply to e14 Contributor

    On 4/12/2013 4:48 PM, Richard Karlquist wrote:

    Both the successful and unsuccessful .dxf files use splines.  They are

    not binary files.  The only unique type in the unsuccessful one is

    "CEPSN TYPE".  However, shouldn't the ULP at least import the types it

    knows about, or produce some sort of error message?  It just happily

    reports zero lines, zero circles, etc.  The .dxf files are being

    produced by my mechanical engineer with his CAD program, so I am not in

    a position to waste his time with endless experimentation with .dxf

    files.  He already tried several different CAD programs that output

    dxf.   I guess there is no documentation as to what is or is not

    supported.

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/74032#74032

     

     

    Hi Richard,

     

    There's more to it than that. The SPLINES are never imported because the

    ULP doesn't support that yet. As of now the ULP supports the following:

     

    LINES,

    ARCS

    CIRCLES,

    POLYLINES,

    and

    LWPOLYLINES

     

    That's it, the file that imports properly has one or more of these

    elements. The one that doesn't lacks these completely.

     

    hth,

    Jorge Garcia