Hello,
Do you know how i can import a dxf file in eagle pro 6.2.0?
Hello,
Do you know how i can import a dxf file in eagle pro 6.2.0?
I tried using the ULP "dxfimport". It worked on a .dxf file that I exported from Visio, but it did not work on a file I exported from a mechanical engineering program. In the latter case, it said there were zero wires, etc; zero of everything. The file that worked had Imperial units and the one that didn't was metric. I did remember to select the correct units in the dialog box. What other reason would explain a file being DOA? BTW, the file imports into Visio OK.
Rick Karlquist
On 4/11/2013 10:44 PM, Richard Karlquist wrote:
I tried using the ULP "dxfimport". It worked on a .dxf file that I
exported from Visio, but it did not work on a file I exported from a
mechanical engineering program. In the latter case, it said there were
zero wires, etc; zero of everything. The file that worked had Imperial
units and the one that didn't was metric. I did remember to select the
correct units in the dialog box. What other reason would explain a file
being DOA? BTW, the file imports into Visio OK.
Rick Karlquist
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/73966#73966
Hi Rick,
I hope you're doing well. The DXF standard supports many types of
objects, texts, lines, arcs, polylines, etc. The dxfimport.ulp currently
implements the most common objects. However there are still programs
that export designs as SPLINES or other less frequent object types and
the ULP currently can't handle them. Also Binary DXFs exist versus the
text based ones the ULP is setup to handle so you have to make sure
you're using a text based DXF file.
If you're program can export various types of DXF files try the
different forms out and see what you get.
hth,
Jorge Garcia
On 4/11/2013 10:44 PM, Richard Karlquist wrote:
I tried using the ULP "dxfimport". It worked on a .dxf file that I
exported from Visio, but it did not work on a file I exported from a
mechanical engineering program. In the latter case, it said there were
zero wires, etc; zero of everything. The file that worked had Imperial
units and the one that didn't was metric. I did remember to select the
correct units in the dialog box. What other reason would explain a file
being DOA? BTW, the file imports into Visio OK.
Rick Karlquist
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/73966#73966
Hi Rick,
I hope you're doing well. The DXF standard supports many types of
objects, texts, lines, arcs, polylines, etc. The dxfimport.ulp currently
implements the most common objects. However there are still programs
that export designs as SPLINES or other less frequent object types and
the ULP currently can't handle them. Also Binary DXFs exist versus the
text based ones the ULP is setup to handle so you have to make sure
you're using a text based DXF file.
If you're program can export various types of DXF files try the
different forms out and see what you get.
hth,
Jorge Garcia
On 4/12/2013 4:48 PM, Richard Karlquist wrote:
Both the successful and unsuccessful .dxf files use splines. They are
not binary files. The only unique type in the unsuccessful one is
"CEPSN TYPE". However, shouldn't the ULP at least import the types it
knows about, or produce some sort of error message? It just happily
reports zero lines, zero circles, etc. The .dxf files are being
produced by my mechanical engineer with his CAD program, so I am not in
a position to waste his time with endless experimentation with .dxf
files. He already tried several different CAD programs that output
dxf. I guess there is no documentation as to what is or is not
supported.
--
To view any images and attachments in this post, visit:
http://www.element14.com/community/message/74032#74032
Hi Richard,
There's more to it than that. The SPLINES are never imported because the
ULP doesn't support that yet. As of now the ULP supports the following:
LINES,
ARCS
CIRCLES,
POLYLINES,
and
LWPOLYLINES
That's it, the file that imports properly has one or more of these
elements. The one that doesn't lacks these completely.
hth,
Jorge Garcia
Both the successful and unsuccessful .dxf files use splines. They are not binary files. The only unique type in the unsuccessful one is "CEPSN TYPE". However, shouldn't the ULP at least import the types it knows about, or produce some sort of error message? It just happily reports zero lines, zero circles, etc. The .dxf files are being produced by my mechanical engineer with his CAD program, so I am not in a position to waste his time with endless experimentation with .dxf files. He already tried several different CAD programs that output .dxf. I guess there is no documentation as to what is or is not supported.