Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) APPCRASH EAGLE 6.4 on WIN 7 64
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 34 replies
  • Subscribers 195 subscribers
  • Views 5022 views
  • Users 0 members are here
  • eagle
Related

APPCRASH EAGLE 6.4 on WIN 7 64

terje
terje over 13 years ago

Dear the support team at Cadsoft!

I have just purchased and installed Eagle pro shematic and layout package on to my brand new win 7 64 computer.

 

I'm now trying to design some new components with the library editor but every 3 to 10 minutes the application crashes and the work is lost.

To me it appears that the crash happens randomly. It can happen when I'm resizing the window, moving a element, copy a element, changing the grid. pushing the undo button  etc. etc.

For now the Eagle is useless as this happens too frequently.

 

The eagle program is installed under C:\eagle

The version is 6.4.0.

 

What did I do wrong?

 

Is this a known issue?

 

 

 

Windows crash report:

 

Problem event name: APPCRASH

Programname: eagle.exe

Programversion: 0.0.0.0

Timestamp for program: 50eaf0df

Error module name: ntdll.dll

Error module version: 6.1.7601.17725

Timestamp on error module: 4ec49b8f

Exeption code: c0000005

Exeption scew: 0002e3be

OS-versjon: 6.1.7601.2.1.0.256.48

ID for national setting: 1044

Additional information 1: 0a9e

Additional information2: 0a9e372d3b4ad19135b953a78882e789

Additional information3: 0a9e

Additional information4: 0a9e372d3b4ad19135b953a78882e789

 

 

 

Best Regards

Terje

  • Sign in to reply
  • Cancel
Parents
  • Krycek
    Krycek over 13 years ago

    I am having the same problems using 6.4.0 under Windows 7 64 bit.

     

    First I could get the app to crash while editing text properties in the schematic editor but now I have just lost a lot of work in the library editor when editing the properties of a plated through hole drill size when modifying an existing part.

     

    When I booted Eagle 6.4.0 back up it had lost the working directory I use as well as where my libraries are stored and reverted back to defaults.

     

    My projects and library files are saved on a network drive and have been since I first started using Eagle at version 6.0 so its not that - I have reverted back to 6.3 so I can continue working on an urgent project.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to Krycek

    TO ALL:

         The problem is with all 32bit programs running within the 64bit Windows. Change from 64 to 32 and probelm solved. From the day Windows XP was avalilable in 32bit and 64bit mode, it has been a problem. And it has not been solved.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • auspoundy
    auspoundy over 13 years ago in reply to e14 Contributor

    This is NOT an x64 vs x86 64-bit/32-bit issue. The app has worked reliably in 6.3.0 on x64 so I strongly feel it's something that has changed in 6.4.0 that is causing the instability.

     

    I too have moved my projects and libraries to a different location. It is on a different logical partition on the same physical hard drive - it's a laptop so it's not network connected.

     

    One of the real issues here that Cadsoft should be taking into account here is that the "user data" store should not default to be inside the program files directory. That's the reason people change these locations - and that's why they should make that a part of the design.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Krycek
    Krycek over 13 years ago in reply to Krycek

    I have just tried the BETA 6.4.2 and I can confirm that changing properties on text as well as opening and closing the help screen haven't caused this version to crash on my system. Fingers crossed for a full release soon.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 13 years ago in reply to COMPACT

    I uninstalled EAGLE 6.4 to trial EAGLE 6.4.2 beta. The crashing has stopped. This is great news.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 13 years ago in reply to COMPACT

    Note to all: Even running EAGLE as administrator has the identical behaviour.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • COMPACT
    COMPACT over 13 years ago in reply to wardelder

    I reported this issue with EAGLE support when I got my new PC (with Windows 8 64-bit) in February but it was promptly dismissed as a user installation error.

     

    This blog trail has confirmed that it was not me and there is actually a fault.

     

    I can confirm that the Press F1 for help and closing the subsequent help dialog box is the fastest way of getting the error.

     

    As a guess it'll be a single cause creating this angst.

     

    Hopefully it will be fixed soon.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • wardelder
    wardelder over 13 years ago in reply to Krycek

    I just installed Eagle 6.4.0 on my second Win7 x64 machine and it works fine.  Both machines are laptops with Win7 x64.  One works, one fails (solid/repeatable failures).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Krycek
    Krycek over 13 years ago in reply to Krycek

    I have this exact same problem with the BETA 6.4.1 so it looks like it hasn't been addressed yet.

     

    Still using 6.3.0 here at work to over come this but I am being asked to start to roll out Eagle to new development engineers and the environment will be the same : Windows 7 64 bit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Krycek
    Krycek over 13 years ago in reply to Krycek

    I have this exact same problem with the BETA 6.4.1 so it looks like it hasn't been addressed yet.

     

    Still using 6.3.0 here at work to over come this but I am being asked to start to roll out Eagle to new development engineers and the environment will be the same : Windows 7 64 bit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • wardelder
    wardelder over 13 years ago in reply to Krycek

    I just installed Eagle 6.4.0 on my second Win7 x64 machine and it works fine.  Both machines are laptops with Win7 x64.  One works, one fails (solid/repeatable failures).