Autodesk EAGLE
  • Products
  • More
Autodesk EAGLE
EAGLE User Support (English) Have a question about CadSoft EAGLE?  Ask our Expert, Jorge!
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 126 replies
  • Subscribers 200 subscribers
  • Views 10894 views
  • Users 0 members are here
  • our
  • have
  • expert
  • eagle?
  • jorge!
  • ask
  • a
  • cadsoft
  • about
  • question
Related

Have a question about CadSoft EAGLE?  Ask our Expert, Jorge!

Jorge_Garcia
Jorge_Garcia over 13 years ago

If you have questions about CadSoft EAGLE, please click here to post your question!


If you'd rather browse other member's questions you can read the CadSoft EAGLE Forums for past questions and answers. Enjoy!

 

richardhammerl.png

 

Jorge Garcia

I'm a young engineer with extensive experience working on EAGLE. My interests include Power Supply design and LED solid state lighting, and I'm always impressed by a well designed PCB.

 

 

If not already, you'll need to

image or image

 


to ask your question.

Otherwise, click reply below.

  • Sign in to reply
  • Cancel
  • Jorge_Garcia
    Jorge_Garcia over 10 years ago in reply to e14 Contributor

    Hello Wayne,

     

    I hope you're doing well. Without seeing gerbers it's hard to tell, but if I had to guess, you might have accidentally added the stopmask layer (tStop) to the copper layer gerber. The space between the mask openings is very small on this board and visually it might trick you into thinking that the pins are shorted into four groups.

     

    If you wish you can send me the files for review to support@cadsoftusa.com.

     

    Let me know if there's anything else I can do for you.

     

    Best regards,

    Jorge Garcia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hello Jorge,

     

    When I try to create gerbers from a board file for the Arduino Pro Mini reference file the pads for the SMT Atmel CPU are shorted together in 4 groups.

    Also other shorts occur as it appears to be filling some of the gaps with copper. I am using the reference board file found at

     

    https://www.arduino.cc/en/uploads/Main/arduino-pro-mini-reference-design.zip

     

    What am I doing wrong?  I used the standard CAM Processor job file gerb274x.cam that is included with the freeware version.

     

    Thanks,

    Wayne

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Jorge_Garcia
    Jorge_Garcia over 10 years ago in reply to autodeskguest

    Hi Henry,

     

    I hope you're doing well. The library receives it's name when you save it, so there isn't really a separate field for that. Components have value placeholders in the library >VALUE this place holder gets replaced by the actual value once you put the part in a design.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to e14 Contributor

    On 11/18/2015 4:01 PM, Chris Nel wrote:

    Thank you Jorge! I really appreciate such a rapid response. I did search

    the help file but I never considered the 'invoke' command. Brilliant!

    Kind regards, Chris

     

    Hi Chris,

     

    Just to clear this up, Rob Pearce was the one that responded. When we

    respond from the forums element14 just shows users as Cadsoft Guest.

     

    Thanks Rob.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to autodeskguest

    Thank you Jorge! I really appreciate such a rapid response. I did search the help file but I never considered the 'invoke' command. Brilliant! Kind regards, Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 10 years ago in reply to e14 Contributor

    On 17/11/15 19:50, Chris Nel wrote:

    Hi Jorge,

    I have only just started using Eagle CAD so this question probably has

    an easy answer. I have added an 74AC04N to my schematic but there are no

    pins available for the ground and Vcc pins (pins 1 and 14). on error

    checking, the software tells me that there is no supply connected. How

    do I do this?

    Kind regards

    Chris

     

    There are two possible methods:

     

    1) use the default supply nets

    The 74xx family uses VCC and GND for supply, so if you add supply

    symbols for VCC and GND on the same schematic page, they will get

    connected automatically.

     

    2) use the seventh gate

    The 74xx04 library device consists of six identical NOT gates, marked to

    be added "NEXT", so that as you drop the gates you get six from one chip

    then start a second. However, there is a seventh gate in the device,

    which is the power pins, marked to be added on "REQUEST". The way you

    get to this is to select the INVOKE tool and click on one of the gates.

    Then you pick the power symbol and place that somewhere (coincident with

    a get will usually line up neatly) and connect your supplies to that.

     

    This is all covered in the tutorial and manual that come with Eagle.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 10 years ago

    Hi Jorge,

    I have only just started using Eagle CAD so this question probably has an easy answer. I have added an 74AC04N to my schematic but there are no pins available for the ground and Vcc pins (pins 1 and 14). When error checking, the software tells me that there is no supply connected. How do I do this?

    Kind regards

    Chris

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to e14 Contributor

    On 8/19/2015 11:16 AM, odyskar wrote:

    Hi Jorge,

     

    Is there a script with which the editors' windows size is configured

    during eagle start-up?

     

     

    Hi Odyskar,

     

    I hope you're doing well. I'm afraid the there's no command I'm aware of

    to setup the Windows size.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to pierrejean

    Hi Jorge,

     

    Is there a script with which the editors' windows size is configured during eagle start-up?

     

    Thanks!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • pierrejean
    pierrejean over 12 years ago

    Ok Lorenz, i am going to see this again..

    Thanks to you!

    Beryann

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
>