Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Custom Component Naming Error
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 5 replies
  • Subscribers 188 subscribers
  • Views 1221 views
  • Users 0 members are here
Related

Custom Component Naming Error

e14 Contributor
e14 Contributor over 13 years ago

Hi all,

 

My first post here, so apologies if I have set my post out wrong, or posted in the wrong place!

 

I am having an issue naming my custom components properly, ie getting Eagle to name them IC1, IC2, etc.

 

I believe on the schematic, you must enter the symbol editor and then set the name of the component to >NAME. This appears correctly next to my schematic symbol.

 

Then when you are in the device editor, it replaces the name with G$1 - which from my understanding of the manual is a placeholder, or the default name - no worries there. I then set the prefix to be IC.

 

However the problem arises when I place the symbol in a schematic. The name appears as IC1G$1. The numbers do increment, but I would prefer not to have the G$1 after IC1.

 

After again reading the manual, it says that G$1 should appear in the device editor, but should be replaced by the IC1 completely in the schematic. Does anyone have an idea of what I am doing wrong?

 

I have connected all the pins to the footprint.

 

If you would like screenshots to understand my problems easier, by all means let me know and I can sort them out for you.

 

Many thanks for your time,

 

Sparky

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    autodeskguest over 13 years ago

    On 9/12/2013 12:22 PM, Michael Basford wrote:

     

     

    After again reading the manual, it says that G$1 should appear in the

    device editor, but should be replaced by the IC1 completely in the

    schematic. Does anyone have an idea of what I am doing wrong?

     

    Hi Sparky,

     

    Check the addlevel of the part and make sure that it's set to Next and

    not something else. Is this a multi-gated component? If it is, then for

    the extra gates you would change the gate name to A,B,C, etc. or some

    other naming convention.

     

    We'll go from there.

     

    I have connected all the pins to the footprint.

     

     

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/88843#88843

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to autodeskguest

    Many thanks for the reply Jorge.

     

    I have made sure the step is "next", and although it is not multi-gated, I have seperated the supply pins to alow me to produce cleaner schematics ( I don't want these to be hidden, however). Perhaps that is where the problem is? I have attached a screenshot below.

     

    Sparkyimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to autodeskguest

    Many thanks for the reply Jorge.

     

    I have made sure the step is "next", and although it is not multi-gated, I have seperated the supply pins to alow me to produce cleaner schematics ( I don't want these to be hidden, however). Perhaps that is where the problem is? I have attached a screenshot below.

     

    Sparkyimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 10 years ago in reply to autodeskguest

    Even though the thread is a few years old, I had the same question and >part didn't work for me. So just in case others ask this in the future like I did... Finally figured it out though and it's adding a prefix in the device editor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 13 years ago in reply to e14 Contributor

    Am 12.09.2013 21:15, schrieb Michael Basford:

    Many thanks for the reply Jorge.

     

    I have made sure the step is "next", and although it is not multi-gated,

    I have seperated the supply pins to alow me to produce cleaner

    schematics ( I don't want these to be hidden, however). Perhaps that is

    where the problem is? I have attached a screenshot below.

     

    Sparky

     

    --

    To view any images and attachments in this post, visit:

    http://www.element14.com/community/message/88847#88847

     

     

    Hi,

     

    it seems your screenshot looks like multigate. A Gate for the

    inputs/outputs. A Gate for supply.

    Your workaround with >Part instead of >Name is a possible way.

     

    Patrick

     

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • e14 Contributor
    e14 Contributor over 13 years ago in reply to e14 Contributor

    I have managed to figure it out!

     

    Instead of typing in >NAME for each symbol, >PART provides just the IC number without the G$ part at the end.

     

    It provides the correct visual form I'm after, but if this is a fudge, I would still appreciate any help. image

     

    Many thanks again.

     

    Michael