EAGLE User Support (English) Wot, still no package land pattern vias?
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
  • Replies 31 replies
  • Subscribers 181 subscribers
  • Views 2967 views
  • Users 0 members are here
Related

Wot, still no package land pattern vias?

Former Member
Former Member over 11 years ago

The one thing I expected to be fixed in v7 was vias in land patterns. Nope, still AWOL, in spite of a glaring need for thermal transfer to ground via the center pad on some parts. What gives? When is this coming?

  • Sign in to reply
  • Cancel

Top Replies

  • autodeskguest
    autodeskguest over 11 years ago +1
    On 9/18/2014 10:58 PM, Ryan Pettigrew wrote: The one thing I expected to be fixed in v7 was vias in land patterns. Nope, still AWOL, in spite of a glaring need for thermal transfer to ground via the center…
Parents
  • autodeskguest
    autodeskguest over 11 years ago

    On 19/09/2014 2:58 p.m., Ryan Pettigrew wrote:

    The one thing I expected to be fixed in v7 was vias in land patterns.

    Nope, still AWOL, in spite of a glaring need for thermal transfer to

    ground via the center pad on some parts. What gives? When is this

    coming?

     

    Hi Ryan

     

    Since version 6 you have been able to create arbitrary pad shapes.

    Search for that in the HELP if you have over looked it.

     

    If you mean a via in a SMD without getting a DRC error or no DRC

    checking between objects within the package, I think that is yet to arrive.

     

     

     

    HTH

    Warren

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to autodeskguest

    "warrenbrayshaw"  skrev i nyhetsmeldingen: lvgk7v$oqv$1@cheetah.cadsoft.de

    ...

    On 19/09/2014 2:58 p.m., Ryan Pettigrew wrote:

    The one thing I expected to be fixed in v7 was vias in land patterns.

    Nope, still AWOL, in spite of a glaring need for thermal transfer to

    ground via the center pad on some parts. What gives? When is this

    coming?

    Since version 6 you have been able to create arbitrary pad shapes. Search

    for that in the HELP if you have over looked it.

    If you mean a via in a SMD without getting a DRC error or no DRC checking

    between objects within the package, I think that is yet to arrive.

     

    He is talking about thermal VIA. A via under the IC just to conduct heat to

    the pcb.. You can do this today by defining them as a thermal IO pins. V7

    lets you merge all those pads into a single symbol pin.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    He is talking about thermal VIA. A via under the IC just to conduct heat to

    the pcb.

    Indeed I am. Put another way, a via under the IC to conduct heat away from the IC.

     

    CadSoft Guest wrote:

     

    You can do this today by defining them as a thermal IO pins. V7

    lets you merge all those pads into a single symbol pin.

    Ah, but will the via be on the via layer, where it belongs?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • autodeskguest
    autodeskguest over 11 years ago in reply to Former Member

    On 20/09/2014 12:43 p.m., Ryan Pettigrew wrote:

    CadSoft Guest wrote:

     

     

     

    He is talking about thermal VIA. A via under the IC just to conduct

    heat to

     

    the pcb.

    Indeed I am. Put another way, a via under the IC to conduct heat away

    from the IC.

     

    CadSoft Guest wrote:

     

     

     

    You can do this today by defining them as a thermal IO pins. V7

     

    lets you merge all those pads into a single symbol pin.

    Ah, but will the via be on the via layer, where it belongs?

     

     

    There is a wee bit of confusion happening here due to terminology.

    I'll try to clarify.

     

    Only on a board can you add a VIA(mouse over the icon to confirm). When

    you add that VIA you can control the layers that VIA goes between.

    Choices are governed by the  layer specification you previously set in

    the DRC.

    The VIA is said to be on the display layer 'VIA' hence you can control

    it's visibility.

     

    In the library you create a package but you don't have access to vias

    there.  You have the similar looking icon that is PAD. (mouse over the

    icon to confirm) This is a through hole pad (PTH) the drill of which

    will always go all the way through the board.

     

    Scenario 1:

    If you are happy to have holes all the way through the board you can

    conduct the heat to the other side of the board or disperse it to any

    inner layer copper area that an inner restring of the PTH can connect

    to. You can build all of this into a package using PADS as fake vias.

     

    Scenario 2:

    If you need a thermal connector that goes between layer Top an inner

    layer of a multi layer board you would need to use a via approach as a

    via is the only object that has these properties.

     

    I cannot see a way to do this currently.

     

    If, in the board editor, you place a via onto a standalone polygon, the

    polygon of an arbitrary pad or an SMD created in a package, you get an

    overlap error when the DRC is run.

     

    You can of course draw a signal polygon onto the board and add vias with

    the same name onto it. No DRC errors arise when you do this but thats

    not we want to have to do. It should all be able to be setup in the library.

     

    Let me know if I have missed something

     

    Warren

     

     

     

     

     

     

     

     

     

     

     

     

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    Let me know if I have missed something

    Yes, apparently, you have; notably, that the title of this part of the forum is "EAGLE Suggestions", and not "EAGLE Help". I'm not asking how to work around the problem of vias not being available in Land Patterns. I'm asking why the feature is still missing after a major version change.

     

    CadSoft Guest wrote:

     

    In the library you create a package but you don't have access to vias

    there.

    Yes, this is the feature that is missing. I want it to no longer be missing, so that it is no longer necessary to work around it.

     

    CadSoft Guest wrote:

     

    Scenario 1:

    If you are happy to have holes all the way through the board you can

    conduct the heat to the other side of the board or disperse it to any

    inner layer copper area that an inner restring of the PTH can connect

    to. You can build all of this into a package using PADS as fake vias.

    Why would I want the PCB manufacturer to make a fake via when I want them to make a real via? Furthermore, isn't this just unnecessarily confusing to the PCB manufacturer, and ultimately, a less reliable way of getting the required board feature? Of course I'm not happy with having holes all the way through the board on the center pad of a surface mount part; that's why I want a tented and filled via there. image

     

     

    Your attempts to help would be better spent in supporting the request for the missing feature.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • Former Member
    Former Member over 11 years ago in reply to autodeskguest

    CadSoft Guest wrote:

     

    Let me know if I have missed something

    Yes, apparently, you have; notably, that the title of this part of the forum is "EAGLE Suggestions", and not "EAGLE Help". I'm not asking how to work around the problem of vias not being available in Land Patterns. I'm asking why the feature is still missing after a major version change.

     

    CadSoft Guest wrote:

     

    In the library you create a package but you don't have access to vias

    there.

    Yes, this is the feature that is missing. I want it to no longer be missing, so that it is no longer necessary to work around it.

     

    CadSoft Guest wrote:

     

    Scenario 1:

    If you are happy to have holes all the way through the board you can

    conduct the heat to the other side of the board or disperse it to any

    inner layer copper area that an inner restring of the PTH can connect

    to. You can build all of this into a package using PADS as fake vias.

    Why would I want the PCB manufacturer to make a fake via when I want them to make a real via? Furthermore, isn't this just unnecessarily confusing to the PCB manufacturer, and ultimately, a less reliable way of getting the required board feature? Of course I'm not happy with having holes all the way through the board on the center pad of a surface mount part; that's why I want a tented and filled via there. image

     

     

    Your attempts to help would be better spent in supporting the request for the missing feature.