Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Wiring problem on Eagle
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 15 replies
  • Answers 2 answers
  • Subscribers 189 subscribers
  • Views 4272 views
  • Users 0 members are here
  • eagle
  • wire to wire
  • symbol
Related

Wiring problem on Eagle

e14 Contributor
e14 Contributor over 10 years ago

Hello,

I got a problem because I can't wire to a component I created. First, I created a library for the component with Symbol, then Package and Device.

But when I am using this component on my schematic, I can't wire it. I used the same scale and grid for all the schematics and I updated libraries. But it is impossible to wire it.

If anyone has an idea to solve my problem ?

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 10 years ago

    On 7/22/2016 11:42 AM, djib ty wrote:

    Hello,

    I got a problem because I can't wire to a component I created. First, I created a library for the component with Symbol, then Package and Device.

    But when I am using this component on my schematic, I can't wire it. I used the same scale and grid for all the schematics and I updated libraries. But it is impossible to wire it.

    If anyone has an idea to solve my problem ?

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/202123

     

    Hi Djib,

     

    I hope you're doing well. Make sure that the part was made to a 0.1"

    grid. Also in order to see the connection points clearly turn on layer

    93 Pins in the schematic. You will now see lots of green circles one for

    each pin. The center of those circles is the connection point, all of

    your nets must start and end on the exact center of these circles(this

    is why it's important to stay on a 0.1" grid). If you don't see green

    circles on your part then that means you didn't use the PIN command and

    you need to go back to your library and create pins. One final thing to

    check make sure you are using the NET command to create your connections.

     

    Let me know if there's anything else I can do for you.

     

    Best Regards,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to autodeskguest

    Hello Jorge,

     

    I turned on layer 93 Pins on the schematic and I can see green circles for each pin of my component.

    Unfortunately, I still can't wire it because the nets don't start or end on the exact center of the circles.

    Meanwhile, I used 0.1 inch grid for Symbol, Package and Device. Then, I updated libraries but it's the same problems with nets which can't connect in the exact center of the circles.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to e14 Contributor

    Hello,

     

    From what you are saying Jorge is right, the issue is things not being on the 0.1" grid. So you need to do a few things.

     

    1) Double check your grid set up on your schematic is 0.1" still.

    2) Use the MOVE function to snap each or your components to the grid using ctrl+click on each to ensure they are correctly aligned to the grid.

    3) If you still have a problem, edit your symbol and perform the same operations as above for each of the pins in the symbol to ensure they are correctly on the grid and then replace the part in the schematic with your updated one.

     

    The steps above should hopefully resolve your problem.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to e14 Contributor

    That's great, I'm glad it's all working for you now :-)

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to autodeskguest

    I understand what you mean.

    In symbol, I don't have the exact dimensions of the connector of the sensor. But I can connect the wires.

    In package, I modified the dimensions of the connector, I put the right ones and I got the exact dimensions of my connector in the layout.

    So, I think the issue is resolved.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to rachaelp

    Yes you are right, I put the right dimensions of the pins in Package and it works. I got the right dimensions in the PCB and in the final schematic.

    I thank you a lot Rachaelp image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • e14 Contributor
    0 e14 Contributor over 10 years ago in reply to rachaelp

    Yes you are right, I put the right dimensions of the pins in Package and it works. I got the right dimensions in the PCB and in the final schematic.

    I thank you a lot Rachaelp image