Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) AC mains on a PCB ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 107 replies
  • Answers 10 answers
  • Subscribers 193 subscribers
  • Views 21292 views
  • Users 0 members are here
Related

AC mains on a PCB ?

anishkgt
anishkgt over 10 years ago

A total newbie to eagle design and PCB fab. So plase bear with on my silly questions, trying to learn.

 

I have pcb that is schematically completed with the layout. Before i start the fabrication process i need some expert advise if the components placed and the wires routed are ok for the ac mains and the others. The load here will be a transformer. The ac mains are 240VAC and all works well as designed in the schematic on a bread broad except for the load for which MOC3023 is yet to arrive from where i've ordered.

 

 

 

Thanks in advance.

 

image

 

image

  • Sign in to reply
  • Cancel
Parents
  • anishkgt
    0 anishkgt over 10 years ago

    How can the trace be routed without breaking the clearance rules from IC4 to IC1 ? maybe a jumper

     

    What would be the need for the resistor between IC4 and IC1, like a current limiter so it does not short out? Yes, its an ATmega328P Microcontroller.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    On 15.09.2016 12:53, George Thomas wrote:

    How can the trace be routed without breaking the clearance rules from IC4 to IC1 ? maybe a jumper

     

    What would be the need for the resistor between IC4 and IC1, like a current limiter so it does not short out? Yes, its an ATmega328P Microcontroller.

     

    If he's in control over the firmware, maybe the IO's can be swapped

    around a bit to allow routing to the closer IO's of IC1. I don't know if

    any of the selected IO's have special functions needed.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago in reply to autodeskguest

    There are only two pins that has the interrupt that is Pin4 and Pin5. Mentioned here. The Pin4 gets the zero crossing from IC4 and send into the pin4 of IC1.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    On 15.09.2016 13:41, George Thomas wrote:

    There are only two pins that has the interrupt that is Pin4 and Pin5. Mentioned here (https://www.arduino.cc/en/uploads/Hacking/Atmega168PinMap2.png). The Pin4 gets the zero crossing from IC4 and send into the pin4 of IC1.

     

     

    Fair enough image

     

    How about swapping space on IC4 and the bridge rectifier and move the

    buzzer away a bit? Imagine pulling the "rope" on this crossover signal

    and push the reg down below IC1, powering it in a vertical line up from

    the middle.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    On 15.09.2016 13:41, George Thomas wrote:

    There are only two pins that has the interrupt that is Pin4 and Pin5. Mentioned here (https://www.arduino.cc/en/uploads/Hacking/Atmega168PinMap2.png). The Pin4 gets the zero crossing from IC4 and send into the pin4 of IC1.

     

     

    Fair enough image

     

    How about swapping space on IC4 and the bridge rectifier and move the

    buzzer away a bit? Imagine pulling the "rope" on this crossover signal

    and push the reg down below IC1, powering it in a vertical line up from

    the middle.