Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) AC mains on a PCB ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 107 replies
  • Answers 10 answers
  • Subscribers 193 subscribers
  • Views 21256 views
  • Users 0 members are here
Related

AC mains on a PCB ?

anishkgt
anishkgt over 10 years ago

A total newbie to eagle design and PCB fab. So plase bear with on my silly questions, trying to learn.

 

I have pcb that is schematically completed with the layout. Before i start the fabrication process i need some expert advise if the components placed and the wires routed are ok for the ac mains and the others. The load here will be a transformer. The ac mains are 240VAC and all works well as designed in the schematic on a bread broad except for the load for which MOC3023 is yet to arrive from where i've ordered.

 

 

 

Thanks in advance.

 

image

 

image

  • Sign in to reply
  • Cancel
  • beic
    0 beic over 8 years ago

    I know it's a old topic, but I'm little bit confused about varistors mentioned above.

     

    B72210S0231K101 and B72210S0271K101 from EPCOS / TDK

     

    are these interchangeable with the:

     

    10D241K and 10D271K from BURNS (because I have them at home)

     

    Thank you!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago

    Thanks to you layout is looking better.image I've moved IC4,5 and B1 such that the GND planes do go underneath them. The connectors are the same since first and they fit with what i can get locally.

     

    Do you need to provide a star point connection between 0V and mains earth? Should you use a mains isolation transformer outside of this unit? Etc....

    I did not get hat you meant here. Please explain............ image

     

    Updated Layout follows

    image

    Update:

                   The earthing would be connecting the GND to the earth. I guess that should solve the safety side of things.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    Hi George,

     

    Your latest layout is definitely improved over earlier versions although I still think there are quite a few things that can still be done to improve things. The clearances are better but not perfect, I'd also try to ensure there are no planes encroaching underneath, IC4/5, B1. I see you still haven't changed the connectors although you had selected some 5.08mm ones in an earlier post if I recall. Why have you chosen not to go with these?

     

    You should also think about the "what if" cases for faults which could allow dangerous mains voltages to appear on the low voltage circuitry (e.g. a fault in TR1). Do you need to provide a star point connection between 0V and mains earth? Should you use a mains isolation transformer outside of this unit? Etc....

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago

    Oh ok.

     

    i guess all is done here. One of them say i've missed the safe distance that i had to keep. How would you consider this layout ?

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    Am 22.09.2016 um 11:08 schrieb George Thomas:

    hmmmm where did everyone go ?

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/206137

     

     

    Tired I suppose. After 3 weeks of support by different people you still

    have not learned to keep the safety distance on the AC tracks.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    Hi George,

     

    Sorry I have been away and not had chance to look at your follow up yet.  Also, I think the link between E14 and the EAGLE newsgroups is broken again (ChristyZ can you check please) as there is lots happening on various threads on EAGLE Central which aren't getting here to E14. You've had at least one reply on there this morning which hasn't made it over here. See: http://www.eaglecentral.ca/index.php/mv/msg/52625/0/100/ce1065d559d9c90166f1a47cd35a9817/

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    On 22.09.2016 11:08, George Thomas wrote:

    hmmmm where did everyone go ?

     

     

    I guess there is a limit to how much ppl will engage in other projects..

    It looks to me like you have sorted the HVAC/DC isolation now. Did you

    read my post about isolating the high voltage welding spots?

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago

    hmmmm where did everyone go ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago

    And now look at the strange angled trace from the '+' pin of B1 which is almost (possibly is) touching the '-' pin. If you don't route at ugly odd angles you wont do this. Use the right mouse button when in routing mode to cycle through the bend styles or use the buttons at the top and use the two 45 degree ones (hint: you need to use both 45 degree styles depending on which way you'd like it to route)

    How could i miss that i did notice it earlier but slipped it, changed it now. Thanks for that.

     

    I've replaced the TVS at the DC side to this and changed the AC side too.

     

    This is sensible advice, I believe I mentioned in earlier posts my concerns about the lack of an earth connection. It all comes back to safety.

    I did notice that suggestion and kept it to be done at the end. So would that go ? just connect it to the earth terminal from the mains ?

    image

    Update: rotated the C1 and C2 for a better route.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    George Thomas wrote:

     

    added AC tvs and PTC

    It looks like you have put the TVS in series with the AC input. This is not correct, it should go in parallel with it.

     

    George Thomas wrote:

     

    Update:

         Rachel the TVS used here are quite big in size, approximately 5mm hence the size in the layout.

     

    The TVS in those DC side locations don't need to be that big. The power rating of 1500W is excessive for where it's located so you could choose smaller ones if you were running out of space.

     

    Rachael wrote:

     

    Finally, It's going to sound nit picky, but I don't like the traces as strange angles.

    And now look at the strange angled trace from the '+' pin of B1 which is almost (possibly is) touching the '-' pin. If you don't route at ugly odd angles you wont do this. Use the right mouse button when in routing mode to cycle through the bend styles or use the buttons at the top and use the two 45 degree ones (hint: you need to use both 45 degree styles depending on which way you'd like it to route)

     

    Morten Leikvoll wrote:

     

    The design looks earthless (isoladed AC). I don't know if there are any compliance rules that says you need to do that, but the fact that the LOAD is ext to pcb, and you are probably exposing the LOAD AC contacts for spot welding, makes me thing you do need it. Maybe it even requires isolated high voltage there, which would make this design require an isolating 1:1 transformer in front.

     

    This is sensible advice, I believe I mentioned in earlier posts my concerns about the lack of an earth connection. It all comes back to safety.

     

    George Thomas wrote:

     

    My idea for the connector was this.

    So what happened to these connectors? It looks like you still have the old ones in the design?

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
>