Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) AC mains on a PCB ?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 107 replies
  • Answers 10 answers
  • Subscribers 193 subscribers
  • Views 21278 views
  • Users 0 members are here
Related

AC mains on a PCB ?

anishkgt
anishkgt over 10 years ago

A total newbie to eagle design and PCB fab. So plase bear with on my silly questions, trying to learn.

 

I have pcb that is schematically completed with the layout. Before i start the fabrication process i need some expert advise if the components placed and the wires routed are ok for the ac mains and the others. The load here will be a transformer. The ac mains are 240VAC and all works well as designed in the schematic on a bread broad except for the load for which MOC3023 is yet to arrive from where i've ordered.

 

 

 

Thanks in advance.

 

image

 

image

  • Sign in to reply
  • Cancel
  • autodeskguest
    0 autodeskguest over 10 years ago in reply to anishkgt

    On 11/09/16 12:02, George Thomas wrote:

    Why two thrustirs to control the load and am trouble witching on yhe Triac.

     

    Triacs can suffer commutation problems with certain types of load -

    highly inductive (like a transformer) is one of the problem cases. The

    problem exhibits as a failure to turn off at the end of a half-cycle. I

    think this is more of an issue when PWMing the mains (light dimmer

    style), which is why I asked that question earlier. For that type of

    application a pair of back-to-back thyristors is more robust.

     

    It may not matter for your application if you occasionally get an extra

    half-cycle (10ms) as long as that is all you suffer. If you find that

    you get worse than that, the two-thyristor design is what you need.

     

    http://link.springer.com/chapter/10.1007%2F978-1-4612-9877-9_12 is worth

    reading on this.

     

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago

    came across this Spot welder controller from the web and he seem to be using tvs diodes as well. Why two thrustirs to control the load and am trouble witching on yhe Triac.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to michaelkellett

    Michael Kellett wrote:

     

    For mains input spike suppression I think you are much better off with this kind of device:

     

    http://uk.farnell.com/epcos/b72214s0231k101/varistor-60-0j-230vac/dp/1004389

    B72214S0231K101

    Farnell 1004389

     

    Yes you are probably right, AC power supplies is a little off my usual area of expertise. It seems some prefer to use a TVS rather than MOV's because MOV's degrade over time every time they see a spike. I was wondering if for this applications, with the AC to the load being switched on and off to a transformer being used for spot welding, whether there would be regular spikes because of that and hence something that can withstand many spikes without degradation may be better?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 10 years ago in reply to rachaelp

    For mains input spike suppression I think you are much better off with this kind of device:

     

    http://uk.farnell.com/epcos/b72214s0231k101/varistor-60-0j-230vac/dp/1004389

    B72214S0231K101

    Farnell 1004389

     

    This one is rated at peak current of 4500A.

    Make sure you pick one rated and intended for the mains voltage it will experience.

    This kind of part has  a much larger volume of material to absorb spike energy than a 'transorb' zener diode like device at a similar price point.

     

    Generally speaking you should not expect the transient suppressor to blow fuses.

     

    It is not normal to protect mains powered equipment from continuous application of excessive voltage - but it should be designed to be happy with the maximum allowed in the locale in which it is used. (I would go for nominal +20% if possible - in the UK the mains is supposed to be 230V AC within  -6%, +10% tolerance).

     

     

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    George Thomas wrote:

     

    Does digikey ship international ?

    Yes they do :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago

    Yea doing GND first would be a better idea like you said it would give a clear view of the other traces to be routed.

     

    Does digikey ship international ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    George Thomas wrote:

     

    So i've nearly placed all the components like in the second layout rachaelp. Would it be ideal to connect all the positive/signals and later add a polygon and name it GND and all the negatives would be connected that way.

     

    Yes that's fine. I actually drew the GND polygon in early to clear away air wires so I had a better idea of how many more nets needed routing. Then once I had sorted the pinout on the MEGA8 to stop unnecessary net crossing it all went in really easily.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 10 years ago in reply to anishkgt

    Hi George,

     

    George Thomas wrote:

     

    How is this from newark ?

     

    That's the right sort of part in general but in my opinion its peak current is too low. I'm not sure what inline fuse you are having, but I think the TVS should have a peak current rating significantly above what is needed to blow that fuse. Maybe something like this: http://www.digikey.co.uk/product-detail/en/stmicroelectronics/1.5KE440CA/497-12742-1-ND/2873806

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago in reply to anishkgt

    So i've nearly placed all the components like in the second layout rachaelp. Would it be ideal to connect all the positive/signals and later add a polygon and name it GND and all the negatives would be connected that way.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 10 years ago in reply to rachaelp

    How is this from newark ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>