EAGLE User Support (English) AC mains on a PCB ?
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
  • State Verified Answer
  • Replies 107 replies
  • Answers 10 answers
  • Subscribers 186 subscribers
  • Views 18171 views
  • Users 0 members are here
Related

AC mains on a PCB ?

anishkgt
anishkgt over 9 years ago

A total newbie to eagle design and PCB fab. So plase bear with on my silly questions, trying to learn.

 

I have pcb that is schematically completed with the layout. Before i start the fabrication process i need some expert advise if the components placed and the wires routed are ok for the ac mains and the others. The load here will be a transformer. The ac mains are 240VAC and all works well as designed in the schematic on a bread broad except for the load for which MOC3023 is yet to arrive from where i've ordered.

 

 

 

Thanks in advance.

 

image

 

image

  • Sign in to reply
  • Cancel

Top Replies

  • rachaelp
    rachaelp over 9 years ago in reply to anishkgt +2
    Hi George, It looks like you're really learning a lot with this design and you've had lots of good advice from people on this thread already and the difference between the initial version you posted and…
  • michaelkellett
    michaelkellett over 9 years ago in reply to rachaelp +1 suggested
    For mains input spike suppression I think you are much better off with this kind of device: http://uk.farnell.com/epcos/b72214s0231k101/varistor-60-0j-230vac/dp/1004389 Farnell 1004389 This one is rated…
  • autodeskguest
    autodeskguest over 9 years ago in reply to anishkgt +1 suggested
    On 11/09/16 12:02, George Thomas wrote: Why two thrustirs to control the load and am trouble witching on yhe Triac. Triacs can suffer commutation problems with certain types of load - highly inductive…
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to anishkgt

    On 05/09/16 23:57, George Thomas wrote:

    Well, after a while, i've managed to move IC5 away from R20, i've also changed the angle for the R23 and IC5 making them more routable during Auto tracking

    .

     

    No, I think you misunderstood. There's no problem with IC5 being close

    to R20, there's a problem with the tracks connected to IC5 being close

    together. You absolutely don't want them passing between the pins!

     

    Rotate IC5 by 180 degrees and move it left by 0.2" or so. Then rotate

    R20 by 180 degrees and move it due south of R22.

     

    IC5 is an optoisolator - its whole purpose is to isolate - so make sure

    you maintain an isolation gap across it.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • michaelkellett
    0 michaelkellett over 9 years ago in reply to autodeskguest

    It might help you with getting the separation between mains and low voltage side stuff if you make sure that there is a gap of at least 4.5 mm between mains and low voltage tracks (this is about the separation on the opto isolator package).

     

    Here's a useful guide to this kind of thing:

     

     

    cache.freescale.com/files/analog/doc/app_note/AN3962.pdf

     

    MK

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Reject Answer
    • Cancel
  • anishkgt
    0 anishkgt over 9 years ago in reply to michaelkellett

    Thanks mate that was very helpful.

    there is a gap of at least 4.5 mm between mains and low voltage tracks (this is about the separation on the opto isolator package).

    ah that explains the use of the opto-couplers. I do know that but that made more sense to why they should be separated.:)

     

    so what all the knowledge gain from this post I am guess this the layout should be ok.

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • rachaelp
    0 rachaelp over 9 years ago in reply to anishkgt

    Hi George,

     

    It looks like you're really learning a lot with this design and you've had lots of good advice from people on this thread already and the difference between the initial version you posted and this latest version is quite substantial. I do wonder if the placement of the connectors, transformer etc could be rearranged such that the AC traces flow much straighter into the transformer, it's hard to see when you don't have the actual design files to experiment on but I think there is scope for further improvement there. I do also wonder if some of your clearances between conductors, for example around the connectors, are a little small. It might also be worth looking at some reference designs for mains power supply circuits to see how they deal with things like EMI filtering, circuit protection and most importantly safety.

     

    The latter is something I can't stress enough. Do your own research and ensure that your circuit, how it's fitted into your final design, and the system as a whole work together to ensure neither you, nor anybody else, can hurt themselves. Sorry if that sounds a little nannying but as you are new to circuit design and you're jumping straight into a mains powered product it probably should be said. All the advice people can give you here is great but you need to do your own research and ensure that what you finally make is safe and this is entirely your own responsibility.

     

    Best Regards,

     

    Rachael

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • MattyLad
    0 MattyLad over 9 years ago in reply to anishkgt

    Looking better on the mains side, although I would still make the tracks to IC 5 thicker - just for durability.

     

    Please review your ground connections, you have some that go through very thin slivers.

    Also under the big IC you have floating copper (not connected to anything).

    A poor return will make your board bad for EMC also.

     

    Matt.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to MattyLad

    Am 06.09.2016 um 17:08 schrieb MattyLad:

    Looking better on the mains side, although I would still make the tracks to IC 5 thicker - just for durability.

     

    Please review your ground connections, you have some that go through very thin slivers.

    Also under the big IC you have floating copper (not connected to anything).

    A poor return will make your board bad for EMC also.

     

    Matt.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/205233

     

     

    Actually I didn't want to cut in here, but I don't like your AC section

    at all.

    Distances on terminals are usually just above the minimums.

    With your track from transformer pin5 to the AC terminal you lessen the

    distance to the second AC terminal pin.

    Although the rule says the shorter the better for large currents it

    doesn't say to forget the minimum distances image

    I would:

    1. exchange the transformer pins 1/5

    2. move R22 right above R20

    3. move the triac about half way between the terminals and R22

    4. move your tracks straight away from the terminals to get a save

    distance before turn towards the triac pins.

    5. The trigger line should go a little straight away from the triac

    before turning towards the optocoupler.

     

    --

    Mit freundlichen Grüßen / With best regards

     

    Joern Paschedag

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 9 years ago in reply to MattyLad

    so talking about removing floating copper, how can it be done manually ? tried to find it but could not. So I checked the creepage table and to me it was so much unfamiliar terms and French. I managed to learn that 8mm is the minimum distance between AC and DC that needs to be kept. other than that nothing.

     

    Would anyone be knowing a simpler document that I could read.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • D_Hersey
    0 D_Hersey over 9 years ago in reply to anishkgt

    The way to take a little foil off of a pc-board is to slice through it with a sharp, newish pen-knife and then heat up the foil one wants to remove with a soldering iron and scrape it away.  The adhesive usually melts precipitantly.

     

    As an aside, the colored boards have a top anti-static layer, sometimes it is important to scrape this away between op-amp inputs. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to anishkgt

    On 06/09/16 17:47, George Thomas wrote:

    so talking about removing floating copper, how can it be done manually ? tried to find it but could not.

     

    Assuming you mean how to avoid the unconnected bits on an Eagle board

    design, the trick is to turn the "orphans" setting OFF on the polygon.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • anishkgt
    0 anishkgt over 9 years ago in reply to autodeskguest

    yea ! your right. That was un-ticked all the while. Ticking it would pour more copper in those empty spaces under IC1.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
<>