Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle: How to convert a 2 layer board to 4 layer?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Subscribers 189 subscribers
  • Views 9461 views
  • Users 0 members are here
  • eagle cad
  • 4-layers
Related

Eagle: How to convert a 2 layer board to 4 layer?

dlchambers
dlchambers over 9 years ago

I have a 2 layer design in Eagle 7.7.0

I want to convert it to 4 layer - basically insert 2 inner layers (power, ground).

Can this be done, and if so, how is it done?

 

Thanks,

-Dave

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 10/21/2016 10:11 AM, Dave Chambers wrote:

    I have a 2 layer design in Eagle 7.7.0

    I want to convert it to 4 layer - basically insert 2 inner layers (power, ground).

    Can this be done, and if so, how is it done?

     

    Thanks,

    -Dave

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/207842

     

     

    Hi Dave,

     

    I hope you're doing well. The short answer is:

     

    1. Click on DRC

    2. Go to the layers tab

    3. Change the setup equation from (1*16) to:

    (12+1516)

    4. Click Apply

    5. Click Cancel

     

    The long answer:

     

    Above I have given you one of the simplest 4 layer setups. It does not

    enable blind or buried vias, so if you need those the above

    configuration won't help.

     

    For more information, please see section 6.5 of the EAGLE manual.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dlchambers
    0 dlchambers over 9 years ago in reply to autodeskguest

    OK, that helps a bit.

    played with the layer setup editor, and I understand what "*" and "+" mean, but the ascending rule is a bit odd.

    I want to be able to connect 1 and 2, 1 and 3, 1 and 4. No need to connect 2 or 3 or 4 to each other.

    How do I specify that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to dlchambers

    On 10/21/2016 12:28 PM, Dave Chambers wrote:

    OK, that helps a bit.

    played with the layer setup editor, and I understand what "*" and "+" mean, but the ascending rule is a bit odd.

    I want to be able to connect 1 and 2, 1 and 3, 1 and 4. No need to connect 2 or 3 or 4 to each other.

    How do I specify that?

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/207844

     

     

    Hi Dave,

     

    It is important to understand that you likely don't need to have to many

    different via configurations. The default through hole via, can reach

    all the layers. EAGLE will automatically isolate the via from any layers

    it is not supposed to connect to.

     

    Using blind and buried vias increases the cost of the board

    substantially. So unless you have a super tight layout I would

    discourage their use.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Reply
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to dlchambers

    On 10/21/2016 12:28 PM, Dave Chambers wrote:

    OK, that helps a bit.

    played with the layer setup editor, and I understand what "*" and "+" mean, but the ascending rule is a bit odd.

    I want to be able to connect 1 and 2, 1 and 3, 1 and 4. No need to connect 2 or 3 or 4 to each other.

    How do I specify that?

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/207844

     

     

    Hi Dave,

     

    It is important to understand that you likely don't need to have to many

    different via configurations. The default through hole via, can reach

    all the layers. EAGLE will automatically isolate the via from any layers

    it is not supposed to connect to.

     

    Using blind and buried vias increases the cost of the board

    substantially. So unless you have a super tight layout I would

    discourage their use.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to dlchambers

    On 10/23/2016 10:57 AM, Dave Chambers wrote:

    the Element14 web interface interprets the asterisks in newsgroup

    postings as "change to bold"

    Yes, that would explain it - I've noticed the bold/italics and was

    puzzled by them. So all along you've been saying "1 star 1 star 15

    star 16" ?

     

     

    For Sunstone (prepreg - core - prepreg), I'd use "1 plus 2 star 15 plus

    16", which is exactly what

    you surmised.

     

    For Advanced circuits (core - prepreg - core), "1 star 2 plus 15 star

    16" is correct.

     

    As Jorge pointed out, if you're using through vias it's mostly

    irrelevant. And unless you have real need to use blind or buried vias,

    through vias are what you want to use.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dlchambers
    0 dlchambers over 9 years ago in reply to autodeskguest

    > the Element14 web interface interprets the asterisks in newsgroup postings as "change to bold"

    Yes, that would explain it - I've noticed the bold/italics and was puzzled by them.

    So all along you've been saying "1 star 1 star 15 star 16" ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to autodeskguest

    On 10/22/2016 10:50 PM, Reece R. Pollack wrote:

    On 10/22/2016 02:32 PM, Dave Chambers wrote:

    "(12*1516)"  (w/o quotes) is not a valid setup string. Eagle

    complains that layer 1516 is an invalid layer. Need some sort of

    separator between each number.

     

    I'm using Sunstone, which has core between 2 and 15, then prepreg

    between 1&2 and 15&16 So, for the simplest stack-up, that would be

    (12*1516) That isn't really what I initially was looking for, but

    as @JorgeGarcia said, Eagle will automatically connect the layers, so

    take that as an answer.

     

    I'm confused. I don't see any difference between what I wrote and what

    you say works. Both read "(12*1516)" on my screen and is exactly what

    I've used with Eagle versions 6 and 7 (w/o the quotes, of course) for

    production by PCB Pool.

     

    If you want through vias that connect to all layers, this works just

    fine. It's when you get into blind and buried vias that only connect

    certain layers that things get interesting and the Eagle layer setup

    really becomes critical.

     

     

    I suspect the problem is the Element14 web interface. It interprets the

    asterisks in newsgroup postings as "change to bold" indicators and

    doesn't show them. The EagleCentral.ca web interface shows the posts

    properly.

     

    Is the Element14 web interface going to go away now that Farnell sold

    CadSoft to Autodesk? Please?

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to dlchambers

    On 10/22/2016 02:32 PM, Dave Chambers wrote:

    "(12*1516)"  (w/o quotes) is not a valid setup string. Eagle

    complains that layer 1516 is an invalid layer. Need some sort of

    separator between each number.

     

    I'm using Sunstone, which has core between 2 and 15, then prepreg

    between 1&2 and 15&16 So, for the simplest stack-up, that would be

    (12*1516) That isn't really what I initially was looking for, but

    as @JorgeGarcia said, Eagle will automatically connect the layers, so

    take that as an answer.

     

    I'm confused. I don't see any difference between what I wrote and what

    you say works. Both read "(12*1516)" on my screen and is exactly what

    I've used with Eagle versions 6 and 7 (w/o the quotes, of course) for

    production by PCB Pool.

     

    If you want through vias that connect to all layers, this works just

    fine. It's when you get into blind and buried vias that only connect

    certain layers that things get interesting and the Eagle layer setup

    really becomes critical.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • omega-5
    0 omega-5 over 9 years ago in reply to dlchambers

    Am 22.10.2016 um 20:32 schrieb Dave Chambers:

    "(12*1516)"  (w/o quotes) is not a valid setup string.

    Eagle complains that layer 1516 is an invalid layer. Need some sort of separator between each number.

     

    I'm using Sunstone, which has core between 2 and 15, then prepreg between 1&2 and 15&16

    So, for the simplest stack-up, that would be (12*1516)

    That isn't really what I initially was looking for, but as @JorgeGarcia said, Eagle will automatically connect the layers, so take that as an answer.

     

    Thanks to all for their input & patience.

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/207869

     

     

     

    Hi Dave,

    what do you think about this? ((12)*(1516))

     

    Freundliche Grüße / Kind regards

    Friedrich

    -


    ... use NNTP://news.cadsoft.de and a

    functional news reader like Thunderbird!

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dlchambers
    0 dlchambers over 9 years ago in reply to autodeskguest

    "(12*1516)"  (w/o quotes) is not a valid setup string.

    Eagle complains that layer 1516 is an invalid layer. Need some sort of separator between each number.

     

    I'm using Sunstone, which has core between 2 and 15, then prepreg between 1&2 and 15&16

    So, for the simplest stack-up, that would be (1+2*15+16)

    That isn't really what I initially was looking for, but as @JorgeGarcia said, Eagle will automatically connect the layers, so take that as an answer.

     

    Thanks to all for their input & patience.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to dlchambers

    On 10/21/2016 03:25 PM, Dave Chambers wrote:

    Excellent info - thanks.

     

    So then which setup is the "standard" 4-layer rule:

    (12)+(1516)     (2 cores with prepreg in between)

    or

    (12)(15+16)  (3 cores)

     

    The stack-up depends entirely on who is making the boards, and whether

    you're looking for a quick-turn prototype or making a large production run.

     

    Advanced Circuits advertises their quick-turn 0.062" 4-layer board as

    being two cores with prepreg between them. Without blind/buried vias

    this is properly entered as "(12+1516)".

     

    However, AP Circuits, Sunstone, PCB-Pool, and OshPark stack-ups are one

    core with prepreg layers added to either side. Without blind/buried

    vias, this is properly entered as "(12*1516)".

     

    If you're not doing blind or buried vias it doesn't make much difference

    which way you enter the stack-up into Eagle. If you ARE doing

    blind/buried, the pluses, asterisks, and extra parentheses tell Eagle

    where you can and can't place vias between the various layers.

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dlchambers
    0 dlchambers over 9 years ago in reply to autodeskguest

    Excellent info - thanks.

     

    So then which setup is the "standard" 4-layer rule:

    (1*2)+(15*16)     (2 cores with prepreg in between)

    or

    (1+2)+(15+16)  (3 cores)

     

    -Dave