Autodesk EAGLE
  • Products & Partners
  • More
Autodesk EAGLE
EAGLE User Support (English) Eagle: How to convert a 2 layer board to 4 layer?
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Autodesk EAGLE to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Verified Answer
  • Replies 11 replies
  • Subscribers 189 subscribers
  • Views 9469 views
  • Users 0 members are here
  • eagle cad
  • 4-layers
Related

Eagle: How to convert a 2 layer board to 4 layer?

dlchambers
dlchambers over 9 years ago

I have a 2 layer design in Eagle 7.7.0

I want to convert it to 4 layer - basically insert 2 inner layers (power, ground).

Can this be done, and if so, how is it done?

 

Thanks,

-Dave

  • Sign in to reply
  • Cancel
Parents
  • autodeskguest
    0 autodeskguest over 9 years ago

    On 10/21/2016 10:11 AM, Dave Chambers wrote:

    I have a 2 layer design in Eagle 7.7.0

    I want to convert it to 4 layer - basically insert 2 inner layers (power, ground).

    Can this be done, and if so, how is it done?

     

    Thanks,

    -Dave

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/207842

     

     

    Hi Dave,

     

    I hope you're doing well. The short answer is:

     

    1. Click on DRC

    2. Go to the layers tab

    3. Change the setup equation from (1*16) to:

    (12+1516)

    4. Click Apply

    5. Click Cancel

     

    The long answer:

     

    Above I have given you one of the simplest 4 layer setups. It does not

    enable blind or buried vias, so if you need those the above

    configuration won't help.

     

    For more information, please see section 6.5 of the EAGLE manual.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dlchambers
    0 dlchambers over 9 years ago in reply to autodeskguest

    OK, that helps a bit.

    played with the layer setup editor, and I understand what "*" and "+" mean, but the ascending rule is a bit odd.

    I want to be able to connect 1 and 2, 1 and 3, 1 and 4. No need to connect 2 or 3 or 4 to each other.

    How do I specify that?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to dlchambers

    On 10/21/2016 12:28 PM, Dave Chambers wrote:

    OK, that helps a bit.

    played with the layer setup editor, and I understand what "*" and "+" mean, but the ascending rule is a bit odd.

    I want to be able to connect 1 and 2, 1 and 3, 1 and 4. No need to connect 2 or 3 or 4 to each other.

    How do I specify that?

     

    --

    To view any images and attachments in this post, visit:

    https://www.element14.com/community/message/207844

     

     

    Hi Dave,

     

    It is important to understand that you likely don't need to have to many

    different via configurations. The default through hole via, can reach

    all the layers. EAGLE will automatically isolate the via from any layers

    it is not supposed to connect to.

     

    Using blind and buried vias increases the cost of the board

    substantially. So unless you have a super tight layout I would

    discourage their use.

     

    hth,

    Jorge Garcia

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Reject Answer
    • Cancel
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to dlchambers

    On 10/23/2016 10:57 AM, Dave Chambers wrote:

    the Element14 web interface interprets the asterisks in newsgroup

    postings as "change to bold"

    Yes, that would explain it - I've noticed the bold/italics and was

    puzzled by them. So all along you've been saying "1 star 1 star 15

    star 16" ?

     

     

    For Sunstone (prepreg - core - prepreg), I'd use "1 plus 2 star 15 plus

    16", which is exactly what

    you surmised.

     

    For Advanced circuits (core - prepreg - core), "1 star 2 plus 15 star

    16" is correct.

     

    As Jorge pointed out, if you're using through vias it's mostly

    irrelevant. And unless you have real need to use blind or buried vias,

    through vias are what you want to use.

     

     

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • dlchambers
    0 dlchambers over 9 years ago in reply to autodeskguest

    > the Element14 web interface interprets the asterisks in newsgroup postings as "change to bold"

    Yes, that would explain it - I've noticed the bold/italics and was puzzled by them.

    So all along you've been saying "1 star 1 star 15 star 16" ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • dlchambers
    0 dlchambers over 9 years ago in reply to autodeskguest

    > the Element14 web interface interprets the asterisks in newsgroup postings as "change to bold"

    Yes, that would explain it - I've noticed the bold/italics and was puzzled by them.

    So all along you've been saying "1 star 1 star 15 star 16" ?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • autodeskguest
    0 autodeskguest over 9 years ago in reply to dlchambers

    On 10/23/2016 10:57 AM, Dave Chambers wrote:

    the Element14 web interface interprets the asterisks in newsgroup

    postings as "change to bold"

    Yes, that would explain it - I've noticed the bold/italics and was

    puzzled by them. So all along you've been saying "1 star 1 star 15

    star 16" ?

     

     

    For Sunstone (prepreg - core - prepreg), I'd use "1 plus 2 star 15 plus

    16", which is exactly what

    you surmised.

     

    For Advanced circuits (core - prepreg - core), "1 star 2 plus 15 star

    16" is correct.

     

    As Jorge pointed out, if you're using through vias it's mostly

    irrelevant. And unless you have real need to use blind or buried vias,

    through vias are what you want to use.